<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic MIPI camera driver in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/MIPI-camera-driver/m-p/1448508#M19309</link>
    <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;I am going to implement a interface to a&amp;nbsp;AR0234CS camera on a iMX1176DV using MIPI interface.&lt;/P&gt;&lt;P&gt;I have made software fore many years, but this is my first time on a iMX platform.&lt;/P&gt;&lt;P&gt;The project I have to implement the interface into, has some MIPI definitions, but no MIPI libraries or interfaces.&lt;/P&gt;&lt;P&gt;Are there any examples or project start code generator to make the interface?&lt;/P&gt;&lt;P&gt;Thank you for your help.&lt;/P&gt;&lt;P&gt;Br Johnny&lt;/P&gt;</description>
    <pubDate>Mon, 25 Apr 2022 11:41:44 GMT</pubDate>
    <dc:creator>JohnnyK</dc:creator>
    <dc:date>2022-04-25T11:41:44Z</dc:date>
    <item>
      <title>MIPI camera driver</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/MIPI-camera-driver/m-p/1448508#M19309</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;I am going to implement a interface to a&amp;nbsp;AR0234CS camera on a iMX1176DV using MIPI interface.&lt;/P&gt;&lt;P&gt;I have made software fore many years, but this is my first time on a iMX platform.&lt;/P&gt;&lt;P&gt;The project I have to implement the interface into, has some MIPI definitions, but no MIPI libraries or interfaces.&lt;/P&gt;&lt;P&gt;Are there any examples or project start code generator to make the interface?&lt;/P&gt;&lt;P&gt;Thank you for your help.&lt;/P&gt;&lt;P&gt;Br Johnny&lt;/P&gt;</description>
      <pubDate>Mon, 25 Apr 2022 11:41:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/MIPI-camera-driver/m-p/1448508#M19309</guid>
      <dc:creator>JohnnyK</dc:creator>
      <dc:date>2022-04-25T11:41:44Z</dc:date>
    </item>
    <item>
      <title>Re: MIPI camera driver</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/MIPI-camera-driver/m-p/1450945#M19377</link>
      <description>&lt;P&gt;Hello&lt;BR /&gt;Hope you are well.&lt;/P&gt;
&lt;P&gt;You can use the SDK examples as reference: &lt;A href="https://mcuxpresso.nxp.com/en/welcome" target="_blank"&gt;https://mcuxpresso.nxp.com/en/welcome&amp;nbsp;&lt;/A&gt;&lt;BR /&gt;This application note also can be helpful, it has a chapter that explains the usage of MIPI-CSI example: &lt;A href="https://www.nxp.com/docs/en/application-note/AN13573.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/application-note/AN13573.pdf&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;If you have more questions do not hesitate to ask me.&lt;BR /&gt;Best regards,&lt;BR /&gt;Omar&lt;/P&gt;</description>
      <pubDate>Thu, 28 Apr 2022 22:45:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/MIPI-camera-driver/m-p/1450945#M19377</guid>
      <dc:creator>Omar_Anguiano</dc:creator>
      <dc:date>2022-04-28T22:45:34Z</dc:date>
    </item>
    <item>
      <title>Re: MIPI camera driver</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/MIPI-camera-driver/m-p/1451137#M19387</link>
      <description>&lt;P&gt;Thank you Omar, I will look into that.&lt;/P&gt;&lt;P&gt;Have a great day &lt;LI-EMOJI id="lia_slightly-smiling-face" title=":slightly_smiling_face:"&gt;&lt;/LI-EMOJI&gt;&lt;/P&gt;&lt;P&gt;Br Johnny&lt;/P&gt;</description>
      <pubDate>Fri, 29 Apr 2022 07:54:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/MIPI-camera-driver/m-p/1451137#M19387</guid>
      <dc:creator>JohnnyK</dc:creator>
      <dc:date>2022-04-29T07:54:04Z</dc:date>
    </item>
    <item>
      <title>Re: MIPI camera driver</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/MIPI-camera-driver/m-p/1526834#M21736</link>
      <description>Hi Omar&lt;BR /&gt;Would you have any example code for connecting an CSI parallel camera to the iMX1176DV?&lt;BR /&gt;I tried to toggle the VID_MUX_CTRL to make it take data from parallel input instead of CSI2, but that is not enough.&lt;BR /&gt;Hope to get a link to a good example.&lt;BR /&gt;Br Johnny</description>
      <pubDate>Thu, 22 Sep 2022 15:10:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/MIPI-camera-driver/m-p/1526834#M21736</guid>
      <dc:creator>JohnnyK</dc:creator>
      <dc:date>2022-09-22T15:10:45Z</dc:date>
    </item>
  </channel>
</rss>