<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Using both UVC and UAC in RT1060 in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Using-both-UVC-and-UAC-in-RT1060/m-p/1447150#M19268</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am trying to integrate both&amp;nbsp;UVC and UAC functions with the MIMXRT1060-EVK, but found that there is only seperated sample code for just UVC or UAC in the SDK.&lt;/P&gt;&lt;P&gt;The sample code for UAC is "evkmimxrt1060_maestro_usb_mic" which only for FreeRTOS.&lt;/P&gt;&lt;P&gt;And the UVC sample code is just for virtual camera, which is "evkmimxrt1060_dev_video_virtual_camera_bm".&lt;/P&gt;&lt;P&gt;I hope NXP will provide a sample code which can support both UVC and UAC functions for the MIMXRT1060-EVK. Thanks a lot.&lt;/P&gt;&lt;P&gt;BTW, I found a similar topic "Using 2 ISO endpoint tranfer in RT1060" in the forums, but it had NOT provided a final solution yet.&lt;/P&gt;</description>
    <pubDate>Thu, 21 Apr 2022 09:55:48 GMT</pubDate>
    <dc:creator>MartinYe</dc:creator>
    <dc:date>2022-04-21T09:55:48Z</dc:date>
    <item>
      <title>Using both UVC and UAC in RT1060</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Using-both-UVC-and-UAC-in-RT1060/m-p/1447150#M19268</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am trying to integrate both&amp;nbsp;UVC and UAC functions with the MIMXRT1060-EVK, but found that there is only seperated sample code for just UVC or UAC in the SDK.&lt;/P&gt;&lt;P&gt;The sample code for UAC is "evkmimxrt1060_maestro_usb_mic" which only for FreeRTOS.&lt;/P&gt;&lt;P&gt;And the UVC sample code is just for virtual camera, which is "evkmimxrt1060_dev_video_virtual_camera_bm".&lt;/P&gt;&lt;P&gt;I hope NXP will provide a sample code which can support both UVC and UAC functions for the MIMXRT1060-EVK. Thanks a lot.&lt;/P&gt;&lt;P&gt;BTW, I found a similar topic "Using 2 ISO endpoint tranfer in RT1060" in the forums, but it had NOT provided a final solution yet.&lt;/P&gt;</description>
      <pubDate>Thu, 21 Apr 2022 09:55:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Using-both-UVC-and-UAC-in-RT1060/m-p/1447150#M19268</guid>
      <dc:creator>MartinYe</dc:creator>
      <dc:date>2022-04-21T09:55:48Z</dc:date>
    </item>
    <item>
      <title>Re: Using both UVC and UAC in RT1060</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Using-both-UVC-and-UAC-in-RT1060/m-p/1448404#M19306</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/199856"&gt;@MartinYe&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;I'm sorry there isn't such demo. You can refer to&amp;nbsp;&lt;SPAN&gt;usb_device_composite_hid_audio_unified and add UVC to it.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Regards,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Jing&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 25 Apr 2022 08:40:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Using-both-UVC-and-UAC-in-RT1060/m-p/1448404#M19306</guid>
      <dc:creator>jingpan</dc:creator>
      <dc:date>2022-04-25T08:40:13Z</dc:date>
    </item>
  </channel>
</rss>