<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic SDRAM with 8-bit data bus connection in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/SDRAM-with-8-bit-data-bus-connection/m-p/1440754#M19062</link>
    <description>&lt;P&gt;We want to connect an RT1020 to an external SDRAM through SEMC. We are looking at ISSI&amp;nbsp;IS42S81600F-7TLI. This memory has an 8-bit data bus. The&amp;nbsp;RT1020 Reference Manual only has a table indicating the connection with a 16-bit SDRAM.&amp;nbsp;&lt;/P&gt;&lt;P&gt;We assumed that the connection is as follows.&lt;BR /&gt;&lt;BR /&gt;SEMC_DATA00 -&amp;gt; DQ0&amp;nbsp;&lt;BR /&gt;SEMC_DATA01&amp;nbsp;-&amp;gt; DQ1&lt;BR /&gt;SEMC_DATA02&amp;nbsp;-&amp;gt; DQ2&lt;BR /&gt;SEMC_DATA03&amp;nbsp;-&amp;gt; DQ3&lt;BR /&gt;SEMC_DATA04&amp;nbsp;-&amp;gt; DQ4&lt;BR /&gt;SEMC_DATA05&amp;nbsp;-&amp;gt; DQ5&lt;BR /&gt;SEMC_DATA06&amp;nbsp;-&amp;gt; DQ6&lt;BR /&gt;SEMC_DATA07&amp;nbsp;-&amp;gt; DQ7&lt;BR /&gt;SEMC_ADDR00&amp;nbsp;-&amp;gt; A0&lt;BR /&gt;SEMC_ADDR01&amp;nbsp;-&amp;gt; A1&lt;BR /&gt;SEMC_ADDR02 -&amp;gt; A2&lt;BR /&gt;SEMC_ADDR03&amp;nbsp;-&amp;gt; A3&lt;BR /&gt;SEMC_ADDR04&amp;nbsp;-&amp;gt; A4&lt;BR /&gt;SEMC_ADDR05&amp;nbsp;-&amp;gt; A5&lt;BR /&gt;SEMC_ADDR06&amp;nbsp;-&amp;gt; A6&lt;BR /&gt;SEMC_ADDR07 - &amp;gt;A7&lt;BR /&gt;SEMC_ADDR08&amp;nbsp;-&amp;gt; A8&lt;BR /&gt;SEMC_ADDR09&amp;nbsp;-&amp;gt; A9&lt;BR /&gt;SEMC_ADDR10&amp;nbsp;-&amp;gt; A10&lt;BR /&gt;SEMC_ADDR11&amp;nbsp;-&amp;gt; A11&lt;BR /&gt;SEMC_BA0&amp;nbsp;-&amp;gt; BA0&lt;BR /&gt;SEMC_BA1&amp;nbsp;-&amp;gt; BA1&lt;BR /&gt;SEMC_WE&amp;nbsp;-&amp;gt; WE&lt;BR /&gt;SEMC_CAS&amp;nbsp;-&amp;gt; CAS&lt;BR /&gt;SEMC_RAS&amp;nbsp;-&amp;gt; RAS&lt;BR /&gt;SEMC_CS0&amp;nbsp;-&amp;gt; CS&lt;BR /&gt;SEMC_DM0&amp;nbsp;-&amp;gt; DQM&lt;/P&gt;&lt;P&gt;Our main questions is about connection. The memory only has one "Data Input/Output Mask" (DQM). We have to connect it to DM0 or DM1 in SEMC?&lt;/P&gt;&lt;P&gt;There is one other thing to keep in mind using 8-bit data bus SDRAM memories?&lt;/P&gt;</description>
    <pubDate>Thu, 07 Apr 2022 16:02:51 GMT</pubDate>
    <dc:creator>gtalocchino</dc:creator>
    <dc:date>2022-04-07T16:02:51Z</dc:date>
    <item>
      <title>SDRAM with 8-bit data bus connection</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/SDRAM-with-8-bit-data-bus-connection/m-p/1440754#M19062</link>
      <description>&lt;P&gt;We want to connect an RT1020 to an external SDRAM through SEMC. We are looking at ISSI&amp;nbsp;IS42S81600F-7TLI. This memory has an 8-bit data bus. The&amp;nbsp;RT1020 Reference Manual only has a table indicating the connection with a 16-bit SDRAM.&amp;nbsp;&lt;/P&gt;&lt;P&gt;We assumed that the connection is as follows.&lt;BR /&gt;&lt;BR /&gt;SEMC_DATA00 -&amp;gt; DQ0&amp;nbsp;&lt;BR /&gt;SEMC_DATA01&amp;nbsp;-&amp;gt; DQ1&lt;BR /&gt;SEMC_DATA02&amp;nbsp;-&amp;gt; DQ2&lt;BR /&gt;SEMC_DATA03&amp;nbsp;-&amp;gt; DQ3&lt;BR /&gt;SEMC_DATA04&amp;nbsp;-&amp;gt; DQ4&lt;BR /&gt;SEMC_DATA05&amp;nbsp;-&amp;gt; DQ5&lt;BR /&gt;SEMC_DATA06&amp;nbsp;-&amp;gt; DQ6&lt;BR /&gt;SEMC_DATA07&amp;nbsp;-&amp;gt; DQ7&lt;BR /&gt;SEMC_ADDR00&amp;nbsp;-&amp;gt; A0&lt;BR /&gt;SEMC_ADDR01&amp;nbsp;-&amp;gt; A1&lt;BR /&gt;SEMC_ADDR02 -&amp;gt; A2&lt;BR /&gt;SEMC_ADDR03&amp;nbsp;-&amp;gt; A3&lt;BR /&gt;SEMC_ADDR04&amp;nbsp;-&amp;gt; A4&lt;BR /&gt;SEMC_ADDR05&amp;nbsp;-&amp;gt; A5&lt;BR /&gt;SEMC_ADDR06&amp;nbsp;-&amp;gt; A6&lt;BR /&gt;SEMC_ADDR07 - &amp;gt;A7&lt;BR /&gt;SEMC_ADDR08&amp;nbsp;-&amp;gt; A8&lt;BR /&gt;SEMC_ADDR09&amp;nbsp;-&amp;gt; A9&lt;BR /&gt;SEMC_ADDR10&amp;nbsp;-&amp;gt; A10&lt;BR /&gt;SEMC_ADDR11&amp;nbsp;-&amp;gt; A11&lt;BR /&gt;SEMC_BA0&amp;nbsp;-&amp;gt; BA0&lt;BR /&gt;SEMC_BA1&amp;nbsp;-&amp;gt; BA1&lt;BR /&gt;SEMC_WE&amp;nbsp;-&amp;gt; WE&lt;BR /&gt;SEMC_CAS&amp;nbsp;-&amp;gt; CAS&lt;BR /&gt;SEMC_RAS&amp;nbsp;-&amp;gt; RAS&lt;BR /&gt;SEMC_CS0&amp;nbsp;-&amp;gt; CS&lt;BR /&gt;SEMC_DM0&amp;nbsp;-&amp;gt; DQM&lt;/P&gt;&lt;P&gt;Our main questions is about connection. The memory only has one "Data Input/Output Mask" (DQM). We have to connect it to DM0 or DM1 in SEMC?&lt;/P&gt;&lt;P&gt;There is one other thing to keep in mind using 8-bit data bus SDRAM memories?&lt;/P&gt;</description>
      <pubDate>Thu, 07 Apr 2022 16:02:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/SDRAM-with-8-bit-data-bus-connection/m-p/1440754#M19062</guid>
      <dc:creator>gtalocchino</dc:creator>
      <dc:date>2022-04-07T16:02:51Z</dc:date>
    </item>
    <item>
      <title>Re: SDRAM with 8-bit data bus connection</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/SDRAM-with-8-bit-data-bus-connection/m-p/1440968#M19075</link>
      <description>&lt;P&gt;SEMC supports 8/16 bit modes, so it is ok to connect 8bit SDRAM to SEMC&lt;/P&gt;
&lt;P&gt;For 16bit SDRAM, SEMC_DM0 &amp;lt;-&amp;gt; SDRAM_DQML corresponds to DQ[7:0];&amp;nbsp;SEMC_DM1 &amp;lt;-&amp;gt; SDRAM_DQMH corresponds to DQ[15:8]&lt;/P&gt;
&lt;P&gt;For 8bit SDRAM, SEMC_DM0 &amp;lt;-&amp;gt; SDRAM_DQM corresponds to DQ[7:0], Keep SEMC_DM1 NC&lt;/P&gt;</description>
      <pubDate>Fri, 08 Apr 2022 07:32:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/SDRAM-with-8-bit-data-bus-connection/m-p/1440968#M19075</guid>
      <dc:creator>jay_heng</dc:creator>
      <dc:date>2022-04-08T07:32:22Z</dc:date>
    </item>
  </channel>
</rss>