<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX RT Crossover MCUsのトピックMaximum ADC Sample Rate</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Maximum-ADC-Sample-Rate/m-p/1431326#M18846</link>
    <description>&lt;P&gt;We are evaluating the i.MX RT 1024 for an application that requires sampling the 12-bit ADC&amp;nbsp;@ 5 mega samples per second and deliver the data to memory using the EDMA.&amp;nbsp;&lt;/P&gt;&lt;P&gt;What is the maximum ADC sample rate of the&amp;nbsp;i.MX RT 1024?&lt;/P&gt;&lt;P&gt;Can the EDAM be used to deliver the samples to RAM?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
    <pubDate>Mon, 21 Mar 2022 13:30:39 GMT</pubDate>
    <dc:creator>scottc385</dc:creator>
    <dc:date>2022-03-21T13:30:39Z</dc:date>
    <item>
      <title>Maximum ADC Sample Rate</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Maximum-ADC-Sample-Rate/m-p/1431326#M18846</link>
      <description>&lt;P&gt;We are evaluating the i.MX RT 1024 for an application that requires sampling the 12-bit ADC&amp;nbsp;@ 5 mega samples per second and deliver the data to memory using the EDMA.&amp;nbsp;&lt;/P&gt;&lt;P&gt;What is the maximum ADC sample rate of the&amp;nbsp;i.MX RT 1024?&lt;/P&gt;&lt;P&gt;Can the EDAM be used to deliver the samples to RAM?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
      <pubDate>Mon, 21 Mar 2022 13:30:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Maximum-ADC-Sample-Rate/m-p/1431326#M18846</guid>
      <dc:creator>scottc385</dc:creator>
      <dc:date>2022-03-21T13:30:39Z</dc:date>
    </item>
    <item>
      <title>Re: Maximum ADC Sample Rate</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Maximum-ADC-Sample-Rate/m-p/1431846#M18868</link>
      <description>&lt;P&gt;The ADC in i.MXRT10xx and i.MXRTxxx supports 12-bit resolution, 1MS/s sampling rate.&lt;/P&gt;
&lt;P&gt;The ADC in i.MXRT11xx supports 12-bit resolution, 4.2MS/s sampling rate.&lt;/P&gt;
&lt;P&gt;For i.MXRT1024, EDMA can be used to deliver data&lt;/P&gt;</description>
      <pubDate>Tue, 22 Mar 2022 09:20:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Maximum-ADC-Sample-Rate/m-p/1431846#M18868</guid>
      <dc:creator>jay_heng</dc:creator>
      <dc:date>2022-03-22T09:20:19Z</dc:date>
    </item>
  </channel>
</rss>