<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: RT1170 Thermal problem reboot in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1170-Thermal-problem-reboot/m-p/1429081#M18775</link>
    <description>&lt;P&gt;I have the same problem even with the RT1170 demo board from NXP! I used the "Cranck_storyboard_helloworld" project and the system dosen't reboot if I heat up the board.&lt;/P&gt;&lt;P&gt;I found that the system, during the reboot, stops before the main is launched with a BusFault exception. I think the system at higher temperature has a communication problem with the flash in the boot phase.... For example the SPI CLK is very bad during the boot phase, and seems fine instead when the main() starts... I thinks thats why the system works fine at high temperature but It can't reboot.&lt;/P&gt;&lt;P&gt;Is it possible to change the flash parameter during the boot phase, maybe with something similar to the eFuse?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 16 Mar 2022 07:55:35 GMT</pubDate>
    <dc:creator>LucaFerrario1978</dc:creator>
    <dc:date>2022-03-16T07:55:35Z</dc:date>
    <item>
      <title>RT1170 Thermal problem reboot</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1170-Thermal-problem-reboot/m-p/1428343#M18763</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I have a thermal problem with RT1170, the system work fine at 80°C, but when I turn off the system and then turn It ON, the RT1170 dosen't start anymore.&lt;/P&gt;&lt;P&gt;When the temperature will drop under 65 °C the system starts without a problem, the problem is the same in debug mode: I can't reset and restart the RT at high temperature.&lt;/P&gt;&lt;P&gt;There is a safety mechanism that prevent the RT from start?&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Tue, 15 Mar 2022 08:59:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1170-Thermal-problem-reboot/m-p/1428343#M18763</guid>
      <dc:creator>LucaFerrario1978</dc:creator>
      <dc:date>2022-03-15T08:59:19Z</dc:date>
    </item>
    <item>
      <title>Re: RT1170 Thermal problem reboot</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1170-Thermal-problem-reboot/m-p/1429081#M18775</link>
      <description>&lt;P&gt;I have the same problem even with the RT1170 demo board from NXP! I used the "Cranck_storyboard_helloworld" project and the system dosen't reboot if I heat up the board.&lt;/P&gt;&lt;P&gt;I found that the system, during the reboot, stops before the main is launched with a BusFault exception. I think the system at higher temperature has a communication problem with the flash in the boot phase.... For example the SPI CLK is very bad during the boot phase, and seems fine instead when the main() starts... I thinks thats why the system works fine at high temperature but It can't reboot.&lt;/P&gt;&lt;P&gt;Is it possible to change the flash parameter during the boot phase, maybe with something similar to the eFuse?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 16 Mar 2022 07:55:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1170-Thermal-problem-reboot/m-p/1429081#M18775</guid>
      <dc:creator>LucaFerrario1978</dc:creator>
      <dc:date>2022-03-16T07:55:35Z</dc:date>
    </item>
    <item>
      <title>Re: RT1170 Thermal problem reboot</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1170-Thermal-problem-reboot/m-p/1430380#M18808</link>
      <description>&lt;P&gt;Hi,&lt;BR /&gt;Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you. &lt;BR /&gt;1) Is it possible to change the flash parameter during the boot phase, maybe with something similar to the eFuse? &lt;BR /&gt;-- No, I'm afraid not. Did you replicate the same phenomenon on the MIMXRT1170 EVK board? &lt;BR /&gt;Moreover, did you use the oscilloscope to verify the 24 MHz crystal oscillator already boot-up?&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Fri, 18 Mar 2022 01:50:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1170-Thermal-problem-reboot/m-p/1430380#M18808</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2022-03-18T01:50:38Z</dc:date>
    </item>
  </channel>
</rss>