<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic i.MX.RT1052 - Is it possible to create a 32bit PWM module using 2 quad timers? in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/i-MX-RT1052-Is-it-possible-to-create-a-32bit-PWM-module-using-2/m-p/1428671#M18767</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Is it possible to generate a 32-bit PWM output using 2 quad timers?&lt;/P&gt;&lt;P&gt;in this post:-&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/t5/Digital-Signal-Controllers/32-bit-compare-with-the-Quad-Timer/m-p/820198" target="_blank"&gt;https://community.nxp.com/t5/Digital-Signal-Controllers/32-bit-compare-with-the-Quad-Timer/m-p/820198&lt;/A&gt;&lt;/P&gt;&lt;P&gt;xiangjun_rong mentioned that:-&lt;/P&gt;&lt;P&gt;"when you use Cascaded counter mode for T3, and T2 output is the tick for T3, the T3:T2 is NOT a standard 32bits single Timer"&lt;/P&gt;&lt;P&gt;My questions is:-&lt;/P&gt;&lt;P&gt;a) How to combine 2 quad timers to form a 32-bit PWM module if cascading 2 quad timers is not the way to do it?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Cindy&lt;/P&gt;</description>
    <pubDate>Tue, 15 Mar 2022 16:46:03 GMT</pubDate>
    <dc:creator>Cindy</dc:creator>
    <dc:date>2022-03-15T16:46:03Z</dc:date>
    <item>
      <title>i.MX.RT1052 - Is it possible to create a 32bit PWM module using 2 quad timers?</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/i-MX-RT1052-Is-it-possible-to-create-a-32bit-PWM-module-using-2/m-p/1428671#M18767</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Is it possible to generate a 32-bit PWM output using 2 quad timers?&lt;/P&gt;&lt;P&gt;in this post:-&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/t5/Digital-Signal-Controllers/32-bit-compare-with-the-Quad-Timer/m-p/820198" target="_blank"&gt;https://community.nxp.com/t5/Digital-Signal-Controllers/32-bit-compare-with-the-Quad-Timer/m-p/820198&lt;/A&gt;&lt;/P&gt;&lt;P&gt;xiangjun_rong mentioned that:-&lt;/P&gt;&lt;P&gt;"when you use Cascaded counter mode for T3, and T2 output is the tick for T3, the T3:T2 is NOT a standard 32bits single Timer"&lt;/P&gt;&lt;P&gt;My questions is:-&lt;/P&gt;&lt;P&gt;a) How to combine 2 quad timers to form a 32-bit PWM module if cascading 2 quad timers is not the way to do it?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Cindy&lt;/P&gt;</description>
      <pubDate>Tue, 15 Mar 2022 16:46:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/i-MX-RT1052-Is-it-possible-to-create-a-32bit-PWM-module-using-2/m-p/1428671#M18767</guid>
      <dc:creator>Cindy</dc:creator>
      <dc:date>2022-03-15T16:46:03Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX.RT1052 - Is it possible to create a 32bit PWM module using 2 quad timers?</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/i-MX-RT1052-Is-it-possible-to-create-a-32bit-PWM-module-using-2/m-p/1428859#M18769</link>
      <description>&lt;P&gt;Hi，&lt;BR /&gt;Thanks for your reply.&lt;BR /&gt;1）Is it possible to generate a 32-bit PWM output using 2 quad timers?&lt;BR /&gt;-- No, the Quad Timer (TMR) doesn't support the feature.&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Wed, 16 Mar 2022 01:55:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/i-MX-RT1052-Is-it-possible-to-create-a-32bit-PWM-module-using-2/m-p/1428859#M18769</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2022-03-16T01:55:50Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX.RT1052 - Is it possible to create a 32bit PWM module using 2 quad timers?</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/i-MX-RT1052-Is-it-possible-to-create-a-32bit-PWM-module-using-2/m-p/1429436#M18784</link>
      <description>&lt;P&gt;Thank you!&lt;/P&gt;</description>
      <pubDate>Wed, 16 Mar 2022 16:12:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/i-MX-RT1052-Is-it-possible-to-create-a-32bit-PWM-module-using-2/m-p/1429436#M18784</guid>
      <dc:creator>Cindy</dc:creator>
      <dc:date>2022-03-16T16:12:08Z</dc:date>
    </item>
  </channel>
</rss>