<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX RT Crossover MCUs中的主题 Re: Understanding EVK Operation</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Understanding-EVK-Operation/m-p/1407767#M18184</link>
    <description>&lt;P&gt;Ok, I guess I may have figured this out myself.&amp;nbsp; From the reference manual section 27.5.15, FlexSPI always supports XIP regardless of flash device if placed in Advanced High Performance Bus (AHB) access mode.&amp;nbsp; In addition, u-boot subsequently copies itself into external RAM (0x80000000) area for better execution performance.&lt;/P&gt;</description>
    <pubDate>Tue, 01 Feb 2022 22:01:55 GMT</pubDate>
    <dc:creator>jautry</dc:creator>
    <dc:date>2022-02-01T22:01:55Z</dc:date>
    <item>
      <title>Understanding EVK Operation</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Understanding-EVK-Operation/m-p/1406869#M18166</link>
      <description>&lt;P&gt;I am trying to understand the ROM boot process.&amp;nbsp; I see the IVT table has start addresses in the flash 0x60000000 range.&amp;nbsp; I look at the boot data start and it also has address in flash 0x60000000 range.&amp;nbsp; I then look at the u-boot map file and all addresses are in the flash 0x60000000 range.&amp;nbsp; The XIP fuse setting is at 0.&amp;nbsp; I thought the flash code was supposed to be copied into OCRAM and executed from there but I see no addressing in the OCRAM area.&amp;nbsp; How is this operating?&amp;nbsp; What am I not understanding?&lt;/P&gt;</description>
      <pubDate>Sun, 30 Jan 2022 03:36:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Understanding-EVK-Operation/m-p/1406869#M18166</guid>
      <dc:creator>jautry</dc:creator>
      <dc:date>2022-01-30T03:36:39Z</dc:date>
    </item>
    <item>
      <title>Re: Understanding EVK Operation</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Understanding-EVK-Operation/m-p/1407767#M18184</link>
      <description>&lt;P&gt;Ok, I guess I may have figured this out myself.&amp;nbsp; From the reference manual section 27.5.15, FlexSPI always supports XIP regardless of flash device if placed in Advanced High Performance Bus (AHB) access mode.&amp;nbsp; In addition, u-boot subsequently copies itself into external RAM (0x80000000) area for better execution performance.&lt;/P&gt;</description>
      <pubDate>Tue, 01 Feb 2022 22:01:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Understanding-EVK-Operation/m-p/1407767#M18184</guid>
      <dc:creator>jautry</dc:creator>
      <dc:date>2022-02-01T22:01:55Z</dc:date>
    </item>
  </channel>
</rss>