<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic flexspi XIP mode write ability in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/flexspi-XIP-mode-write-ability/m-p/1400575#M18015</link>
    <description>&lt;P&gt;Hello world!&lt;/P&gt;&lt;P&gt;When booting fro psram in XIP mode it seems I can't write to separate regions of the psram chip. This is unfortunate because I was hoping to use the psram+flexspi as RWX ram like the SEMC or OCRAM, but it seems to be only RX. Is this an expected result or am I configuring something wrong. I am booting the IMXRT1060-evk from SD-card at the moment and copying the program binary to the psram.&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 18 Jan 2022 02:36:23 GMT</pubDate>
    <dc:creator>Mr-Bossman</dc:creator>
    <dc:date>2022-01-18T02:36:23Z</dc:date>
    <item>
      <title>flexspi XIP mode write ability</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/flexspi-XIP-mode-write-ability/m-p/1400575#M18015</link>
      <description>&lt;P&gt;Hello world!&lt;/P&gt;&lt;P&gt;When booting fro psram in XIP mode it seems I can't write to separate regions of the psram chip. This is unfortunate because I was hoping to use the psram+flexspi as RWX ram like the SEMC or OCRAM, but it seems to be only RX. Is this an expected result or am I configuring something wrong. I am booting the IMXRT1060-evk from SD-card at the moment and copying the program binary to the psram.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 18 Jan 2022 02:36:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/flexspi-XIP-mode-write-ability/m-p/1400575#M18015</guid>
      <dc:creator>Mr-Bossman</dc:creator>
      <dc:date>2022-01-18T02:36:23Z</dc:date>
    </item>
    <item>
      <title>Re: flexspi XIP mode write ability</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/flexspi-XIP-mode-write-ability/m-p/1400700#M18020</link>
      <description>&lt;P&gt;Hi，&lt;BR /&gt;Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.&lt;BR /&gt;1) Is this an expected result or am I configuring something wrong?&lt;BR /&gt;-- In my opinion, it's impossible to implement Read While Write(RWW) on PSRAM.&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Tue, 18 Jan 2022 06:23:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/flexspi-XIP-mode-write-ability/m-p/1400700#M18020</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2022-01-18T06:23:42Z</dc:date>
    </item>
  </channel>
</rss>