<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX RT Crossover MCUsのトピックRe: IMX RT1052 LVGL DISPLAY ROTATE QUESTION</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IMX-RT1052-LVGL-DISPLAY-ROTATE-QUESTION/m-p/1397648#M17948</link>
    <description>&lt;P&gt;Hello&lt;/P&gt;
&lt;P&gt;Hope you are well.&lt;BR /&gt;Does this issue persist when you set the screen resolution to 240x240? I believe that this issue is caused because the resolution also changes or some parameters from the screen are modified.&lt;BR /&gt;For the rotation I suggest you use the PXP module, you can find an example in the SDK so you can integrate it into your application.&lt;BR /&gt;&lt;BR /&gt;If you have more questions do not hesitate to ask me.&lt;BR /&gt;Best regards,&lt;BR /&gt;Omar&lt;/P&gt;</description>
    <pubDate>Wed, 12 Jan 2022 00:27:08 GMT</pubDate>
    <dc:creator>Omar_Anguiano</dc:creator>
    <dc:date>2022-01-12T00:27:08Z</dc:date>
    <item>
      <title>IMX RT1052 LVGL DISPLAY ROTATE QUESTION</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IMX-RT1052-LVGL-DISPLAY-ROTATE-QUESTION/m-p/1395631#M17898</link>
      <description>&lt;P&gt;Platform : imxRT1052&amp;nbsp;&lt;/P&gt;&lt;P&gt;lcd : 320(hor_res) * 240(ver_res)&lt;/P&gt;&lt;P&gt;the a&lt;SPAN&gt;pplication need change to 240(hor_res) * 320(ver_res) display&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;PROGRESS:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; 1.use SDK_2_10_0_MIMXRT1052xxxxB create my own project with lvgl and&amp;nbsp; freertos&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;2.change LCDIF parameter&amp;nbsp;to my lcd module。&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;3.I need rotate 90 degree in my application . i notice LVGL v7.10.1 do not support software rotation support.So i upgrade lvgl version to V7.11.0. From this version LVGL support&amp;nbsp;software rotation support.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; 4.when I&amp;nbsp;rotate 90 or 270 degree,LCD do not work well.but when I&amp;nbsp;rotate 0 or180 degree,LCD work fine.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp;does anyone know why??&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp;PIC as&amp;nbsp;below：&lt;BR /&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; A. do not rotate&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="ruihuan_0-1641474764237.jpeg" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/166894iF76A184390DEE060/image-size/medium?v=v2&amp;amp;px=400" role="button" title="ruihuan_0-1641474764237.jpeg" alt="ruihuan_0-1641474764237.jpeg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; B.&amp;nbsp;rotate 270 degree&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="ruihuan_2-1641474785406.jpeg" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/166897i4AF97EDBF5D2CE53/image-size/medium?v=v2&amp;amp;px=400" role="button" title="ruihuan_2-1641474785406.jpeg" alt="ruihuan_2-1641474785406.jpeg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; C.rotate 180 degree&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="ruihuan_1-1641474775546.jpeg" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/166895iF6CA00310AC0EB70/image-size/medium?v=v2&amp;amp;px=400" role="button" title="ruihuan_1-1641474775546.jpeg" alt="ruihuan_1-1641474775546.jpeg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 06 Jan 2022 13:13:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IMX-RT1052-LVGL-DISPLAY-ROTATE-QUESTION/m-p/1395631#M17898</guid>
      <dc:creator>ruihuan</dc:creator>
      <dc:date>2022-01-06T13:13:45Z</dc:date>
    </item>
    <item>
      <title>Re: IMX RT1052 LVGL DISPLAY ROTATE QUESTION</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IMX-RT1052-LVGL-DISPLAY-ROTATE-QUESTION/m-p/1397648#M17948</link>
      <description>&lt;P&gt;Hello&lt;/P&gt;
&lt;P&gt;Hope you are well.&lt;BR /&gt;Does this issue persist when you set the screen resolution to 240x240? I believe that this issue is caused because the resolution also changes or some parameters from the screen are modified.&lt;BR /&gt;For the rotation I suggest you use the PXP module, you can find an example in the SDK so you can integrate it into your application.&lt;BR /&gt;&lt;BR /&gt;If you have more questions do not hesitate to ask me.&lt;BR /&gt;Best regards,&lt;BR /&gt;Omar&lt;/P&gt;</description>
      <pubDate>Wed, 12 Jan 2022 00:27:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IMX-RT1052-LVGL-DISPLAY-ROTATE-QUESTION/m-p/1397648#M17948</guid>
      <dc:creator>Omar_Anguiano</dc:creator>
      <dc:date>2022-01-12T00:27:08Z</dc:date>
    </item>
  </channel>
</rss>