<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic MAX17260 Battery Connection or Removal Status in IMXRT 1050 controller in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/MAX17260-Battery-Connection-or-Removal-Status-in-IMXRT-1050/m-p/1389858#M17661</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am using IMXRT 1050 micro controller and MAX 17260 chip for battery capacity reading.&lt;/P&gt;&lt;P&gt;Now i want to check whether battery is connected or removed.&lt;/P&gt;&lt;P&gt;As per the datasheet i am reading the register "CONFIG REGISTER" it is always coming value as 0x2210&lt;/P&gt;&lt;P&gt;In CONFIG Register(0x1D),&lt;/P&gt;&lt;P&gt;Bit positions:&lt;/P&gt;&lt;P&gt;0th bit&amp;nbsp; D0 - Ber &amp;nbsp;&amp;nbsp;&amp;nbsp; (battery Removal)&lt;/P&gt;&lt;P&gt;1st bit&amp;nbsp; D1 - Bei &amp;nbsp;&amp;nbsp;&amp;nbsp; (battery Insertion)&lt;/P&gt;&lt;P&gt;Can anyone please guide me how to get the connection or removal status of MAX 17260 battery.&lt;/P&gt;</description>
    <pubDate>Tue, 21 Dec 2021 06:28:17 GMT</pubDate>
    <dc:creator>yvkrkrishna</dc:creator>
    <dc:date>2021-12-21T06:28:17Z</dc:date>
    <item>
      <title>MAX17260 Battery Connection or Removal Status in IMXRT 1050 controller</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/MAX17260-Battery-Connection-or-Removal-Status-in-IMXRT-1050/m-p/1389858#M17661</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am using IMXRT 1050 micro controller and MAX 17260 chip for battery capacity reading.&lt;/P&gt;&lt;P&gt;Now i want to check whether battery is connected or removed.&lt;/P&gt;&lt;P&gt;As per the datasheet i am reading the register "CONFIG REGISTER" it is always coming value as 0x2210&lt;/P&gt;&lt;P&gt;In CONFIG Register(0x1D),&lt;/P&gt;&lt;P&gt;Bit positions:&lt;/P&gt;&lt;P&gt;0th bit&amp;nbsp; D0 - Ber &amp;nbsp;&amp;nbsp;&amp;nbsp; (battery Removal)&lt;/P&gt;&lt;P&gt;1st bit&amp;nbsp; D1 - Bei &amp;nbsp;&amp;nbsp;&amp;nbsp; (battery Insertion)&lt;/P&gt;&lt;P&gt;Can anyone please guide me how to get the connection or removal status of MAX 17260 battery.&lt;/P&gt;</description>
      <pubDate>Tue, 21 Dec 2021 06:28:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/MAX17260-Battery-Connection-or-Removal-Status-in-IMXRT-1050/m-p/1389858#M17661</guid>
      <dc:creator>yvkrkrishna</dc:creator>
      <dc:date>2021-12-21T06:28:17Z</dc:date>
    </item>
    <item>
      <title>Re: MAX17260 Battery Connection or Removal Status in IMXRT 1050 controller</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/MAX17260-Battery-Connection-or-Removal-Status-in-IMXRT-1050/m-p/1390488#M17674</link>
      <description>&lt;P&gt;Hi,&lt;BR /&gt;Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.&lt;BR /&gt;I think you'd better contact Maxim integrated apply for some advice or suggestions, as I'm not familiar with their products.&lt;/P&gt;
&lt;P&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Wed, 22 Dec 2021 05:22:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/MAX17260-Battery-Connection-or-Removal-Status-in-IMXRT-1050/m-p/1390488#M17674</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2021-12-22T05:22:03Z</dc:date>
    </item>
  </channel>
</rss>