<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic MIMXRT1176 LPADC voltage  reference scaling in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/MIMXRT1176-LPADC-voltage-reference-scaling/m-p/1386125#M17537</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I'm considering the RT1176 MCU for our next product (ethernet attached data acquisition)&lt;/P&gt;&lt;P&gt;Could you please help with the following:&lt;/P&gt;&lt;P&gt;The documentation is not very clear about the LPADC voltage reference scaling feature. Is there any additional documentation, maybe an application note with complete feature description of LPADC?&amp;nbsp;&lt;/P&gt;&lt;P&gt;I need to digitize multiple external analog signals, and it will be really useful to have an&amp;nbsp;individual reference&amp;nbsp;voltage setting for each&amp;nbsp;analog input.&amp;nbsp;&lt;/P&gt;&lt;P&gt;In the current documentation I see that CSW&amp;nbsp; (channel scale width) shows that scaling could be not supported on a particular device, or scale control&amp;nbsp;field could be 1 or 6 bits in size.&lt;/P&gt;&lt;P&gt;Could you please help to find more info about that feature? How can I find what&amp;nbsp;devices support 6 bit scale?&lt;/P&gt;&lt;P&gt;Thanks for the help!&lt;/P&gt;</description>
    <pubDate>Tue, 14 Dec 2021 06:53:11 GMT</pubDate>
    <dc:creator>sergeydanilov</dc:creator>
    <dc:date>2021-12-14T06:53:11Z</dc:date>
    <item>
      <title>MIMXRT1176 LPADC voltage  reference scaling</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/MIMXRT1176-LPADC-voltage-reference-scaling/m-p/1386125#M17537</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I'm considering the RT1176 MCU for our next product (ethernet attached data acquisition)&lt;/P&gt;&lt;P&gt;Could you please help with the following:&lt;/P&gt;&lt;P&gt;The documentation is not very clear about the LPADC voltage reference scaling feature. Is there any additional documentation, maybe an application note with complete feature description of LPADC?&amp;nbsp;&lt;/P&gt;&lt;P&gt;I need to digitize multiple external analog signals, and it will be really useful to have an&amp;nbsp;individual reference&amp;nbsp;voltage setting for each&amp;nbsp;analog input.&amp;nbsp;&lt;/P&gt;&lt;P&gt;In the current documentation I see that CSW&amp;nbsp; (channel scale width) shows that scaling could be not supported on a particular device, or scale control&amp;nbsp;field could be 1 or 6 bits in size.&lt;/P&gt;&lt;P&gt;Could you please help to find more info about that feature? How can I find what&amp;nbsp;devices support 6 bit scale?&lt;/P&gt;&lt;P&gt;Thanks for the help!&lt;/P&gt;</description>
      <pubDate>Tue, 14 Dec 2021 06:53:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/MIMXRT1176-LPADC-voltage-reference-scaling/m-p/1386125#M17537</guid>
      <dc:creator>sergeydanilov</dc:creator>
      <dc:date>2021-12-14T06:53:11Z</dc:date>
    </item>
    <item>
      <title>Re: MIMXRT1176 LPADC voltage  reference scaling</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/MIMXRT1176-LPADC-voltage-reference-scaling/m-p/1387185#M17582</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/55802"&gt;@sergeydanilov&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp; Thanks for your interest in the NXP MIMXRT product, I would like to provide service for you.&lt;/P&gt;
&lt;P&gt;About the RT1170 reference voltage for ADC, please check the following information:&lt;/P&gt;
&lt;P&gt;ADC on RT1170 Supports only 1.0-1.8V reference (no support for 3V reference)&lt;/P&gt;
&lt;P&gt;NEVERTHELESS ADC inputs can accept higher input voltages utilizing channel scale factor of 30/64. For example: if 3.3V input voltage required then scale factor must be enabled ADC reference must be set to 1.54V (only supported on VREFH).&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;As my understand, it is just support 1bit scale now, use the CSCALE choose. 6bit still not support.&lt;/P&gt;
&lt;P&gt;You can see, it is just one bit:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="kerryzhou_0-1639559798765.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/165291iC602F8C5E97835D0/image-size/medium?v=v2&amp;amp;px=400" role="button" title="kerryzhou_0-1639559798765.png" alt="kerryzhou_0-1639559798765.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;If you still have question about it, please kindly let me know.&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Kerry&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 15 Dec 2021 09:17:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/MIMXRT1176-LPADC-voltage-reference-scaling/m-p/1387185#M17582</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2021-12-15T09:17:09Z</dc:date>
    </item>
    <item>
      <title>Re: MIMXRT1176 LPADC voltage  reference scaling</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/MIMXRT1176-LPADC-voltage-reference-scaling/m-p/1392300#M17740</link>
      <description>&lt;P&gt;Thanks for an answer!&lt;/P&gt;&lt;P&gt;Mai I ask if there any way to find out what&amp;nbsp; MCUs support variable (6bit) CSCALE ?&lt;/P&gt;</description>
      <pubDate>Mon, 27 Dec 2021 14:43:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/MIMXRT1176-LPADC-voltage-reference-scaling/m-p/1392300#M17740</guid>
      <dc:creator>sergeydanilov</dc:creator>
      <dc:date>2021-12-27T14:43:12Z</dc:date>
    </item>
    <item>
      <title>Re: MIMXRT1176 LPADC voltage  reference scaling</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/MIMXRT1176-LPADC-voltage-reference-scaling/m-p/1392385#M17747</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/55802"&gt;@sergeydanilov&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp; Until now, I still didn't find other RT chip support 6bit scale, I think it is used for the future new IP consideration, but still no released product until now.&lt;/P&gt;
&lt;P&gt;&amp;nbsp; Wish it helps you!&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Kerry&lt;/P&gt;</description>
      <pubDate>Tue, 28 Dec 2021 02:46:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/MIMXRT1176-LPADC-voltage-reference-scaling/m-p/1392385#M17747</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2021-12-28T02:46:43Z</dc:date>
    </item>
  </channel>
</rss>