<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: RT1050evbk UART example? in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1050evbk-UART-example/m-p/1377226#M17289</link>
    <description>&lt;P&gt;Hi Anthony,&lt;/P&gt;
&lt;P&gt;You read correctly, the examples ask you to connect the board to USB because the UART pins that are configured are connected to the on-board debugger (LPC4322) that works as a USB-UART bridge so you do not need to use external FTDI.&lt;/P&gt;
&lt;P&gt;If you like to use different pins you will need to change the pins used in the example.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Felipe&lt;/P&gt;</description>
    <pubDate>Thu, 25 Nov 2021 19:21:27 GMT</pubDate>
    <dc:creator>FelipeGarcia</dc:creator>
    <dc:date>2021-11-25T19:21:27Z</dc:date>
    <item>
      <title>RT1050evbk UART example?</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1050evbk-UART-example/m-p/1375133#M17244</link>
      <description>&lt;P&gt;Okay I have gotten the RT1050evbk to program and run.&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;I downloaded two of the uart examples.&lt;BR /&gt;&lt;BR /&gt;The flexio one and the Freertos example.&amp;nbsp;&lt;BR /&gt;I hooked up J22 pins 1,2 as rx tx, and then j24 pin 7 as ground to an ftdi cable with the port open at 115200. Ran the examples and nothing. Notta.&lt;BR /&gt;&lt;BR /&gt;So I reread the instructions and whoever wrote them was not overly clear, but it seems like they want me to connect the board to USB? Like a built in FTDI? Not exactly what I was wanting as this is just a UART.&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;Any help would be appreciated. If I am reading it wrong tell me where the proper documentation is. I would like the FreeRTOS example if one could work. I would like to use the pins I mentioned as a UART&lt;/P&gt;</description>
      <pubDate>Mon, 22 Nov 2021 16:27:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1050evbk-UART-example/m-p/1375133#M17244</guid>
      <dc:creator>anthonygarza</dc:creator>
      <dc:date>2021-11-22T16:27:33Z</dc:date>
    </item>
    <item>
      <title>Re: RT1050evbk UART example?</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1050evbk-UART-example/m-p/1377226#M17289</link>
      <description>&lt;P&gt;Hi Anthony,&lt;/P&gt;
&lt;P&gt;You read correctly, the examples ask you to connect the board to USB because the UART pins that are configured are connected to the on-board debugger (LPC4322) that works as a USB-UART bridge so you do not need to use external FTDI.&lt;/P&gt;
&lt;P&gt;If you like to use different pins you will need to change the pins used in the example.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Felipe&lt;/P&gt;</description>
      <pubDate>Thu, 25 Nov 2021 19:21:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1050evbk-UART-example/m-p/1377226#M17289</guid>
      <dc:creator>FelipeGarcia</dc:creator>
      <dc:date>2021-11-25T19:21:27Z</dc:date>
    </item>
  </channel>
</rss>