<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic ADC reference not connected in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/ADC-reference-not-connected/m-p/1375053#M17241</link>
    <description>&lt;P&gt;Hello, fellows engineers.&lt;/P&gt;&lt;P&gt;On an RT1051-based board, I forgot to connect the ADC reference (pin N14, VDDA_ADC).&lt;/P&gt;&lt;P&gt;The strange fact is that the ADC seems to work more or less correctly, as if there were an internal connection to VCC.&lt;/P&gt;&lt;P&gt;Do you have any idea about this? Is there any settings that allows the ADC to work even if there is no external reference?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;G.&lt;/P&gt;</description>
    <pubDate>Mon, 22 Nov 2021 13:37:16 GMT</pubDate>
    <dc:creator>giuseppescarpi</dc:creator>
    <dc:date>2021-11-22T13:37:16Z</dc:date>
    <item>
      <title>ADC reference not connected</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/ADC-reference-not-connected/m-p/1375053#M17241</link>
      <description>&lt;P&gt;Hello, fellows engineers.&lt;/P&gt;&lt;P&gt;On an RT1051-based board, I forgot to connect the ADC reference (pin N14, VDDA_ADC).&lt;/P&gt;&lt;P&gt;The strange fact is that the ADC seems to work more or less correctly, as if there were an internal connection to VCC.&lt;/P&gt;&lt;P&gt;Do you have any idea about this? Is there any settings that allows the ADC to work even if there is no external reference?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;G.&lt;/P&gt;</description>
      <pubDate>Mon, 22 Nov 2021 13:37:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/ADC-reference-not-connected/m-p/1375053#M17241</guid>
      <dc:creator>giuseppescarpi</dc:creator>
      <dc:date>2021-11-22T13:37:16Z</dc:date>
    </item>
    <item>
      <title>Re: ADC reference not connected</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/ADC-reference-not-connected/m-p/1375279#M17247</link>
      <description>&lt;P&gt;Hi,&lt;BR /&gt;Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.&lt;BR /&gt;The VDDA_ADC_3P3 must be powered.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="jeremyzhou_0-1637633017063.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/162888iE8AB3063D5B18A46/image-size/medium?v=v2&amp;amp;px=400" role="button" title="jeremyzhou_0-1637633017063.png" alt="jeremyzhou_0-1637633017063.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;jeremyzhou_0-1637633017063.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Hope this is clear.&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Tue, 23 Nov 2021 02:03:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/ADC-reference-not-connected/m-p/1375279#M17247</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2021-11-23T02:03:51Z</dc:date>
    </item>
    <item>
      <title>Re: ADC reference not connected</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/ADC-reference-not-connected/m-p/1376145#M17264</link>
      <description>&lt;P&gt;Hi TIC,&lt;/P&gt;&lt;P&gt;Thank you for your reply, the datasheet is very clear.&lt;/P&gt;&lt;P&gt;Nonetheless, on this board with VDDA_ADC disconnected we see that the peripheral works as expected, it is only not very precise (the measurement is repeatable, but scaled down). I suspect that the peripheral gets back-supplied.&lt;/P&gt;&lt;P&gt;We may even think to connect another ADC pin as a sort of "external reference"... I reckon this sounds horrible from an engineering point of view, but I would like to have a better understanding.&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Giuseppe&lt;/P&gt;</description>
      <pubDate>Wed, 24 Nov 2021 09:11:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/ADC-reference-not-connected/m-p/1376145#M17264</guid>
      <dc:creator>giuseppescarpi</dc:creator>
      <dc:date>2021-11-24T09:11:57Z</dc:date>
    </item>
  </channel>
</rss>