<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Octo SPI in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Octo-SPI/m-p/1368359#M17055</link>
    <description>&lt;P&gt;I look at the diagram. (IMXRT1160RM.pdf)&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="qspi.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/161635i134802F85BEF0D3A/image-size/medium?v=v2&amp;amp;px=400" role="button" title="qspi.png" alt="qspi.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;This is a master side. As I understand read/write direction is set with&amp;nbsp;A_DQS pin on a slave side.&lt;/P&gt;&lt;P&gt;I have to implement a slave side on FPGA. When I should set the data bus in High-Z state on a slave side? And the master side - when the data bus is input? A_DQS&amp;nbsp; = 1?&lt;/P&gt;&lt;P&gt;Is there any example of the master? I found only Quad SPI examples.&lt;/P&gt;</description>
    <pubDate>Tue, 09 Nov 2021 08:31:23 GMT</pubDate>
    <dc:creator>john71</dc:creator>
    <dc:date>2021-11-09T08:31:23Z</dc:date>
    <item>
      <title>Octo SPI</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Octo-SPI/m-p/1368359#M17055</link>
      <description>&lt;P&gt;I look at the diagram. (IMXRT1160RM.pdf)&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="qspi.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/161635i134802F85BEF0D3A/image-size/medium?v=v2&amp;amp;px=400" role="button" title="qspi.png" alt="qspi.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;This is a master side. As I understand read/write direction is set with&amp;nbsp;A_DQS pin on a slave side.&lt;/P&gt;&lt;P&gt;I have to implement a slave side on FPGA. When I should set the data bus in High-Z state on a slave side? And the master side - when the data bus is input? A_DQS&amp;nbsp; = 1?&lt;/P&gt;&lt;P&gt;Is there any example of the master? I found only Quad SPI examples.&lt;/P&gt;</description>
      <pubDate>Tue, 09 Nov 2021 08:31:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Octo-SPI/m-p/1368359#M17055</guid>
      <dc:creator>john71</dc:creator>
      <dc:date>2021-11-09T08:31:23Z</dc:date>
    </item>
    <item>
      <title>Re: Octo SPI</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Octo-SPI/m-p/1368875#M17076</link>
      <description>&lt;P&gt;Hi,&lt;BR /&gt;Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.&lt;BR /&gt;Firstly, to provide the fastest possible support, I'd highly recommend you to refer to the &lt;A href="https://www.cnblogs.com/henjay724/p/14438002.html" target="_self"&gt;post&lt;/A&gt; to learn the DQS Signal, next, please refer to the FlexSPI demos to learn how to contact the slave device.&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Wed, 10 Nov 2021 02:47:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Octo-SPI/m-p/1368875#M17076</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2021-11-10T02:47:46Z</dc:date>
    </item>
    <item>
      <title>Re: Octo SPI</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Octo-SPI/m-p/1369026#M17082</link>
      <description>&lt;P&gt;Thanks a lot for the link. As soon as I will learn chines I'll use it.&lt;/P&gt;&lt;P&gt;Meanwhile as I try to implement&lt;STRONG&gt; a slave side &lt;/STRONG&gt;I need to understand - how can I control a master read cycle as a slave.&lt;/P&gt;&lt;P&gt;Regards.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 10 Nov 2021 07:18:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Octo-SPI/m-p/1369026#M17082</guid>
      <dc:creator>john71</dc:creator>
      <dc:date>2021-11-10T07:18:59Z</dc:date>
    </item>
  </channel>
</rss>