<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX RT Crossover MCUsのトピックRe: About UB/LB Signals behavior when SEMC is used as SRAM-I/F</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/About-UB-LB-Signals-behavior-when-SEMC-is-used-as-SRAM-I-F/m-p/1360394#M16836</link>
    <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/167536"&gt;@FelipeGarcia&lt;/a&gt;,&lt;/P&gt;&lt;P&gt;Thank you for your sincere response.&lt;/P&gt;&lt;P&gt;I will continue to wait for your reply.&lt;/P&gt;&lt;P&gt;BR,&lt;BR /&gt;George&lt;/P&gt;</description>
    <pubDate>Sun, 24 Oct 2021 15:33:51 GMT</pubDate>
    <dc:creator>george</dc:creator>
    <dc:date>2021-10-24T15:33:51Z</dc:date>
    <item>
      <title>About UB/LB Signals behavior when SEMC is used as SRAM-I/F</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/About-UB-LB-Signals-behavior-when-SEMC-is-used-as-SRAM-I-F/m-p/1340745#M16339</link>
      <description>&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;We are going to use SEMC as SRAM-I/F(ASYNC non-ADMUX w/ WAIT) to connect to FPGA.&lt;/P&gt;&lt;P&gt;Please tell me the behavior of the &lt;STRONG&gt;UB&lt;/STRONG&gt;/&lt;STRONG&gt;LB&lt;/STRONG&gt; signals.&lt;BR /&gt;Can you provide me with a timing diagram showing those behaviors?&lt;/P&gt;&lt;P&gt;BR,&lt;BR /&gt;George&lt;/P&gt;</description>
      <pubDate>Wed, 15 Sep 2021 16:05:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/About-UB-LB-Signals-behavior-when-SEMC-is-used-as-SRAM-I-F/m-p/1340745#M16339</guid>
      <dc:creator>george</dc:creator>
      <dc:date>2021-09-15T16:05:10Z</dc:date>
    </item>
    <item>
      <title>Re: About UB/LB Signals behavior when SEMC is used as SRAM-I/F</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/About-UB-LB-Signals-behavior-when-SEMC-is-used-as-SRAM-I-F/m-p/1342421#M16389</link>
      <description>&lt;P&gt;Hi George,&lt;/P&gt;
&lt;P&gt;These signals are Upper and Lower Byte select pins. SRAM will read or write upper or lower data byte depending on this signals. We do not have timing diagrams including these pins but you can find more information of this in your specific memory datasheet.&lt;/P&gt;
&lt;P&gt;Have a great day,&lt;/P&gt;
&lt;P&gt;Felipe&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;/P&gt;
&lt;P&gt;Note:&lt;/P&gt;
&lt;P&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored. Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;------------------------------------------------------------------------------&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 17 Sep 2021 18:59:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/About-UB-LB-Signals-behavior-when-SEMC-is-used-as-SRAM-I-F/m-p/1342421#M16389</guid>
      <dc:creator>FelipeGarcia</dc:creator>
      <dc:date>2021-09-17T18:59:32Z</dc:date>
    </item>
    <item>
      <title>Re: About UB/LB Signals behavior when SEMC is used as SRAM-I/F</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/About-UB-LB-Signals-behavior-when-SEMC-is-used-as-SRAM-I-F/m-p/1345682#M16453</link>
      <description>&lt;P&gt;Dear &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/167536"&gt;@FelipeGarcia&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The device that connects to the RT1175 is an FPGA.&lt;BR /&gt;We have to configure the FPGA according to the RT1175 I/F specifications.&lt;BR /&gt;Therefore, we need to know the cycle-based signal transition.&lt;/P&gt;&lt;P&gt;Other signal timings seem to be variable by the registers, but it remains unclear where the signal transitions occur for UB and LB.&lt;/P&gt;&lt;P&gt;For example, in the following mode :&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="PRI_20210924-162706.bmp" style="width: 636px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/157237i10C360D147E77548/image-size/large?v=v2&amp;amp;px=999" role="button" title="PRI_20210924-162706.bmp" alt="PRI_20210924-162706.bmp" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;At what timing in this figure the UB and LB signals transition?&lt;/P&gt;&lt;P&gt;And where is it when read ?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="PRI_20210924-165459.bmp" style="width: 639px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/157243iCAFDC2CA5995214C/image-size/large?v=v2&amp;amp;px=999" role="button" title="PRI_20210924-165459.bmp" alt="PRI_20210924-165459.bmp" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;BR,&lt;BR /&gt;George.&lt;/P&gt;</description>
      <pubDate>Fri, 24 Sep 2021 10:47:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/About-UB-LB-Signals-behavior-when-SEMC-is-used-as-SRAM-I-F/m-p/1345682#M16453</guid>
      <dc:creator>george</dc:creator>
      <dc:date>2021-09-24T10:47:28Z</dc:date>
    </item>
    <item>
      <title>Re: About UB/LB Signals behavior when SEMC is used as SRAM-I/F</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/About-UB-LB-Signals-behavior-when-SEMC-is-used-as-SRAM-I-F/m-p/1349357#M16544</link>
      <description>&lt;P&gt;Hi George,&lt;/P&gt;
&lt;P&gt;Unfortunately, we do not have timing diagrams including these signals. However, just for reference you can check SRAM datasheets for example: &lt;A href="https://www.issi.com/WW/pdf/65WV25616ALL_BLL.pdf" target="_blank"&gt;https://www.issi.com/WW/pdf/65WV25616ALL_BLL.pdf&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;There you will find more info about timing and behavior of these signals.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Felipe&lt;/P&gt;</description>
      <pubDate>Thu, 30 Sep 2021 23:14:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/About-UB-LB-Signals-behavior-when-SEMC-is-used-as-SRAM-I-F/m-p/1349357#M16544</guid>
      <dc:creator>FelipeGarcia</dc:creator>
      <dc:date>2021-09-30T23:14:22Z</dc:date>
    </item>
    <item>
      <title>Re: About UB/LB Signals behavior when SEMC is used as SRAM-I/F</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/About-UB-LB-Signals-behavior-when-SEMC-is-used-as-SRAM-I-F/m-p/1349890#M16562</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/167536"&gt;@FelipeGarcia&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The documentation you presented to me allowed me to understand the behavior of UB/LB.&lt;/P&gt;&lt;P&gt;I think you can guarantee that UB / LB is valid during &lt;STRONG&gt;&lt;FONT color="#339966"&gt;green&lt;/FONT&gt;&lt;/STRONG&gt; period I added in &lt;STRONG&gt;&lt;FONT color="#FF0000"&gt;red&lt;/FONT&gt;&lt;/STRONG&gt;.&lt;BR /&gt;Is my understanding correct?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="aw.png" style="width: 636px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/158154iEC6599038F86DA2C/image-size/large?v=v2&amp;amp;px=999" role="button" title="aw.png" alt="aw.png" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="ar.png" style="width: 639px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/158155iBD0B2863CD91BE06/image-size/large?v=v2&amp;amp;px=999" role="button" title="ar.png" alt="ar.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;BR,&lt;BR /&gt;George&lt;/P&gt;</description>
      <pubDate>Mon, 04 Oct 2021 06:54:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/About-UB-LB-Signals-behavior-when-SEMC-is-used-as-SRAM-I-F/m-p/1349890#M16562</guid>
      <dc:creator>george</dc:creator>
      <dc:date>2021-10-04T06:54:00Z</dc:date>
    </item>
    <item>
      <title>Re: About UB/LB Signals behavior when SEMC is used as SRAM-I/F</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/About-UB-LB-Signals-behavior-when-SEMC-is-used-as-SRAM-I-F/m-p/1352058#M16602</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/39147"&gt;@george&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Could you please provide what was the thinking behind this timing diagrams? Please be as detailed as possible.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Felipe&lt;/P&gt;</description>
      <pubDate>Thu, 07 Oct 2021 16:20:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/About-UB-LB-Signals-behavior-when-SEMC-is-used-as-SRAM-I-F/m-p/1352058#M16602</guid>
      <dc:creator>FelipeGarcia</dc:creator>
      <dc:date>2021-10-07T16:20:09Z</dc:date>
    </item>
    <item>
      <title>Re: About UB/LB Signals behavior when SEMC is used as SRAM-I/F</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/About-UB-LB-Signals-behavior-when-SEMC-is-used-as-SRAM-I-F/m-p/1353846#M16666</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/167536"&gt;@FelipeGarcia&lt;/a&gt;,&lt;/P&gt;&lt;P&gt;Sorry for the late reply.&lt;/P&gt;&lt;P&gt;The UB/LB I added may have been too extreme.&lt;BR /&gt;It may be necessary to extend the valid fields backward by one semc_clk.&lt;/P&gt;&lt;P&gt;My thoughts are as follows.&lt;/P&gt;&lt;P&gt;First, Write timing:&lt;BR /&gt;SRAM needs to capture UB/LB-gated DATA at WE# rising edge.&lt;BR /&gt;I think UB/LB needs setup and hold at WE# rising edge.&lt;/P&gt;&lt;P&gt;Second, Read timing:&lt;BR /&gt;SRAM needs to control the DATA output with UB/LB and OE, which requires setup and hold for the internal rxclkn rising edge.&lt;/P&gt;&lt;P&gt;Please tell me the valid period for which you can guarantee.&lt;/P&gt;&lt;P&gt;BR,&lt;/P&gt;&lt;P&gt;George&lt;/P&gt;</description>
      <pubDate>Tue, 12 Oct 2021 03:28:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/About-UB-LB-Signals-behavior-when-SEMC-is-used-as-SRAM-I-F/m-p/1353846#M16666</guid>
      <dc:creator>george</dc:creator>
      <dc:date>2021-10-12T03:28:49Z</dc:date>
    </item>
    <item>
      <title>Re: About UB/LB Signals behavior when SEMC is used as SRAM-I/F</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/About-UB-LB-Signals-behavior-when-SEMC-is-used-as-SRAM-I-F/m-p/1355958#M16723</link>
      <description>&lt;P&gt;Hi George,&lt;/P&gt;
&lt;P&gt;I will check internally if we have any information about this.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Felipe&lt;/P&gt;</description>
      <pubDate>Thu, 14 Oct 2021 16:00:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/About-UB-LB-Signals-behavior-when-SEMC-is-used-as-SRAM-I-F/m-p/1355958#M16723</guid>
      <dc:creator>FelipeGarcia</dc:creator>
      <dc:date>2021-10-14T16:00:50Z</dc:date>
    </item>
    <item>
      <title>Re: About UB/LB Signals behavior when SEMC is used as SRAM-I/F</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/About-UB-LB-Signals-behavior-when-SEMC-is-used-as-SRAM-I-F/m-p/1360236#M16829</link>
      <description>&lt;P&gt;Hi George,&lt;/P&gt;
&lt;P&gt;To give you an update. We are still trying to get further information from IP owner. Once I get more information I will post it here.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Felipe&lt;/P&gt;</description>
      <pubDate>Fri, 22 Oct 2021 18:19:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/About-UB-LB-Signals-behavior-when-SEMC-is-used-as-SRAM-I-F/m-p/1360236#M16829</guid>
      <dc:creator>FelipeGarcia</dc:creator>
      <dc:date>2021-10-22T18:19:28Z</dc:date>
    </item>
    <item>
      <title>Re: About UB/LB Signals behavior when SEMC is used as SRAM-I/F</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/About-UB-LB-Signals-behavior-when-SEMC-is-used-as-SRAM-I-F/m-p/1360394#M16836</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/167536"&gt;@FelipeGarcia&lt;/a&gt;,&lt;/P&gt;&lt;P&gt;Thank you for your sincere response.&lt;/P&gt;&lt;P&gt;I will continue to wait for your reply.&lt;/P&gt;&lt;P&gt;BR,&lt;BR /&gt;George&lt;/P&gt;</description>
      <pubDate>Sun, 24 Oct 2021 15:33:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/About-UB-LB-Signals-behavior-when-SEMC-is-used-as-SRAM-I-F/m-p/1360394#M16836</guid>
      <dc:creator>george</dc:creator>
      <dc:date>2021-10-24T15:33:51Z</dc:date>
    </item>
    <item>
      <title>Re: About UB/LB Signals behavior when SEMC is used as SRAM-I/F</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/About-UB-LB-Signals-behavior-when-SEMC-is-used-as-SRAM-I-F/m-p/1361075#M16855</link>
      <description>&lt;P&gt;Hi George,&lt;/P&gt;
&lt;P&gt;I received an update, you can take as reference see the LB#/UB# signals in ASYNC SRAM write in Non-ADMUX address mode.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-center" image-alt="FelipeGarcia_1-1635204627286.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/160063i91310679CFBA9C38/image-size/large?v=v2&amp;amp;px=999" role="button" title="FelipeGarcia_1-1635204627286.png" alt="FelipeGarcia_1-1635204627286.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Felipe&lt;/P&gt;</description>
      <pubDate>Mon, 25 Oct 2021 23:30:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/About-UB-LB-Signals-behavior-when-SEMC-is-used-as-SRAM-I-F/m-p/1361075#M16855</guid>
      <dc:creator>FelipeGarcia</dc:creator>
      <dc:date>2021-10-25T23:30:47Z</dc:date>
    </item>
    <item>
      <title>Re: About UB/LB Signals behavior when SEMC is used as SRAM-I/F</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/About-UB-LB-Signals-behavior-when-SEMC-is-used-as-SRAM-I-F/m-p/1364365#M16948</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/167536"&gt;@FelipeGarcia&lt;/a&gt;,&lt;/P&gt;&lt;P&gt;Sorry for the late reply.&lt;/P&gt;&lt;P&gt;Thank you for the update.&lt;/P&gt;&lt;P&gt;In other words, we understand that &lt;STRONG&gt;UB#&lt;/STRONG&gt;/&lt;STRONG&gt;LB#&lt;/STRONG&gt; is &lt;STRONG&gt;Low-Active between AS and WEH&lt;/STRONG&gt; in the internal state.&lt;/P&gt;&lt;P&gt;Thanks,&lt;BR /&gt;George&lt;/P&gt;</description>
      <pubDate>Mon, 01 Nov 2021 07:00:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/About-UB-LB-Signals-behavior-when-SEMC-is-used-as-SRAM-I-F/m-p/1364365#M16948</guid>
      <dc:creator>george</dc:creator>
      <dc:date>2021-11-01T07:00:09Z</dc:date>
    </item>
  </channel>
</rss>