<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: IMXRT1024 LPUART EDMA Multi Channel Usage and tcdMemoryPoolPtr in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IMXRT1024-LPUART-EDMA-Multi-Channel-Usage-and-tcdMemoryPoolPtr/m-p/1353037#M16640</link>
    <description>&lt;P&gt;Hi,&lt;BR /&gt;Thanks for your reply.&lt;BR /&gt;1) Could you please help me about the implementation? Do you have any directive or example code for multiple LPUART with EDMA?&lt;BR /&gt;-- In the lpuart_edma_rb_transfer demo, it uses the LUART1 for example, if you want to use the multiple LPUART, for instance, the LPUART2, LPUART3, etc, it's easy to do that via copy the original demo code, then adjust the code a bit.&lt;BR /&gt;Have a great day.&lt;BR /&gt;TIC&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
    <pubDate>Sat, 09 Oct 2021 07:37:59 GMT</pubDate>
    <dc:creator>jeremyzhou</dc:creator>
    <dc:date>2021-10-09T07:37:59Z</dc:date>
    <item>
      <title>IMXRT1024 LPUART EDMA Multi Channel Usage and tcdMemoryPoolPtr</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IMXRT1024-LPUART-EDMA-Multi-Channel-Usage-and-tcdMemoryPoolPtr/m-p/1349105#M16532</link>
      <description>&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;I am just trying to use multiple LPUART with DMA. I am using lpuart_edma_rb_transfer SDK example as reference.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="c"&gt;.
..
...
/* Allocate TCD memory poll with ring buffer used. */
AT_NONCACHEABLE_SECTION_ALIGN(static edma_tcd_t tcdMemoryPoolPtr[1], sizeof(edma_tcd_t));
...
..
.&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="c"&gt;/* Start ring buffer. */
static void EXAMPLE_StartRingBufferEDMA(void)
{
    edma_transfer_config_t xferConfig;

    /* Install TCD memory for using only one TCD queue. */
    EDMA_InstallTCDMemory(&amp;amp;g_lpuartRxEdmaHandle, (edma_tcd_t *)&amp;amp;tcdMemoryPoolPtr[0], 1U);

    /* Prepare transfer to receive data to ring buffer. */
    EDMA_PrepareTransfer(&amp;amp;xferConfig, (void *)(uint32_t *)LPUART_GetDataRegisterAddress(EXAMPLE_LPUART),
                         sizeof(uint8_t), g_ringBuffer, sizeof(uint8_t), sizeof(uint8_t), EXAMPLE_RING_BUFFER_SIZE,
                         kEDMA_PeripheralToMemory);

    /* Submit transfer. */
    g_lpuartRxEdmaHandle.tcdUsed = 1U;
    g_lpuartRxEdmaHandle.tail    = 0U;
    EDMA_TcdReset(&amp;amp;g_lpuartRxEdmaHandle.tcdPool[0U]);
    EDMA_TcdSetTransferConfig(&amp;amp;g_lpuartRxEdmaHandle.tcdPool[0U], &amp;amp;xferConfig, tcdMemoryPoolPtr);

    /* Enable major interrupt for counting received bytes. */
    g_lpuartRxEdmaHandle.tcdPool[0U].CSR |= DMA_CSR_INTMAJOR_MASK;

    /* There is no live chain, TCD block need to be installed in TCD registers. */
    EDMA_InstallTCD(g_lpuartRxEdmaHandle.base, g_lpuartRxEdmaHandle.channel, &amp;amp;g_lpuartRxEdmaHandle.tcdPool[0U]);

    /* Setup call back function. */
    EDMA_SetCallback(&amp;amp;g_lpuartRxEdmaHandle, EXAMPLE_RxEDMACallback, NULL);

    /* Start EDMA transfer. */
    EDMA_StartTransfer(&amp;amp;g_lpuartRxEdmaHandle);

    /* Enable LPUART RX EDMA. */
    LPUART_EnableRxDMA(EXAMPLE_LPUART, true);

    /* Enable RX interrupt for detecting the IDLE line interrupt. */
    LPUART_EnableInterrupts(EXAMPLE_LPUART, kLPUART_IdleLineInterruptEnable);
    EnableIRQ(EXAMPLE_LPUART_IRQn);
}&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is it enough to change below parameters to use multiple EDMA for multiple LPUART&lt;/P&gt;&lt;P&gt;tcdMemoryPoolPtr[manipulated_size]&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;g_lpuartRxEdmaHandle.tcdUsed = 1U;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;g_lpuartRxEdmaHandle.tail = 0U;&lt;/P&gt;&lt;P&gt;EDMA_TcdReset(&amp;amp;g_lpuartRxEdmaHandle.tcdPool[manipulated_index]);&lt;/P&gt;&lt;P&gt;EDMA_TcdSetTransferConfig(&amp;amp;g_lpuartRxEdmaHandle.tcdPool[manipulated_index], &amp;amp;xferConfig, tcdMemoryPoolPtr);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks and Regards.&lt;/P&gt;</description>
      <pubDate>Thu, 30 Sep 2021 11:46:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IMXRT1024-LPUART-EDMA-Multi-Channel-Usage-and-tcdMemoryPoolPtr/m-p/1349105#M16532</guid>
      <dc:creator>Lukas_Frank</dc:creator>
      <dc:date>2021-09-30T11:46:14Z</dc:date>
    </item>
    <item>
      <title>Re: IMXRT1024 LPUART EDMA Multi Channel Usage and tcdMemoryPoolPtr</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IMXRT1024-LPUART-EDMA-Multi-Channel-Usage-and-tcdMemoryPoolPtr/m-p/1351741#M16593</link>
      <description>&lt;P&gt;Hi Dear&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/56840"&gt;@jeremyzhou&lt;/a&gt;,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Could you please help me about the topic?&lt;/P&gt;&lt;P&gt;Thanks and Regards.&lt;/P&gt;</description>
      <pubDate>Thu, 07 Oct 2021 08:26:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IMXRT1024-LPUART-EDMA-Multi-Channel-Usage-and-tcdMemoryPoolPtr/m-p/1351741#M16593</guid>
      <dc:creator>Lukas_Frank</dc:creator>
      <dc:date>2021-10-07T08:26:28Z</dc:date>
    </item>
    <item>
      <title>Re: IMXRT1024 LPUART EDMA Multi Channel Usage and tcdMemoryPoolPtr</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IMXRT1024-LPUART-EDMA-Multi-Channel-Usage-and-tcdMemoryPoolPtr/m-p/1352549#M16618</link>
      <description>&lt;P&gt;Hi,&lt;BR /&gt;Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.&lt;BR /&gt;1) Is it enough to change below parameters to use multiple EDMA for multiple LPUART&lt;BR /&gt;--- No, I'm afraid not.&lt;BR /&gt;Have a great day.&lt;BR /&gt;TIC&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Fri, 08 Oct 2021 08:53:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IMXRT1024-LPUART-EDMA-Multi-Channel-Usage-and-tcdMemoryPoolPtr/m-p/1352549#M16618</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2021-10-08T08:53:21Z</dc:date>
    </item>
    <item>
      <title>Re: IMXRT1024 LPUART EDMA Multi Channel Usage and tcdMemoryPoolPtr</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IMXRT1024-LPUART-EDMA-Multi-Channel-Usage-and-tcdMemoryPoolPtr/m-p/1352679#M16621</link>
      <description>&lt;P&gt;Hi Dear &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/56840"&gt;@jeremyzhou&lt;/a&gt;,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks for your feedback. Could you please help me about the implementation? Do you have any directive or example code for multiple LPUART with EDMA. It has really high importance for the project.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 08 Oct 2021 12:47:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IMXRT1024-LPUART-EDMA-Multi-Channel-Usage-and-tcdMemoryPoolPtr/m-p/1352679#M16621</guid>
      <dc:creator>Lukas_Frank</dc:creator>
      <dc:date>2021-10-08T12:47:39Z</dc:date>
    </item>
    <item>
      <title>Re: IMXRT1024 LPUART EDMA Multi Channel Usage and tcdMemoryPoolPtr</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IMXRT1024-LPUART-EDMA-Multi-Channel-Usage-and-tcdMemoryPoolPtr/m-p/1353037#M16640</link>
      <description>&lt;P&gt;Hi,&lt;BR /&gt;Thanks for your reply.&lt;BR /&gt;1) Could you please help me about the implementation? Do you have any directive or example code for multiple LPUART with EDMA?&lt;BR /&gt;-- In the lpuart_edma_rb_transfer demo, it uses the LUART1 for example, if you want to use the multiple LPUART, for instance, the LPUART2, LPUART3, etc, it's easy to do that via copy the original demo code, then adjust the code a bit.&lt;BR /&gt;Have a great day.&lt;BR /&gt;TIC&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Sat, 09 Oct 2021 07:37:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IMXRT1024-LPUART-EDMA-Multi-Channel-Usage-and-tcdMemoryPoolPtr/m-p/1353037#M16640</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2021-10-09T07:37:59Z</dc:date>
    </item>
    <item>
      <title>Re: IMXRT1024 LPUART EDMA Multi Channel Usage and tcdMemoryPoolPtr</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IMXRT1024-LPUART-EDMA-Multi-Channel-Usage-and-tcdMemoryPoolPtr/m-p/1353121#M16645</link>
      <description>&lt;P&gt;Hi Dear&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/56840"&gt;@jeremyzhou&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks for your feedback. I just get confused a little bit when you said "&lt;SPAN&gt;--- No, I'm afraid not.". Could you please confirm my code about the way I go ? I will be shairing below. Could you check that please? &lt;STRONG&gt;(lpuart_edma_rb_transfer.c attached)&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I have some highlited questions here:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Q1&lt;/STRONG&gt; : Should I use separate &lt;STRONG&gt;lpuart_edma_handle_t&lt;/STRONG&gt; for each UARTx object?&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Q2:&lt;/STRONG&gt; Should I align tcdMemoryPoolPtr like below ?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="c"&gt;//Increased tcdMemoryPoolPtr[1] to tcdMemoryPoolPtr[2]
AT_NONCACHEABLE_SECTION_ALIGN(static edma_tcd_t tcdMemoryPoolPtr[2], sizeof(edma_tcd_t)); &lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Q3:&lt;/STRONG&gt;&amp;nbsp;Should I use seperate &lt;STRONG&gt;edma_handle_t&lt;/STRONG&gt; for each RX(like g_lpuartRxEdmaHandle, g_lpuartRxEdmaHandle2, so on)&amp;nbsp; or Can I use one &lt;STRONG&gt;g_lpuartRxEdmaHandle&lt;/STRONG&gt; for all and only change tcdUsed? For the time being, I used like below. There are some missing point for me in comment lines for &lt;STRONG&gt;tcdUsed, tail,&amp;nbsp;tcdMemoryPoolPtr[&lt;/STRONG&gt;indexValue=?&lt;STRONG&gt;]&amp;nbsp;&lt;/STRONG&gt;and &lt;STRONG&gt;tcdPool[&lt;/STRONG&gt;indexValue=?&lt;STRONG&gt;]&lt;/STRONG&gt;. Could you please check that?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="c"&gt;static void EXAMPLE_StartRingBufferEDMA2(void)
{
    edma_transfer_config_t xferConfig;

    EDMA_InstallTCDMemory(&amp;amp;g_lpuartRxEdmaHandle2, (edma_tcd_t *)&amp;amp;tcdMemoryPoolPtr[1], 1U); //NOT SURE
    EDMA_PrepareTransfer(&amp;amp;xferConfig, (void *)(uint32_t *)LPUART_GetDataRegisterAddress(EXAMPLE_LPUART2),
                         sizeof(uint8_t), g_ringBuffer2, sizeof(uint8_t), sizeof(uint8_t), EXAMPLE_RING_BUFFER_SIZE,
                         kEDMA_PeripheralToMemory);

    g_lpuartRxEdmaHandle2.tcdUsed = 2U; //NOT SURE 1U or 2U
    g_lpuartRxEdmaHandle2.tail    = 0U; //NOT SURE What?
    EDMA_TcdReset(&amp;amp;g_lpuartRxEdmaHandle2.tcdPool[1U]);
    EDMA_TcdSetTransferConfig(&amp;amp;g_lpuartRxEdmaHandle2.tcdPool[1U], &amp;amp;xferConfig, tcdMemoryPoolPtr);


    g_lpuartRxEdmaHandle2.tcdPool[1U].CSR |= DMA_CSR_INTMAJOR_MASK;
    EDMA_InstallTCD(g_lpuartRxEdmaHandle2.base, g_lpuartRxEdmaHandle2.channel, &amp;amp;g_lpuartRxEdmaHandle2.tcdPool[1U]);
    EDMA_SetCallback(&amp;amp;g_lpuartRxEdmaHandle2, EXAMPLE_RxEDMACallback2, NULL);
    EDMA_StartTransfer(&amp;amp;g_lpuartRxEdmaHandle2);
    LPUART_EnableRxDMA(EXAMPLE_LPUART2, true);
    LPUART_EnableInterrupts(EXAMPLE_LPUART2, kLPUART_IdleLineInterruptEnable);
    EnableIRQ(EXAMPLE_LPUART_IRQn2);
}&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am appretiate for your help.&lt;/P&gt;&lt;P&gt;Thanks and Regards.&lt;/P&gt;&lt;DIV&gt;&lt;DIV class="gtx-trans-icon"&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/DIV&gt;</description>
      <pubDate>Sun, 10 Oct 2021 09:52:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IMXRT1024-LPUART-EDMA-Multi-Channel-Usage-and-tcdMemoryPoolPtr/m-p/1353121#M16645</guid>
      <dc:creator>Lukas_Frank</dc:creator>
      <dc:date>2021-10-10T09:52:17Z</dc:date>
    </item>
    <item>
      <title>Re: IMXRT1024 LPUART EDMA Multi Channel Usage and tcdMemoryPoolPtr</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IMXRT1024-LPUART-EDMA-Multi-Channel-Usage-and-tcdMemoryPoolPtr/m-p/1353531#M16653</link>
      <description>&lt;P&gt;Hi,&lt;BR /&gt;Q1 : Should I use separate lpuart_edma_handle_t for each UARTx object?&lt;BR /&gt;-- Yes.&lt;BR /&gt;Q2: Should I align tcdMemoryPoolPtr like below ? &lt;BR /&gt;-- Yes.&lt;BR /&gt;Q3: Should I use seperate edma_handle_t for each RX(like g_lpuartRxEdmaHandle, g_lpuartRxEdmaHandle2, so on) &lt;BR /&gt;-- Yes.&lt;BR /&gt;Q4: Could you please check that?&lt;BR /&gt;-- Yes.&lt;/P&gt;
&lt;LI-CODE lang="c"&gt;static void EXAMPLE_StartRingBufferEDMA2(void)
{
    edma_transfer_config_t xferConfig;

    EDMA_InstallTCDMemory(&amp;amp;g_lpuartRxEdmaHandle2, (edma_tcd_t *)&amp;amp;tcdMemoryPoolPtr[1], 1U); //NOT SURE
    EDMA_PrepareTransfer(&amp;amp;xferConfig, (void *)(uint32_t *)LPUART_GetDataRegisterAddress(EXAMPLE_LPUART2),
                         sizeof(uint8_t), g_ringBuffer2, sizeof(uint8_t), sizeof(uint8_t), EXAMPLE_RING_BUFFER_SIZE,
                         kEDMA_PeripheralToMemory);

    g_lpuartRxEdmaHandle2.tcdUsed = 1U; //NOT SURE 1U or 2U
    g_lpuartRxEdmaHandle2.tail    = 0U; //NOT SURE What?
    EDMA_TcdReset(&amp;amp;g_lpuartRxEdmaHandle2.tcdPool[0U]);
    EDMA_TcdSetTransferConfig(&amp;amp;g_lpuartRxEdmaHandle2.tcdPool[0U], &amp;amp;xferConfig, tcdMemoryPoolPtr[1]);


    g_lpuartRxEdmaHandle2.tcdPool[1U].CSR |= DMA_CSR_INTMAJOR_MASK;
    EDMA_InstallTCD(g_lpuartRxEdmaHandle2.base, g_lpuartRxEdmaHandle2.channel, &amp;amp;g_lpuartRxEdmaHandle2.tcdPool[0]);
    EDMA_SetCallback(&amp;amp;g_lpuartRxEdmaHandle2, EXAMPLE_RxEDMACallback2, NULL);
    EDMA_StartTransfer(&amp;amp;g_lpuartRxEdmaHandle2);
    LPUART_EnableRxDMA(EXAMPLE_LPUART2, true);
    LPUART_EnableInterrupts(EXAMPLE_LPUART2, kLPUART_IdleLineInterruptEnable);
    EnableIRQ(EXAMPLE_LPUART_IRQn2);
}&lt;/LI-CODE&gt;
&lt;P&gt;Have a great day.&lt;BR /&gt;TIC&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Mon, 11 Oct 2021 12:25:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IMXRT1024-LPUART-EDMA-Multi-Channel-Usage-and-tcdMemoryPoolPtr/m-p/1353531#M16653</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2021-10-11T12:25:25Z</dc:date>
    </item>
    <item>
      <title>Re: IMXRT1024 LPUART EDMA Multi Channel Usage and tcdMemoryPoolPtr</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IMXRT1024-LPUART-EDMA-Multi-Channel-Usage-and-tcdMemoryPoolPtr/m-p/1354036#M16670</link>
      <description>&lt;P&gt;Thank you Dear&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/56840"&gt;@jeremyzhou&lt;/a&gt;.&lt;/P&gt;&lt;P&gt;Best wishes &lt;LI-EMOJI id="lia_slightly-smiling-face" title=":slightly_smiling_face:"&gt;&lt;/LI-EMOJI&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 12 Oct 2021 08:19:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IMXRT1024-LPUART-EDMA-Multi-Channel-Usage-and-tcdMemoryPoolPtr/m-p/1354036#M16670</guid>
      <dc:creator>Lukas_Frank</dc:creator>
      <dc:date>2021-10-12T08:19:28Z</dc:date>
    </item>
  </channel>
</rss>