<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MIMXRT1170-EVK: How to enable instruction trace on the RT1170 evaluation board? in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/MIMXRT1170-EVK-How-to-enable-instruction-trace-on-the-RT1170/m-p/1349302#M16541</link>
    <description>&lt;P&gt;In case anyone else is trying to get the RT1170-EVK to work with Segger's J-Trace, here's what I found:&lt;BR /&gt;&lt;BR /&gt;Segger verified that they have done the work-around for ERR050708 errata.&lt;BR /&gt;&lt;BR /&gt;Segger also verified that the only modifications needed to the RT1170-EVK is installing 0-ohm resistors R1881, R1882, R1883, R1884, R1885, and R1886.&lt;BR /&gt;&lt;BR /&gt;The primary change that allows instruction trace to work is to adjust the sampling point of the TRACE_D0-3.&amp;nbsp; Segger's example &lt;A href="https://wiki.segger.com/i.MXRT1176#Tracing_on_iMXRT1176_series" target="_self"&gt;here&lt;/A&gt; defaults to +2ns adjustment.&amp;nbsp; This does not work...their example (which uses just 1-bit width) should have had 0ns adjustment.&amp;nbsp; I verified that 0ns works with 1-bit, but when I enabled 4-bit trace, I got more errors.&amp;nbsp; Adjusting sampling by -0.5ns for all 4 trace lines seems to have solved the problem.&lt;BR /&gt;&lt;BR /&gt;The next step to getting trace to work for an application that runs from the QSPI Flash is to modify the&amp;nbsp;Ozone.jdebug trace debugger script file per this web page:&amp;nbsp;&lt;A href="https://wiki.segger.com/Debug_on_a_Target_with_Bootloader#ROM_bootloader" target="_blank"&gt;https://wiki.segger.com/Debug_on_a_Target_with_Bootloader#ROM_bootloader&lt;/A&gt;&amp;nbsp;.&amp;nbsp; The main thing is to do what is at the bottom of the page and make&amp;nbsp;AfterTargetDownload()&amp;nbsp;and&amp;nbsp;AfterTargetReset() empty functions so that the RT1176's ROM loader does the SP and PC initialization.&lt;BR /&gt;&lt;BR /&gt;Another thing to know is that Segger's troubleshooting says to use their J-Trace Pro Webserver application to see the "half-sync detection" status, but this always indicates an error on the RT1176 even when trace is working.&amp;nbsp; Segger technical support said this does not work due to NXP's pattern.&amp;nbsp; Segger will be updating their documentation.&amp;nbsp; The best way to determine if instruction trace is working is to change the trace timing configuration in Ozone.&amp;nbsp; Stop the application and then restart it.&amp;nbsp; If the instruction trace window starts displaying data and there are no errors in the console, then it is working.&lt;BR /&gt;&lt;BR /&gt;Instruction trace on the RT1170-EVK using Ozone seems to be working well now, but I do occasionally get "Trace overflow detected. Trace packets may have been lost." errors in the console.&amp;nbsp; Segger technical support said this was because the RT1176 trace clock rate is too low in relation to the 1GHZ processor speed.&amp;nbsp; The only solution is to reduce the processor speed.&amp;nbsp; It looks like the RT1176 always uses a 50MHZ Trace Clock.&amp;nbsp; I don't know if this can be increased or not yet, but seems adequate most of the time as long as using 4-bit trace width so I'm happy with this for now.&amp;nbsp; This Segger webpage has more info.&amp;nbsp;&amp;nbsp;&lt;A href="https://wiki.segger.com/J-Trace_overflow_error" target="_blank"&gt;https://wiki.segger.com/J-Trace_overflow_error&lt;/A&gt;&amp;nbsp;.&amp;nbsp; #1 is the error condition I'm intermittently seeing.&lt;I&gt;&lt;BR /&gt;&lt;/I&gt;&lt;/P&gt;&lt;P&gt;I'm building the application using MCUXpresso, but debugging using Segger's Ozone when I need instruction trace capability.&amp;nbsp; Hopefully someday, instruction trace capability will be added to MCUXpresso...&lt;/P&gt;</description>
    <pubDate>Thu, 30 Sep 2021 19:20:24 GMT</pubDate>
    <dc:creator>mrd</dc:creator>
    <dc:date>2021-09-30T19:20:24Z</dc:date>
    <item>
      <title>MIMXRT1170-EVK: How to enable instruction trace on the RT1170 evaluation board?</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/MIMXRT1170-EVK-How-to-enable-instruction-trace-on-the-RT1170/m-p/1335662#M16203</link>
      <description>&lt;P&gt;I have a Segger J-Trace Cortex-M debug probe and want to enable instruction trace (ETM Trace) on the RT1170 Evaluation Board.&amp;nbsp; What needs to be modified on the board?&lt;/P&gt;&lt;P&gt;I have installed 0-ohm resistors R1881, R1882, R1883, R1884, R1885, and R1886 (schematic page 7 lower right) so that TRACE_CLK, TRACE_SWO, and TRACE_D3:0 are connected to the RT1170, but it still does not work.&amp;nbsp; The J-Trace complains of "Unknown trace data packet detected".&amp;nbsp; I have checked for opens &amp;amp; shorts in the trace connections.&amp;nbsp; Seems okay.&amp;nbsp; I have also tried 1-bit and 4-bit trace width.&lt;/P&gt;&lt;P&gt;Are there any parts that need to be removed to allow instruction trace to work?&lt;/P&gt;&lt;P&gt;Has anyone else made instruction trace work with a J-Trace or any other debug probe?&lt;/P&gt;&lt;P&gt;I am using Segger's pre-compiled iMXRT1176_M7 demo project for the RT1170-EVK that is &lt;A href="https://wiki.segger.com/i.MXRT1176#Tracing_on_iMXRT1176_series" target="_self"&gt;here&lt;/A&gt;.&amp;nbsp; Segger's instructions say that "some solder bridges had to be closed" and to consult the board's manual, but I don't see anything about this in the demo &lt;A href="https://www.nxp.com/webapp/Download?colCode=MIMXRT1170EVKHUG" target="_self"&gt;board's user guide&lt;/A&gt;.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any help would be very much appreciated!&lt;/P&gt;</description>
      <pubDate>Tue, 07 Sep 2021 00:41:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/MIMXRT1170-EVK-How-to-enable-instruction-trace-on-the-RT1170/m-p/1335662#M16203</guid>
      <dc:creator>mrd</dc:creator>
      <dc:date>2021-09-07T00:41:00Z</dc:date>
    </item>
    <item>
      <title>Re: MIMXRT1170-EVK: How to enable instruction trace on the RT1170 evaluation board?</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/MIMXRT1170-EVK-How-to-enable-instruction-trace-on-the-RT1170/m-p/1339382#M16305</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/182979"&gt;@mrd&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;MCUXpresso IDE supports SWO trace for RT1170. Instruction trace capture is supported only in conjunction with an MCU’s Embedded Trace Buffer (ETB) or Micro Trace Buffer (MTB).&lt;BR /&gt;Unfortunately, neither is implemented by RT1170, so instruction trace is not supported on MCUXpresso IDE.&lt;/P&gt;
&lt;P&gt;Other probe vendors may offer support for ETM-based trace capture in other IDEs. For J-Trace details please refer to Segger.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Jing&lt;/P&gt;</description>
      <pubDate>Tue, 14 Sep 2021 02:21:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/MIMXRT1170-EVK-How-to-enable-instruction-trace-on-the-RT1170/m-p/1339382#M16305</guid>
      <dc:creator>jingpan</dc:creator>
      <dc:date>2021-09-14T02:21:47Z</dc:date>
    </item>
    <item>
      <title>Re: MIMXRT1170-EVK: How to enable instruction trace on the RT1170 evaluation board?</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/MIMXRT1170-EVK-How-to-enable-instruction-trace-on-the-RT1170/m-p/1339813#M16311</link>
      <description>&lt;P&gt;Hi.&amp;nbsp; Thank you for the reply.&amp;nbsp; I know that MCUXpresso does not currently support ETM trace. [It would be wonderful though if NXP added this sometime.]&amp;nbsp; I am using &lt;A href="https://www.segger.com/products/development-tools/ozone-j-link-debugger/" target="_self"&gt;Segger's Ozone debugger&lt;/A&gt;, which does support ETM instruction trace.&lt;/P&gt;&lt;P&gt;The question I'm asking is what hardware modifications need to be done on &lt;A href="https://www.nxp.com/downloads/en/design-support/MIMXRT1170-EVK-DESIGNFILES.zip" target="_self"&gt;NXP's MIMXRT1170-EVK&lt;/A&gt; (RT1170 evaluation board) rev C1 to allow ETM instruction trace to work. Is it only installing 0-ohm resistors R1881, R1882, R1883, R1884, R1885, and R1886? Or do some parts need to be removed to decrease loading on TRACE_CLK, TRACE_SMO, or TRACE_D3:0?&lt;/P&gt;&lt;P&gt;Since NXP designed the MIMXRT1170-EVK evaluation board, it seems like this should be information that NXP would provide, but I cannot find it in the user manual. The EVK's designer obviously intended for the board to support ETM trace since it is mentioned in the board's rev C revision history on page #1 of the schematic. Also, page #27 of the schematic labels J58 connector as "Cortex Debug + ETM".&lt;/P&gt;&lt;P&gt;Please provide instructions about which parts need to be installed (added) and if any need to be removed from MIMXRT1170-EVK rev C1.&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;</description>
      <pubDate>Tue, 14 Sep 2021 12:59:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/MIMXRT1170-EVK-How-to-enable-instruction-trace-on-the-RT1170/m-p/1339813#M16311</guid>
      <dc:creator>mrd</dc:creator>
      <dc:date>2021-09-14T12:59:47Z</dc:date>
    </item>
    <item>
      <title>Re: MIMXRT1170-EVK: How to enable instruction trace on the RT1170 evaluation board?</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/MIMXRT1170-EVK-How-to-enable-instruction-trace-on-the-RT1170/m-p/1340445#M16330</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Installing 0&lt;SPAN&gt;-ohm resistors R1881, R1882, R1883, R1884, R1885, and R1886 is enough.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Regards,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Jing&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 15 Sep 2021 08:51:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/MIMXRT1170-EVK-How-to-enable-instruction-trace-on-the-RT1170/m-p/1340445#M16330</guid>
      <dc:creator>jingpan</dc:creator>
      <dc:date>2021-09-15T08:51:26Z</dc:date>
    </item>
    <item>
      <title>Re: MIMXRT1170-EVK: How to enable instruction trace on the RT1170 evaluation board?</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/MIMXRT1170-EVK-How-to-enable-instruction-trace-on-the-RT1170/m-p/1340495#M16331</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;In RT1170 errata, there is a ERR050708. Debugger can not access ROM table by default. I wonder Jtrace may can't access ETM or TPIU if there isn't workaround driver.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Jing&lt;/P&gt;</description>
      <pubDate>Wed, 15 Sep 2021 09:44:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/MIMXRT1170-EVK-How-to-enable-instruction-trace-on-the-RT1170/m-p/1340495#M16331</guid>
      <dc:creator>jingpan</dc:creator>
      <dc:date>2021-09-15T09:44:33Z</dc:date>
    </item>
    <item>
      <title>Re: MIMXRT1170-EVK: How to enable instruction trace on the RT1170 evaluation board?</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/MIMXRT1170-EVK-How-to-enable-instruction-trace-on-the-RT1170/m-p/1349302#M16541</link>
      <description>&lt;P&gt;In case anyone else is trying to get the RT1170-EVK to work with Segger's J-Trace, here's what I found:&lt;BR /&gt;&lt;BR /&gt;Segger verified that they have done the work-around for ERR050708 errata.&lt;BR /&gt;&lt;BR /&gt;Segger also verified that the only modifications needed to the RT1170-EVK is installing 0-ohm resistors R1881, R1882, R1883, R1884, R1885, and R1886.&lt;BR /&gt;&lt;BR /&gt;The primary change that allows instruction trace to work is to adjust the sampling point of the TRACE_D0-3.&amp;nbsp; Segger's example &lt;A href="https://wiki.segger.com/i.MXRT1176#Tracing_on_iMXRT1176_series" target="_self"&gt;here&lt;/A&gt; defaults to +2ns adjustment.&amp;nbsp; This does not work...their example (which uses just 1-bit width) should have had 0ns adjustment.&amp;nbsp; I verified that 0ns works with 1-bit, but when I enabled 4-bit trace, I got more errors.&amp;nbsp; Adjusting sampling by -0.5ns for all 4 trace lines seems to have solved the problem.&lt;BR /&gt;&lt;BR /&gt;The next step to getting trace to work for an application that runs from the QSPI Flash is to modify the&amp;nbsp;Ozone.jdebug trace debugger script file per this web page:&amp;nbsp;&lt;A href="https://wiki.segger.com/Debug_on_a_Target_with_Bootloader#ROM_bootloader" target="_blank"&gt;https://wiki.segger.com/Debug_on_a_Target_with_Bootloader#ROM_bootloader&lt;/A&gt;&amp;nbsp;.&amp;nbsp; The main thing is to do what is at the bottom of the page and make&amp;nbsp;AfterTargetDownload()&amp;nbsp;and&amp;nbsp;AfterTargetReset() empty functions so that the RT1176's ROM loader does the SP and PC initialization.&lt;BR /&gt;&lt;BR /&gt;Another thing to know is that Segger's troubleshooting says to use their J-Trace Pro Webserver application to see the "half-sync detection" status, but this always indicates an error on the RT1176 even when trace is working.&amp;nbsp; Segger technical support said this does not work due to NXP's pattern.&amp;nbsp; Segger will be updating their documentation.&amp;nbsp; The best way to determine if instruction trace is working is to change the trace timing configuration in Ozone.&amp;nbsp; Stop the application and then restart it.&amp;nbsp; If the instruction trace window starts displaying data and there are no errors in the console, then it is working.&lt;BR /&gt;&lt;BR /&gt;Instruction trace on the RT1170-EVK using Ozone seems to be working well now, but I do occasionally get "Trace overflow detected. Trace packets may have been lost." errors in the console.&amp;nbsp; Segger technical support said this was because the RT1176 trace clock rate is too low in relation to the 1GHZ processor speed.&amp;nbsp; The only solution is to reduce the processor speed.&amp;nbsp; It looks like the RT1176 always uses a 50MHZ Trace Clock.&amp;nbsp; I don't know if this can be increased or not yet, but seems adequate most of the time as long as using 4-bit trace width so I'm happy with this for now.&amp;nbsp; This Segger webpage has more info.&amp;nbsp;&amp;nbsp;&lt;A href="https://wiki.segger.com/J-Trace_overflow_error" target="_blank"&gt;https://wiki.segger.com/J-Trace_overflow_error&lt;/A&gt;&amp;nbsp;.&amp;nbsp; #1 is the error condition I'm intermittently seeing.&lt;I&gt;&lt;BR /&gt;&lt;/I&gt;&lt;/P&gt;&lt;P&gt;I'm building the application using MCUXpresso, but debugging using Segger's Ozone when I need instruction trace capability.&amp;nbsp; Hopefully someday, instruction trace capability will be added to MCUXpresso...&lt;/P&gt;</description>
      <pubDate>Thu, 30 Sep 2021 19:20:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/MIMXRT1170-EVK-How-to-enable-instruction-trace-on-the-RT1170/m-p/1349302#M16541</guid>
      <dc:creator>mrd</dc:creator>
      <dc:date>2021-09-30T19:20:24Z</dc:date>
    </item>
    <item>
      <title>Re: MIMXRT1170-EVK: How to enable instruction trace on the RT1170 evaluation board?</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/MIMXRT1170-EVK-How-to-enable-instruction-trace-on-the-RT1170/m-p/1677306#M25696</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/61241"&gt;@jingpan&lt;/a&gt;&amp;nbsp; Can you confirm if this same approach for ETM trace will work for MIMXRT1170-EVKB? &amp;nbsp; I made the same setup, but never get a TRACE_CLK signal. &amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I confirmed the PCB trace is connected properly to the MCU by creating a GPIO project to toggle the same pin and using an oscilloscope on the ETM header pin and I can see the pin changing, so it is something about the TRACE_CLK configuration that is not working. &amp;nbsp;The EVKB seems somewhat different than the original MIMXRT1170-EVK.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any help is appreciated!&lt;/P&gt;</description>
      <pubDate>Tue, 27 Jun 2023 23:51:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/MIMXRT1170-EVK-How-to-enable-instruction-trace-on-the-RT1170/m-p/1677306#M25696</guid>
      <dc:creator>jackking</dc:creator>
      <dc:date>2023-06-27T23:51:58Z</dc:date>
    </item>
    <item>
      <title>Re: MIMXRT1170-EVK: How to enable instruction trace on the RT1170 evaluation board?</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/MIMXRT1170-EVK-How-to-enable-instruction-trace-on-the-RT1170/m-p/1677847#M25716</link>
      <description>&lt;P&gt;Hi.&amp;nbsp; I don't have the&amp;nbsp;&lt;SPAN&gt;EVKB version of the evaluation board.&amp;nbsp; I compared schematics briefly.&amp;nbsp; The only difference I saw that may be causing the problem is that they changed the 10/100mbs ethernet chip from KSZ8081 to RTL8201.&amp;nbsp; The TRACE_xxx signals are connected to the ethernet chip and may need to be disconnected on the EVKB board for the trace feature to work.&amp;nbsp; [If NXP tech support sees this, please let us know.]&amp;nbsp; For the EVKB version, NXP has added 0-ohm resistors so that TRACE_xxx signals can be isolated from the RTL8201.&amp;nbsp; For example, R1290 could be removed to disconnect from TRACE_CLK.&amp;nbsp; See picture below.&amp;nbsp; The trace feature is very helpful for debugging, but its too bad one has to give up using the 10/100 ethernet interface.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="mrd_0-1687952912417.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/229856i4865AE6297BFA0C9/image-size/medium?v=v2&amp;amp;px=400" role="button" title="mrd_0-1687952912417.png" alt="mrd_0-1687952912417.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 28 Jun 2023 11:51:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/MIMXRT1170-EVK-How-to-enable-instruction-trace-on-the-RT1170/m-p/1677847#M25716</guid>
      <dc:creator>mrd</dc:creator>
      <dc:date>2023-06-28T11:51:26Z</dc:date>
    </item>
    <item>
      <title>Re: MIMXRT1170-EVK: How to enable instruction trace on the RT1170 evaluation board?</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/MIMXRT1170-EVK-How-to-enable-instruction-trace-on-the-RT1170/m-p/1677864#M25719</link>
      <description>&lt;P&gt;Thanks for the reply. I have also removed the ethernet related jumpers, it had no effect on the TRACE_CLK signal.&lt;BR /&gt;&lt;BR /&gt;With the GPIO test, I can confirm that the TRACE_CLK pin of the ETM header is connected and controllable by the MCU.&lt;BR /&gt;&lt;BR /&gt;I have tried both the Segger Ozone Trace sample project as well as some of the NXP MCUXpresso SDK samples and the TRACE_CLK signal is never output.&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 28 Jun 2023 12:24:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/MIMXRT1170-EVK-How-to-enable-instruction-trace-on-the-RT1170/m-p/1677864#M25719</guid>
      <dc:creator>jackking</dc:creator>
      <dc:date>2023-06-28T12:24:32Z</dc:date>
    </item>
    <item>
      <title>Re: MIMXRT1170-EVK: How to enable instruction trace on the RT1170 evaluation board?</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/MIMXRT1170-EVK-How-to-enable-instruction-trace-on-the-RT1170/m-p/1697316#M26164</link>
      <description>&lt;P&gt;your post was SO GREAT for me as the newbie user of segger JTRACE PRO.&lt;/P&gt;&lt;P&gt;Before I saw your article I was so desperated about the segger probe.&lt;/P&gt;&lt;P&gt;Now I still have two questions:&amp;nbsp;&lt;/P&gt;&lt;P&gt;1. how do you adjust the "-0.5ns" for the 4-bit traces. Do you use a high-end oscilliloscope to monitor the trace data signal quality?&lt;/P&gt;&lt;P&gt;2. after I follow your instruction, I can now have a much stabiler communiction between the probe and imxrt1170evk. But the trace performace disappoint me a little. Do you know how to downgrade the 1GHz&amp;nbsp; of CM7 core to a certain value?&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 02 Aug 2023 07:29:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/MIMXRT1170-EVK-How-to-enable-instruction-trace-on-the-RT1170/m-p/1697316#M26164</guid>
      <dc:creator>auftrag2021</dc:creator>
      <dc:date>2023-08-02T07:29:13Z</dc:date>
    </item>
    <item>
      <title>Re: MIMXRT1170-EVK: How to enable instruction trace on the RT1170 evaluation board?</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/MIMXRT1170-EVK-How-to-enable-instruction-trace-on-the-RT1170/m-p/1697994#M26176</link>
      <description>&lt;P&gt;Glad you found the post useful.&lt;/P&gt;&lt;P&gt;1) Timing was adjusted via trial &amp;amp; error.&amp;nbsp; No scope was used.&amp;nbsp; Even a really good scope probe would likely put too much capacitive load on the high frequency trace signals to be able to make useful measurements.&lt;/P&gt;&lt;P&gt;2) I use MCUExpresso ConfigTools&amp;gt;Clocks to edit the Cortex M7 Core Root Clock.&amp;nbsp; The excerpt below shows 792MHZ used with industrial grade RT1176.&amp;nbsp; I still frequently get trace buffer overruns at this clock rate, but it works well enough that I can eventually get a good trace when I'm debugging a problem where trace is useful.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="ConfigToolsClocks.png" style="width: 916px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/234819iFEB25EDCBD0AA842/image-size/large?v=v2&amp;amp;px=999" role="button" title="ConfigToolsClocks.png" alt="ConfigToolsClocks.png" /&gt;&lt;/span&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 02 Aug 2023 19:40:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/MIMXRT1170-EVK-How-to-enable-instruction-trace-on-the-RT1170/m-p/1697994#M26176</guid>
      <dc:creator>mrd</dc:creator>
      <dc:date>2023-08-02T19:40:18Z</dc:date>
    </item>
    <item>
      <title>Re: MIMXRT1170-EVK: How to enable instruction trace on the RT1170 evaluation board?</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/MIMXRT1170-EVK-How-to-enable-instruction-trace-on-the-RT1170/m-p/1698024#M26178</link>
      <description>&lt;P&gt;thank for your kindly feedback.&amp;nbsp;&lt;/P&gt;&lt;P&gt;just for your interesting:&amp;nbsp;&lt;/P&gt;&lt;P&gt;I downgraded the ARM PLL to a VERY low level. (168MHz)&lt;/P&gt;&lt;P&gt;Why 168MHz? because in the SEGGER JTRACE delivery there is a small test board with SMT32 chip which has 168MHz as system clk.&amp;nbsp;&lt;/P&gt;&lt;P&gt;What amazing me is, the instruction trace function in Ozone worked so well by this STM32 test board. I can smoothly play the trace record permanently without any trace overflow.&amp;nbsp;&lt;/P&gt;&lt;P&gt;but with the imxrt1170 evk, I still frequently have trace overflow problem. I also tried with some other frequencies, nothing better.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 02 Aug 2023 20:39:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/MIMXRT1170-EVK-How-to-enable-instruction-trace-on-the-RT1170/m-p/1698024#M26178</guid>
      <dc:creator>auftrag2021</dc:creator>
      <dc:date>2023-08-02T20:39:37Z</dc:date>
    </item>
  </channel>
</rss>