<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Could I use DCD to initialize HyperRAM? in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Could-I-use-DCD-to-initialize-HyperRAM/m-p/1336595#M16228</link>
    <description>&lt;P&gt;Hi, I'm using RT1062 for a GUI application, the hardware design is NAND+HyperRAM. Right now I'm using a second bootloader to initialize HyperRAM and DCD to initialize the NAND flash, could I use DCD for both the HyperRAM and NAND initizlization?&lt;/P&gt;</description>
    <pubDate>Wed, 08 Sep 2021 07:13:34 GMT</pubDate>
    <dc:creator>BlackTurbo</dc:creator>
    <dc:date>2021-09-08T07:13:34Z</dc:date>
    <item>
      <title>Could I use DCD to initialize HyperRAM?</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Could-I-use-DCD-to-initialize-HyperRAM/m-p/1336595#M16228</link>
      <description>&lt;P&gt;Hi, I'm using RT1062 for a GUI application, the hardware design is NAND+HyperRAM. Right now I'm using a second bootloader to initialize HyperRAM and DCD to initialize the NAND flash, could I use DCD for both the HyperRAM and NAND initizlization?&lt;/P&gt;</description>
      <pubDate>Wed, 08 Sep 2021 07:13:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Could-I-use-DCD-to-initialize-HyperRAM/m-p/1336595#M16228</guid>
      <dc:creator>BlackTurbo</dc:creator>
      <dc:date>2021-09-08T07:13:34Z</dc:date>
    </item>
    <item>
      <title>Re: Could I use DCD to initialize HyperRAM?</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Could-I-use-DCD-to-initialize-HyperRAM/m-p/1337235#M16238</link>
      <description>&lt;P&gt;Hi，&lt;BR /&gt;Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.&lt;BR /&gt;1） Could I use DCD for both the HyperRAM and NAND initialization?&lt;BR /&gt;-- No, I'm afraid not.&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Thu, 09 Sep 2021 00:20:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Could-I-use-DCD-to-initialize-HyperRAM/m-p/1337235#M16238</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2021-09-09T00:20:32Z</dc:date>
    </item>
  </channel>
</rss>