<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Multiple application firmware in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Multiple-application-firmware/m-p/1332830#M16149</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am working on a solution which allow the firmware update without effecting current mode of operation.&lt;/P&gt;&lt;P&gt;Couple of questions that I have are:&lt;/P&gt;&lt;P&gt;Can ROM bootloader support multiple images e.g. one at address 0x0X and other at address 0x0Y?&lt;/P&gt;&lt;P&gt;Also does it have the facility to boot from a particular address based on some sort flags?&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;</description>
    <pubDate>Wed, 01 Sep 2021 03:07:19 GMT</pubDate>
    <dc:creator>LoneWalker</dc:creator>
    <dc:date>2021-09-01T03:07:19Z</dc:date>
    <item>
      <title>Multiple application firmware</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Multiple-application-firmware/m-p/1332830#M16149</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am working on a solution which allow the firmware update without effecting current mode of operation.&lt;/P&gt;&lt;P&gt;Couple of questions that I have are:&lt;/P&gt;&lt;P&gt;Can ROM bootloader support multiple images e.g. one at address 0x0X and other at address 0x0Y?&lt;/P&gt;&lt;P&gt;Also does it have the facility to boot from a particular address based on some sort flags?&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;</description>
      <pubDate>Wed, 01 Sep 2021 03:07:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Multiple-application-firmware/m-p/1332830#M16149</guid>
      <dc:creator>LoneWalker</dc:creator>
      <dc:date>2021-09-01T03:07:19Z</dc:date>
    </item>
    <item>
      <title>Re: Multiple application firmware</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Multiple-application-firmware/m-p/1332904#M16151</link>
      <description>&lt;P&gt;Hi,&lt;BR /&gt;Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.&lt;BR /&gt;1) Can the ROM bootloader support multiple images e.g. one at address 0x0X and the other at address 0x0Y?&lt;BR /&gt;-- No, I'm afraid not.&lt;BR /&gt;2) Also does it have the facility to boot from a particular address based on some sort flags?&lt;BR /&gt;-- No.&lt;BR /&gt;Regarding your solution, I'd highly recommend you to refer to the &lt;A href="https://www.nxp.com/docs/en/application-note/AN12604.pdf" target="_self"&gt;application note&lt;/A&gt; to make it.&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Wed, 01 Sep 2021 05:50:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Multiple-application-firmware/m-p/1332904#M16151</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2021-09-01T05:50:34Z</dc:date>
    </item>
  </channel>
</rss>