<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Secure Provision Tool using UART not working in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Secure-Provision-Tool-using-UART-not-working/m-p/1322484#M15835</link>
    <description>&lt;P&gt;Thanks for trying, Victor, I will try another time. Good to know it works.&lt;/P&gt;&lt;P&gt;Ping&lt;/P&gt;</description>
    <pubDate>Thu, 12 Aug 2021 08:15:29 GMT</pubDate>
    <dc:creator>ping1</dc:creator>
    <dc:date>2021-08-12T08:15:29Z</dc:date>
    <item>
      <title>Secure Provision Tool using UART not working</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Secure-Provision-Tool-using-UART-not-working/m-p/1318217#M15655</link>
      <description>&lt;P&gt;Hi, All&lt;/P&gt;&lt;P&gt;Try to use serial mode with UART on EVK-RT1024 with SPT, and cannot get it working, I connect the PC UART to board J17, pin 8 &amp;amp;10, and also put the board into serial mode, however, the USB connect test shows failed result as below when click test Connection button.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="ping1_0-1628086759088.png" style="width: 291px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/151799iCE1EC9E344BC2FF3/image-dimensions/291x202?v=v2" width="291" height="202" role="button" title="ping1_0-1628086759088.png" alt="ping1_0-1628086759088.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;ping1_0-1628086759088.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I am intended to use the UART for our target board for factory programming using the SPT, not sure it works, there is no room for USB layout on this particular product.&lt;/P&gt;&lt;P&gt;Urgent help is needed please - does SPT support UART? or what I have done wrong?&lt;/P&gt;&lt;P&gt;Regards!&lt;/P&gt;&lt;P&gt;Ping&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 04 Aug 2021 14:23:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Secure-Provision-Tool-using-UART-not-working/m-p/1318217#M15655</guid>
      <dc:creator>ping1</dc:creator>
      <dc:date>2021-08-04T14:23:02Z</dc:date>
    </item>
    <item>
      <title>Re: Secure Provision Tool using UART not working</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Secure-Provision-Tool-using-UART-not-working/m-p/1319315#M15688</link>
      <description>&lt;P&gt;Hello Ping,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I just made a couple of tests on my end, and I didn't face any problems. I connect the board to the computer through J23 since the UART1 pins are connected to this USB connector.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-center" image-alt="victorjimenez_0-1628207772336.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/152047iBE73515ADCDC181F/image-size/medium?v=v2&amp;amp;px=400" role="button" title="victorjimenez_0-1628207772336.png" alt="victorjimenez_0-1628207772336.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;victorjimenez_0-1628207772336.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-center" image-alt="victorjimenez_1-1628207789363.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/152048iDE312FD714449365/image-size/medium?v=v2&amp;amp;px=400" role="button" title="victorjimenez_1-1628207789363.png" alt="victorjimenez_1-1628207789363.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;victorjimenez_1-1628207789363.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;You need to connect the USB cable to the same USB connector that you use for the debugger. Also, verify that you are selecting the correct COM Port.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Victor&amp;nbsp;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 05 Aug 2021 23:57:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Secure-Provision-Tool-using-UART-not-working/m-p/1319315#M15688</guid>
      <dc:creator>victorjimenez</dc:creator>
      <dc:date>2021-08-05T23:57:48Z</dc:date>
    </item>
    <item>
      <title>Re: Secure Provision Tool using UART not working</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Secure-Provision-Tool-using-UART-not-working/m-p/1322484#M15835</link>
      <description>&lt;P&gt;Thanks for trying, Victor, I will try another time. Good to know it works.&lt;/P&gt;&lt;P&gt;Ping&lt;/P&gt;</description>
      <pubDate>Thu, 12 Aug 2021 08:15:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Secure-Provision-Tool-using-UART-not-working/m-p/1322484#M15835</guid>
      <dc:creator>ping1</dc:creator>
      <dc:date>2021-08-12T08:15:29Z</dc:date>
    </item>
  </channel>
</rss>