<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: imxrt1021 sdram initialization parameter in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/imxrt1021-sdram-initialization-parameter/m-p/1317352#M15635</link>
    <description>&lt;P&gt;&lt;SPAN class="tgt highlight"&gt;I used this (\driver_examples\semc) test and it also failed to read the SDRAM without reading any data.&lt;/SPAN&gt;&lt;SPAN class="tgt"&gt; May I ask what other debugging means?&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Tue, 03 Aug 2021 12:48:27 GMT</pubDate>
    <dc:creator>mollygqs</dc:creator>
    <dc:date>2021-08-03T12:48:27Z</dc:date>
    <item>
      <title>imxrt1021 sdram initialization parameter</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/imxrt1021-sdram-initialization-parameter/m-p/1316796#M15616</link>
      <description>&lt;P&gt;Our IMXRT1021 PCB board, SDRAM cannot read and write. Sdram is the default SDK initialization parameter. What is the way to test the SDRAM clock, and then modify the initial SDRAM clock. Sdram is is42s16160.&lt;/P&gt;&lt;P&gt;sdramconfig.csxPinMux = kSEMC_MUXCSX0;&lt;BR /&gt;sdramconfig.address = 0x80000000;&lt;BR /&gt;sdramconfig.memsize_kbytes = 32 * 1024; /* 32MB = 32*1024*1KBytes*/&lt;BR /&gt;sdramconfig.portSize = kSEMC_PortSize16Bit;&lt;BR /&gt;sdramconfig.burstLen = kSEMC_Sdram_BurstLen1;&lt;BR /&gt;sdramconfig.columnAddrBitNum = kSEMC_SdramColunm_9bit;&lt;BR /&gt;sdramconfig.casLatency = kSEMC_LatencyThree;&lt;BR /&gt;sdramconfig.tPrecharge2Act_Ns = 18; /* Trp 18ns */&lt;BR /&gt;sdramconfig.tAct2ReadWrite_Ns = 18; /* Trcd 18ns */&lt;BR /&gt;sdramconfig.tRefreshRecovery_Ns = (60 + 67);&lt;BR /&gt;sdramconfig.tWriteRecovery_Ns = 12; /* 12ns */&lt;BR /&gt;sdramconfig.tCkeOff_Ns =&lt;BR /&gt;42; /* The minimum cycle of SDRAM CLK off state. CKE is off in self refresh at a minimum period tRAS.*/&lt;BR /&gt;sdramconfig.tAct2Prechage_Ns = 42; /* Tras 42ns */&lt;BR /&gt;sdramconfig.tSelfRefRecovery_Ns = 67;&lt;BR /&gt;sdramconfig.tRefresh2Refresh_Ns = 60;&lt;BR /&gt;sdramconfig.tAct2Act_Ns = 60;&lt;BR /&gt;sdramconfig.tPrescalePeriod_Ns = 160 * (1000000000 / clockFrq);&lt;BR /&gt;sdramconfig.refreshPeriod_nsPerRow = 64 * 1000000 / 8192; /* 64ms/8192 */&lt;BR /&gt;sdramconfig.refreshUrgThreshold = sdramconfig.refreshPeriod_nsPerRow;&lt;/P&gt;</description>
      <pubDate>Mon, 02 Aug 2021 15:18:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/imxrt1021-sdram-initialization-parameter/m-p/1316796#M15616</guid>
      <dc:creator>mollygqs</dc:creator>
      <dc:date>2021-08-02T15:18:01Z</dc:date>
    </item>
    <item>
      <title>Re: imxrt1021 sdram initialization parameter</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/imxrt1021-sdram-initialization-parameter/m-p/1317010#M15623</link>
      <description>&lt;P&gt;Hi,&lt;BR /&gt;Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.&lt;BR /&gt;Maybe you can use evkmimxrt1020_semc directly for testing, as the MIMXRT1020 also uses the IS42S16160.&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Tue, 03 Aug 2021 03:17:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/imxrt1021-sdram-initialization-parameter/m-p/1317010#M15623</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2021-08-03T03:17:22Z</dc:date>
    </item>
    <item>
      <title>Re: imxrt1021 sdram initialization parameter</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/imxrt1021-sdram-initialization-parameter/m-p/1317352#M15635</link>
      <description>&lt;P&gt;&lt;SPAN class="tgt highlight"&gt;I used this (\driver_examples\semc) test and it also failed to read the SDRAM without reading any data.&lt;/SPAN&gt;&lt;SPAN class="tgt"&gt; May I ask what other debugging means?&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 03 Aug 2021 12:48:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/imxrt1021-sdram-initialization-parameter/m-p/1317352#M15635</guid>
      <dc:creator>mollygqs</dc:creator>
      <dc:date>2021-08-03T12:48:27Z</dc:date>
    </item>
    <item>
      <title>Re: imxrt1021 sdram initialization parameter</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/imxrt1021-sdram-initialization-parameter/m-p/1317620#M15640</link>
      <description>&lt;P&gt;Hi,&lt;BR /&gt;Thanks for your reply.&lt;BR /&gt;1) May I ask what other debugging means?&lt;BR /&gt;-- From my experience, I'd highly recommend you to check the hardware via reviewing the schematic and using the oscilloscope firstly, especially, on the condition that all custom boards have this kind of issue.&lt;BR /&gt;Next, you can try the tool as the post introduce to do some test for SDRAM.&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Wed, 04 Aug 2021 01:53:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/imxrt1021-sdram-initialization-parameter/m-p/1317620#M15640</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2021-08-04T01:53:42Z</dc:date>
    </item>
  </channel>
</rss>