<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic RT1020 does not debug/ does not connect | 15: target error from Read Memory in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1020-does-not-debug-does-not-connect-15-target-error-from-Read/m-p/1313499#M15486</link>
    <description>&lt;P&gt;I was trying to implement the example powermode driver to my project. When attempting to change the powermode, the dev board hard faulted. Now, the dev board refuses program. Another board does not even connect to the computer anymore. It shows this message on the debug console. I believe the problem comes from changing the clock frequency when there is sdram code implemented. I was wondering how I could make the board program again and how to potentially avoid this problem again. Thank you!&lt;/P&gt;&lt;P&gt;MCUXpresso IDE RedlinkMulti Driver v11.3 (Mar 30 2021 16:50:12 - crt_emu_cm_redlink build 18)&lt;BR /&gt;Found chip XML file in C:/Users/jaeye/Documents/MCUXpressoIDE_11.3.1_5262/workspace/evkmimxrt1020_freertos_hello/Debug\MIMXRT1021xxxxx.xml&lt;BR /&gt;Reconnected to existing LinkServer process.&lt;BR /&gt;============= SCRIPT: RT1020_connect.scp =============&lt;BR /&gt;RT1020 Connect Script&lt;BR /&gt;DpID = 0BD11477&lt;BR /&gt;APID = 0x04770041&lt;BR /&gt;Disabling MPU&lt;BR /&gt;Configure FlexRAM for 128KB OC RAM, 64KB I-TCM, 64KB D-TCM&lt;BR /&gt;Finished&lt;BR /&gt;============= END SCRIPT =============================&lt;BR /&gt;Probe Firmware: DAPLink CMSIS-DAP (ARM)&lt;BR /&gt;Serial Number: 0226000047784e4500299003d917000fe561000097969900&lt;BR /&gt;VID:PID: 0D28:0204&lt;BR /&gt;USB Path: \\?\hid#vid_0d28&amp;amp;pid_0204&amp;amp;mi_03#7&amp;amp;1aee426a&amp;amp;0&amp;amp;0000#{4d1e55b2-f16f-11cf-88cb-001111000030}&lt;BR /&gt;Using memory from core 0 after searching for a good core&lt;BR /&gt;debug interface type = CoreSight DP (DAP DP ID 0BD11477) over SWD TAP 0&lt;BR /&gt;processor type = Cortex-M7 (CPU ID 00000C27) on DAP AP 0&lt;BR /&gt;number of h/w breakpoints = 8&lt;BR /&gt;number of flash patches = 0&lt;BR /&gt;number of h/w watchpoints = 4&lt;BR /&gt;Probe(0): Connected&amp;amp;Reset. DpID: 0BD11477. CpuID: 00000C27. Info: &amp;lt;None&amp;gt;&lt;BR /&gt;Debug protocol: SWD. RTCK: Disabled. Vector catch: Disabled.&lt;BR /&gt;Content of CoreSight Debug ROM(s):&lt;BR /&gt;RBASE E00FD000: CID B105100D PID 000008E88C ROM (type 0x1)&lt;BR /&gt;ROM 1 E00FE000: CID B105100D PID 04000BB4C8 ROM (type 0x1)&lt;BR /&gt;ROM 2 E00FF000: CID B105100D PID 04000BB4C7 ROM (type 0x1)&lt;BR /&gt;ROM 3 E000E000: CID B105E00D PID 04000BB00C Gen SCS (type 0x0)&lt;BR /&gt;ROM 3 E0001000: CID B105E00D PID 04000BB002 Gen DWT (type 0x0)&lt;BR /&gt;ROM 3 E0002000: CID B105E00D PID 04000BB00E Gen (type 0x0)&lt;BR /&gt;ROM 3 E0000000: CID B105E00D PID 04000BB001 Gen ITM (type 0x0)&lt;BR /&gt;ROM 2 E0041000: CID B105900D PID 04001BB975 CSt ARM ETMv4.0 type 0x13 Trace Source - Core&lt;BR /&gt;ROM 2 E0042000: CID B105900D PID 04004BB906 CSt type 0x14 Debug Control - Trigger, e.g. ECT&lt;BR /&gt;ROM 1 E0040000: CID B105900D PID 04000BB9A9 CSt type 0x11 Trace Sink - TPIU&lt;BR /&gt;ROM 1 E0043000: CID B105F00D PID 04001BB101 Sys (type 0x0)&lt;BR /&gt;NXP: MIMXRT1021xxxxx&lt;BR /&gt;DAP stride is 1024 bytes (256 words)&lt;BR /&gt;XML Error - no license-type XML file 'crt_common.xme' on path.&lt;BR /&gt;note - part information contained no product license-type data&lt;BR /&gt;Inspected v.2 External Flash Device on SPI MIMXRT1020-EVK_IS25LP064.cfx&lt;BR /&gt;Image 'MIMXRT1020-EVK_IS25LP064A Mar 22 2021 08:15:06'&lt;BR /&gt;Connected: was_reset=false. was_stopped=true&lt;BR /&gt;Awaiting telnet connection to port 3331 ...&lt;BR /&gt;GDB nonstop mode disabled (using allstop mode)&lt;BR /&gt;After error Nn(05). Wire ACK Wait in DAP access -&lt;BR /&gt;Failed to read address register in DAP - Nn(05). Wire ACK Wait in DAP access&lt;BR /&gt;Target error from Read Memory: Em(17). Debug port inaccessible after access at location 0x60006A60&lt;BR /&gt;FreeRTOS stack backtrace is enabled&lt;BR /&gt;Opening flash driver MIMXRT1020-EVK_IS25LP064.cfx&lt;BR /&gt;Target error from Commit Flash write: Nn(05). Wire ACK Wait in DAP access&lt;BR /&gt;GDB stub (crt_emu_cm_redlink) terminating - GDB protocol problem: Pipe has been closed by GDB.&lt;BR /&gt;state - running or following reset request - re-read of state failed - rc Nn(05). Wire ACK Wait in DAP access&lt;/P&gt;</description>
    <pubDate>Tue, 27 Jul 2021 02:34:55 GMT</pubDate>
    <dc:creator>VolcanicCheese</dc:creator>
    <dc:date>2021-07-27T02:34:55Z</dc:date>
    <item>
      <title>RT1020 does not debug/ does not connect | 15: target error from Read Memory</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1020-does-not-debug-does-not-connect-15-target-error-from-Read/m-p/1313499#M15486</link>
      <description>&lt;P&gt;I was trying to implement the example powermode driver to my project. When attempting to change the powermode, the dev board hard faulted. Now, the dev board refuses program. Another board does not even connect to the computer anymore. It shows this message on the debug console. I believe the problem comes from changing the clock frequency when there is sdram code implemented. I was wondering how I could make the board program again and how to potentially avoid this problem again. Thank you!&lt;/P&gt;&lt;P&gt;MCUXpresso IDE RedlinkMulti Driver v11.3 (Mar 30 2021 16:50:12 - crt_emu_cm_redlink build 18)&lt;BR /&gt;Found chip XML file in C:/Users/jaeye/Documents/MCUXpressoIDE_11.3.1_5262/workspace/evkmimxrt1020_freertos_hello/Debug\MIMXRT1021xxxxx.xml&lt;BR /&gt;Reconnected to existing LinkServer process.&lt;BR /&gt;============= SCRIPT: RT1020_connect.scp =============&lt;BR /&gt;RT1020 Connect Script&lt;BR /&gt;DpID = 0BD11477&lt;BR /&gt;APID = 0x04770041&lt;BR /&gt;Disabling MPU&lt;BR /&gt;Configure FlexRAM for 128KB OC RAM, 64KB I-TCM, 64KB D-TCM&lt;BR /&gt;Finished&lt;BR /&gt;============= END SCRIPT =============================&lt;BR /&gt;Probe Firmware: DAPLink CMSIS-DAP (ARM)&lt;BR /&gt;Serial Number: 0226000047784e4500299003d917000fe561000097969900&lt;BR /&gt;VID:PID: 0D28:0204&lt;BR /&gt;USB Path: \\?\hid#vid_0d28&amp;amp;pid_0204&amp;amp;mi_03#7&amp;amp;1aee426a&amp;amp;0&amp;amp;0000#{4d1e55b2-f16f-11cf-88cb-001111000030}&lt;BR /&gt;Using memory from core 0 after searching for a good core&lt;BR /&gt;debug interface type = CoreSight DP (DAP DP ID 0BD11477) over SWD TAP 0&lt;BR /&gt;processor type = Cortex-M7 (CPU ID 00000C27) on DAP AP 0&lt;BR /&gt;number of h/w breakpoints = 8&lt;BR /&gt;number of flash patches = 0&lt;BR /&gt;number of h/w watchpoints = 4&lt;BR /&gt;Probe(0): Connected&amp;amp;Reset. DpID: 0BD11477. CpuID: 00000C27. Info: &amp;lt;None&amp;gt;&lt;BR /&gt;Debug protocol: SWD. RTCK: Disabled. Vector catch: Disabled.&lt;BR /&gt;Content of CoreSight Debug ROM(s):&lt;BR /&gt;RBASE E00FD000: CID B105100D PID 000008E88C ROM (type 0x1)&lt;BR /&gt;ROM 1 E00FE000: CID B105100D PID 04000BB4C8 ROM (type 0x1)&lt;BR /&gt;ROM 2 E00FF000: CID B105100D PID 04000BB4C7 ROM (type 0x1)&lt;BR /&gt;ROM 3 E000E000: CID B105E00D PID 04000BB00C Gen SCS (type 0x0)&lt;BR /&gt;ROM 3 E0001000: CID B105E00D PID 04000BB002 Gen DWT (type 0x0)&lt;BR /&gt;ROM 3 E0002000: CID B105E00D PID 04000BB00E Gen (type 0x0)&lt;BR /&gt;ROM 3 E0000000: CID B105E00D PID 04000BB001 Gen ITM (type 0x0)&lt;BR /&gt;ROM 2 E0041000: CID B105900D PID 04001BB975 CSt ARM ETMv4.0 type 0x13 Trace Source - Core&lt;BR /&gt;ROM 2 E0042000: CID B105900D PID 04004BB906 CSt type 0x14 Debug Control - Trigger, e.g. ECT&lt;BR /&gt;ROM 1 E0040000: CID B105900D PID 04000BB9A9 CSt type 0x11 Trace Sink - TPIU&lt;BR /&gt;ROM 1 E0043000: CID B105F00D PID 04001BB101 Sys (type 0x0)&lt;BR /&gt;NXP: MIMXRT1021xxxxx&lt;BR /&gt;DAP stride is 1024 bytes (256 words)&lt;BR /&gt;XML Error - no license-type XML file 'crt_common.xme' on path.&lt;BR /&gt;note - part information contained no product license-type data&lt;BR /&gt;Inspected v.2 External Flash Device on SPI MIMXRT1020-EVK_IS25LP064.cfx&lt;BR /&gt;Image 'MIMXRT1020-EVK_IS25LP064A Mar 22 2021 08:15:06'&lt;BR /&gt;Connected: was_reset=false. was_stopped=true&lt;BR /&gt;Awaiting telnet connection to port 3331 ...&lt;BR /&gt;GDB nonstop mode disabled (using allstop mode)&lt;BR /&gt;After error Nn(05). Wire ACK Wait in DAP access -&lt;BR /&gt;Failed to read address register in DAP - Nn(05). Wire ACK Wait in DAP access&lt;BR /&gt;Target error from Read Memory: Em(17). Debug port inaccessible after access at location 0x60006A60&lt;BR /&gt;FreeRTOS stack backtrace is enabled&lt;BR /&gt;Opening flash driver MIMXRT1020-EVK_IS25LP064.cfx&lt;BR /&gt;Target error from Commit Flash write: Nn(05). Wire ACK Wait in DAP access&lt;BR /&gt;GDB stub (crt_emu_cm_redlink) terminating - GDB protocol problem: Pipe has been closed by GDB.&lt;BR /&gt;state - running or following reset request - re-read of state failed - rc Nn(05). Wire ACK Wait in DAP access&lt;/P&gt;</description>
      <pubDate>Tue, 27 Jul 2021 02:34:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1020-does-not-debug-does-not-connect-15-target-error-from-Read/m-p/1313499#M15486</guid>
      <dc:creator>VolcanicCheese</dc:creator>
      <dc:date>2021-07-27T02:34:55Z</dc:date>
    </item>
    <item>
      <title>Re: RT1020 does not debug/ does not connect | 15: target error from Read Memory</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1020-does-not-debug-does-not-connect-15-target-error-from-Read/m-p/1313637#M15494</link>
      <description>&lt;P&gt;Hi,&lt;BR /&gt;Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.&lt;BR /&gt;Firstly, I'd like to know which board you tested, next, please follow the below steps to restore the board.&lt;BR /&gt;&amp;nbsp;1) Configure the board to Serial Downloader mode.&lt;BR /&gt;&amp;nbsp;2) Power on the board, debug the demo project.&lt;BR /&gt;&amp;nbsp;3) After that, power off and recover the board to the original mode, then power on again.&lt;BR /&gt;&amp;nbsp;4) Give a debug again.&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Tue, 27 Jul 2021 06:40:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1020-does-not-debug-does-not-connect-15-target-error-from-Read/m-p/1313637#M15494</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2021-07-27T06:40:37Z</dc:date>
    </item>
    <item>
      <title>Re: RT1020 does not debug/ does not connect | 15: target error from Read Memory</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1020-does-not-debug-does-not-connect-15-target-error-from-Read/m-p/1313926#M15500</link>
      <description>&lt;P&gt;I am using the&amp;nbsp;MIMXRT1020-EVK board. How do I configure the board to Serial Downloader mode? Also, would this solution work on board that does not seem to power-up when connecting with a micro USB. Thank you! I appreciate all the help given.&lt;/P&gt;</description>
      <pubDate>Tue, 27 Jul 2021 13:25:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1020-does-not-debug-does-not-connect-15-target-error-from-Read/m-p/1313926#M15500</guid>
      <dc:creator>VolcanicCheese</dc:creator>
      <dc:date>2021-07-27T13:25:17Z</dc:date>
    </item>
    <item>
      <title>Re: RT1020 does not debug/ does not connect | 15: target error from Read Memory</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1020-does-not-debug-does-not-connect-15-target-error-from-Read/m-p/1314176#M15508</link>
      <description>&lt;P&gt;Hi,&lt;BR /&gt;Thanks for your reply.&lt;BR /&gt;1) How do I configure the board to Serial Downloader mode? &lt;BR /&gt;-- Please refer to the &lt;A href="https://www.mouser.com/pdfdocs/NXP_MIMXRT1020-EVK_UG.pdf" target="_self"&gt;MIMXRT1020 EVK Board Hardware User's Guide&lt;/A&gt;.&lt;BR /&gt;2) would this solution work on board that does not seem to power-up when connecting with a micro USB. &lt;BR /&gt;-- Whether you mean the board can't power-up yet now, if yes, you'd better check the power supply setting of the MIMXRT1020 EVK Board and the above guide also introduce the information.&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Wed, 28 Jul 2021 02:28:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1020-does-not-debug-does-not-connect-15-target-error-from-Read/m-p/1314176#M15508</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2021-07-28T02:28:03Z</dc:date>
    </item>
  </channel>
</rss>