<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Use usb host port on MXRT1050-evk in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Use-usb-host-port-on-MXRT1050-evk/m-p/833584#M1536</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jeremy,&lt;/P&gt;&lt;P&gt;Thanks for the reply. Your solution works perfectly.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 08 Jan 2019 09:59:18 GMT</pubDate>
    <dc:creator>poneponecar</dc:creator>
    <dc:date>2019-01-08T09:59:18Z</dc:date>
    <item>
      <title>Use usb host port on MXRT1050-evk</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Use-usb-host-port-on-MXRT1050-evk/m-p/833582#M1534</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;There are two usb ports available on the MXRT1050-EVK, J9 is the OTG port, and J10 is the usb host port according to the EVK user guide.&lt;/P&gt;&lt;P&gt;The usb examples provided in the SDK, even the usb host example, for example, the host_cdc_bm, all use the J9, i.e. the OTG port.&lt;/P&gt;&lt;P&gt;How could I modify the examples to use J10 as to connect to my own USB device?&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Dec 2018 11:45:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Use-usb-host-port-on-MXRT1050-evk/m-p/833582#M1534</guid>
      <dc:creator>poneponecar</dc:creator>
      <dc:date>2018-12-26T11:45:07Z</dc:date>
    </item>
    <item>
      <title>Re: Use usb host port on MXRT1050-evk</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Use-usb-host-port-on-MXRT1050-evk/m-p/833583#M1535</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A _jive_internal="true" data-content-finding="Community" data-userid="324800" data-username="poneponecar" href="https://community.nxp.com/people/poneponecar"&gt;Jay Yeh&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.&lt;BR /&gt;To select alternative CONTROLLER ID: &lt;EM&gt;&lt;STRONG&gt;kUSB_ControllerEhci1&lt;/STRONG&gt;&lt;/EM&gt;.&lt;/P&gt;&lt;P&gt;Please give a try.&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 03 Jan 2019 09:20:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Use-usb-host-port-on-MXRT1050-evk/m-p/833583#M1535</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2019-01-03T09:20:08Z</dc:date>
    </item>
    <item>
      <title>Re: Use usb host port on MXRT1050-evk</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Use-usb-host-port-on-MXRT1050-evk/m-p/833584#M1536</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jeremy,&lt;/P&gt;&lt;P&gt;Thanks for the reply. Your solution works perfectly.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 08 Jan 2019 09:59:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Use-usb-host-port-on-MXRT1050-evk/m-p/833584#M1536</guid>
      <dc:creator>poneponecar</dc:creator>
      <dc:date>2019-01-08T09:59:18Z</dc:date>
    </item>
    <item>
      <title>Re: Use usb host port on MXRT1050-evk</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Use-usb-host-port-on-MXRT1050-evk/m-p/833585#M1537</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/jeremyzhou"&gt;jeremyzhou&lt;/A&gt;‌&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In both the source code and the USB stack documentation, the following comment exists:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;/*!&amp;lt; EHCI 1U, Currently, there are no platforms which have two EHCI IPs, this is reserved&lt;BR /&gt; to be used in the future. */&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I assume that this comment is out of date and that the RT1050 does use both&amp;nbsp;kUSB_ControllerEhci0 and&amp;nbsp;kUSB_ControllerEhci1. The comment and documentation should be updated to reflect this.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Aug 2019 14:56:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Use-usb-host-port-on-MXRT1050-evk/m-p/833585#M1537</guid>
      <dc:creator>amwilhite</dc:creator>
      <dc:date>2019-08-29T14:56:54Z</dc:date>
    </item>
  </channel>
</rss>