<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX RT Crossover MCUsのトピックRe: RT101x LPSPI API Master Blocking Transfer No SDI Signal</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT101x-LPSPI-API-Master-Blocking-Transfer-No-SDI-Signal/m-p/1308087#M15290</link>
    <description>&lt;P&gt;Hi,&lt;BR /&gt;Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.&lt;BR /&gt;For the SPI master device, the SDI pin is a MISO pin of the SPI interface, it doesn't have signals otherwise, the slave device transfers the data to the master device.&lt;BR /&gt;Hope this is clear.&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
    <pubDate>Thu, 15 Jul 2021 03:17:52 GMT</pubDate>
    <dc:creator>jeremyzhou</dc:creator>
    <dc:date>2021-07-15T03:17:52Z</dc:date>
    <item>
      <title>RT101x LPSPI API Master Blocking Transfer No SDI Signal</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT101x-LPSPI-API-Master-Blocking-Transfer-No-SDI-Signal/m-p/1307995#M15285</link>
      <description>&lt;P&gt;On a custom RT1011 platform I am trying to bring up some SPI peripherals, but I see no signal on the SDI pin configured in the pin mux tool. I do see the SPI clock signal on the scope from its configured pin with the expected number of cycles as the number of bits I am writing.&lt;/P&gt;&lt;P&gt;I am using the LPSPI1 peripheral, SCK on GPIO_AD_06, SDI on GPIO_AD_03, SDO on GPIO_AD_04, CS not used, LPSPI API Master Blocking Transfer. What am I missing here?&lt;/P&gt;</description>
      <pubDate>Wed, 14 Jul 2021 23:25:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT101x-LPSPI-API-Master-Blocking-Transfer-No-SDI-Signal/m-p/1307995#M15285</guid>
      <dc:creator>vishayp</dc:creator>
      <dc:date>2021-07-14T23:25:06Z</dc:date>
    </item>
    <item>
      <title>Re: RT101x LPSPI API Master Blocking Transfer No SDI Signal</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT101x-LPSPI-API-Master-Blocking-Transfer-No-SDI-Signal/m-p/1308087#M15290</link>
      <description>&lt;P&gt;Hi,&lt;BR /&gt;Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.&lt;BR /&gt;For the SPI master device, the SDI pin is a MISO pin of the SPI interface, it doesn't have signals otherwise, the slave device transfers the data to the master device.&lt;BR /&gt;Hope this is clear.&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Thu, 15 Jul 2021 03:17:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT101x-LPSPI-API-Master-Blocking-Transfer-No-SDI-Signal/m-p/1308087#M15290</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2021-07-15T03:17:52Z</dc:date>
    </item>
  </channel>
</rss>