<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Ethernet based camera interfacing in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Ethernet-based-camera-interfacing/m-p/1307973#M15280</link>
    <description>&lt;P&gt;Hello Jagadeesh,&lt;/P&gt;
&lt;P&gt;You should be able to receive the IP camera stream on the i.MXRT1170. There is not an example with the IP Camera implementation per se. However, the i.MXRT1170 SDK have some Ethernet and lwip examples, which may help as a starting point.&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Gustavo&lt;/P&gt;</description>
    <pubDate>Wed, 14 Jul 2021 22:03:29 GMT</pubDate>
    <dc:creator>gusarambula</dc:creator>
    <dc:date>2021-07-14T22:03:29Z</dc:date>
    <item>
      <title>Ethernet based camera interfacing</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Ethernet-based-camera-interfacing/m-p/1306992#M15258</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Can we interface the IP camera in RT1170&amp;nbsp; EVK via ethernet.&lt;/P&gt;&lt;P&gt;Please Guide us.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Jagadeesh&lt;/P&gt;</description>
      <pubDate>Tue, 13 Jul 2021 13:23:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Ethernet-based-camera-interfacing/m-p/1306992#M15258</guid>
      <dc:creator>jagadeesh_11</dc:creator>
      <dc:date>2021-07-13T13:23:24Z</dc:date>
    </item>
    <item>
      <title>Re: Ethernet based camera interfacing</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Ethernet-based-camera-interfacing/m-p/1307973#M15280</link>
      <description>&lt;P&gt;Hello Jagadeesh,&lt;/P&gt;
&lt;P&gt;You should be able to receive the IP camera stream on the i.MXRT1170. There is not an example with the IP Camera implementation per se. However, the i.MXRT1170 SDK have some Ethernet and lwip examples, which may help as a starting point.&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Gustavo&lt;/P&gt;</description>
      <pubDate>Wed, 14 Jul 2021 22:03:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Ethernet-based-camera-interfacing/m-p/1307973#M15280</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2021-07-14T22:03:29Z</dc:date>
    </item>
  </channel>
</rss>