<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX RT Crossover MCUsのトピックProblem with RT1064 USB and sdphost</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Problem-with-RT1064-USB-and-sdphost/m-p/1307369#M15270</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am trying to program the MIMXRT1064 over USB interface using the sdphost utility. The chip is blank and hence is expected to enter the serial downloader mode.&lt;/P&gt;&lt;P&gt;When connected over USB the chip appears as a HID device with VID,PID 0x1fc9,0x0135. But if I try to communicate with it using spdhost utility, all commands are failing giving error response&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&lt;STRONG&gt;GetOverlappedResult failed with error 31: A device attached to the system is not functioning.&lt;/STRONG&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&lt;STRONG&gt;SDPFileDataProducer.writePacket error 1&lt;/STRONG&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;The command &lt;STRONG&gt;sdphost.exe -t 50000 -u 0x1fc9,0x0135 -V -d -- error-status&amp;nbsp;&lt;/STRONG&gt;fails with response&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&lt;STRONG&gt;Status (HAB mode) = 1450735702 (0x56787856) HAB disabled.&lt;/STRONG&gt;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;&lt;STRONG&gt;Reponse Status = 858993459 (0x33333333) HAB failure.&lt;/STRONG&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;Can someone please help with this error? I am not understanding if the chip has entered serial downloader mode or if there is an issue with the USB communication. Our production programming has been stalled due to this issue.&lt;/P&gt;&lt;P&gt;P.S: We tried with the NXPBootUtility as well but we get the same errors.&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;P&gt;Mayuresh&lt;/P&gt;</description>
    <pubDate>Wed, 14 Jul 2021 05:40:44 GMT</pubDate>
    <dc:creator>mayureshmanjrek</dc:creator>
    <dc:date>2021-07-14T05:40:44Z</dc:date>
    <item>
      <title>Problem with RT1064 USB and sdphost</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Problem-with-RT1064-USB-and-sdphost/m-p/1307369#M15270</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am trying to program the MIMXRT1064 over USB interface using the sdphost utility. The chip is blank and hence is expected to enter the serial downloader mode.&lt;/P&gt;&lt;P&gt;When connected over USB the chip appears as a HID device with VID,PID 0x1fc9,0x0135. But if I try to communicate with it using spdhost utility, all commands are failing giving error response&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&lt;STRONG&gt;GetOverlappedResult failed with error 31: A device attached to the system is not functioning.&lt;/STRONG&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&lt;STRONG&gt;SDPFileDataProducer.writePacket error 1&lt;/STRONG&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;The command &lt;STRONG&gt;sdphost.exe -t 50000 -u 0x1fc9,0x0135 -V -d -- error-status&amp;nbsp;&lt;/STRONG&gt;fails with response&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&lt;STRONG&gt;Status (HAB mode) = 1450735702 (0x56787856) HAB disabled.&lt;/STRONG&gt;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;&lt;STRONG&gt;Reponse Status = 858993459 (0x33333333) HAB failure.&lt;/STRONG&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;Can someone please help with this error? I am not understanding if the chip has entered serial downloader mode or if there is an issue with the USB communication. Our production programming has been stalled due to this issue.&lt;/P&gt;&lt;P&gt;P.S: We tried with the NXPBootUtility as well but we get the same errors.&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;P&gt;Mayuresh&lt;/P&gt;</description>
      <pubDate>Wed, 14 Jul 2021 05:40:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Problem-with-RT1064-USB-and-sdphost/m-p/1307369#M15270</guid>
      <dc:creator>mayureshmanjrek</dc:creator>
      <dc:date>2021-07-14T05:40:44Z</dc:date>
    </item>
  </channel>
</rss>