<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX RT Crossover MCUsのトピック9-bit uart MDB protocol</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/9-bit-uart-MDB-protocol/m-p/1307117#M15265</link>
    <description>&lt;P&gt;We currently have a system which is controlling an MDB bus and we are investigating if we can move to NXP chips. Everything is looking great, the only thing I can't seem to find is whether 9bit uart works "out of the box". I've read [&lt;A href="https://community.nxp.com/t5/i-MX-Processors/IMX6-UART-9-bit-MDB-protocol/m-p/827362" target="_self"&gt;link&lt;/A&gt;], [&lt;A href="https://community.nxp.com/t5/i-MX-Processors/Receiving-UART-data-in-9-bit-RS-485-mode/m-p/643589" target="_self"&gt;link&lt;/A&gt;] and [&lt;A href="https://community.nxp.com/t5/i-MX-Processors/Some-experiences-with-iMX-6-9-bit-UART-mode/m-p/711522" target="_self"&gt;link&lt;/A&gt;] but these concern the imx6 series and I am still not 100% sure whether it will work on i.MXRT102x without having to bit bang anything.&lt;/P&gt;&lt;P&gt;Does the NXP chip support 9bit uart on hardware level?&lt;/P&gt;</description>
    <pubDate>Tue, 13 Jul 2021 17:27:22 GMT</pubDate>
    <dc:creator>BvLeeuwen</dc:creator>
    <dc:date>2021-07-13T17:27:22Z</dc:date>
    <item>
      <title>9-bit uart MDB protocol</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/9-bit-uart-MDB-protocol/m-p/1307117#M15265</link>
      <description>&lt;P&gt;We currently have a system which is controlling an MDB bus and we are investigating if we can move to NXP chips. Everything is looking great, the only thing I can't seem to find is whether 9bit uart works "out of the box". I've read [&lt;A href="https://community.nxp.com/t5/i-MX-Processors/IMX6-UART-9-bit-MDB-protocol/m-p/827362" target="_self"&gt;link&lt;/A&gt;], [&lt;A href="https://community.nxp.com/t5/i-MX-Processors/Receiving-UART-data-in-9-bit-RS-485-mode/m-p/643589" target="_self"&gt;link&lt;/A&gt;] and [&lt;A href="https://community.nxp.com/t5/i-MX-Processors/Some-experiences-with-iMX-6-9-bit-UART-mode/m-p/711522" target="_self"&gt;link&lt;/A&gt;] but these concern the imx6 series and I am still not 100% sure whether it will work on i.MXRT102x without having to bit bang anything.&lt;/P&gt;&lt;P&gt;Does the NXP chip support 9bit uart on hardware level?&lt;/P&gt;</description>
      <pubDate>Tue, 13 Jul 2021 17:27:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/9-bit-uart-MDB-protocol/m-p/1307117#M15265</guid>
      <dc:creator>BvLeeuwen</dc:creator>
      <dc:date>2021-07-13T17:27:22Z</dc:date>
    </item>
    <item>
      <title>Re: 9-bit uart MDB protocol</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/9-bit-uart-MDB-protocol/m-p/1307992#M15283</link>
      <description>&lt;P&gt;Hello,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The LPUART of the RT1020 family has the following feature: programmable&amp;nbsp;7-bit, 8-bit, 9-bit, or 10-bit character length. For more information regarding this, refer to section 44.3.6.1 of the RT1020 reference manual.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Victor&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 14 Jul 2021 23:07:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/9-bit-uart-MDB-protocol/m-p/1307992#M15283</guid>
      <dc:creator>victorjimenez</dc:creator>
      <dc:date>2021-07-14T23:07:11Z</dc:date>
    </item>
  </channel>
</rss>