<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic RT1050 with external 16-bit low power SDRAM in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1050-with-external-16-bit-low-power-SDRAM/m-p/832966#M1507</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have configured the RT1050 to use the SEMC to interface to a external 16-bit SDRAM. The SDRAM is a Winbond 512Mb Low Power SDRAM (W989D6DB) operating at 1.8V power supply.&lt;/P&gt;&lt;P&gt;The SDRAM works fine most at the time, but some times it happens that the memory access fails after power up sequence. Does any one have a idea what can cause this problem?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 04 Dec 2018 16:37:49 GMT</pubDate>
    <dc:creator>matthiaspimming</dc:creator>
    <dc:date>2018-12-04T16:37:49Z</dc:date>
    <item>
      <title>RT1050 with external 16-bit low power SDRAM</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1050-with-external-16-bit-low-power-SDRAM/m-p/832966#M1507</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have configured the RT1050 to use the SEMC to interface to a external 16-bit SDRAM. The SDRAM is a Winbond 512Mb Low Power SDRAM (W989D6DB) operating at 1.8V power supply.&lt;/P&gt;&lt;P&gt;The SDRAM works fine most at the time, but some times it happens that the memory access fails after power up sequence. Does any one have a idea what can cause this problem?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 04 Dec 2018 16:37:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1050-with-external-16-bit-low-power-SDRAM/m-p/832966#M1507</guid>
      <dc:creator>matthiaspimming</dc:creator>
      <dc:date>2018-12-04T16:37:49Z</dc:date>
    </item>
    <item>
      <title>Re: RT1050 with external 16-bit low power SDRAM</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1050-with-external-16-bit-low-power-SDRAM/m-p/832967#M1508</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; I think, it makes sense to discuss memory (power up) initialization sequence&lt;/P&gt;&lt;P&gt;with memory manufacturer directly. I do not see such specs in their Datasheet.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.winbond.com/resource-files/w989dxdb_pkg_datasheet_a01-002_20161201.pdf" title="https://www.winbond.com/resource-files/w989dxdb_pkg_datasheet_a01-002_20161201.pdf"&gt;https://www.winbond.com/resource-files/w989dxdb_pkg_datasheet_a01-002_20161201.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Dec 2018 06:04:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1050-with-external-16-bit-low-power-SDRAM/m-p/832967#M1508</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2018-12-06T06:04:15Z</dc:date>
    </item>
  </channel>
</rss>