<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX RT Crossover MCUsのトピックRe: RT1050 Rom Boot loader devices connections</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1050-Rom-Boot-loader-devices-connections/m-p/716916#M15</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Carlos_Musich: Thank you for help and promise for more info.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 23 Mar 2018 21:12:02 GMT</pubDate>
    <dc:creator>jamesli</dc:creator>
    <dc:date>2018-03-23T21:12:02Z</dc:date>
    <item>
      <title>RT1050 Rom Boot loader devices connections</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1050-Rom-Boot-loader-devices-connections/m-p/716914#M13</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;On the latest data sheet, when boot loader from UART1, Table 79 show 4 pins are used,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/36838i59C9636DE7B3CD66/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;But on reference manual table 8-1 as follows:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_2.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/36744iBA047CE8B73E751C/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Only two pins are needed. Which one I should to use, if the UART1 port does not use CTS and RTS signals, is boot loader still to talk the device? Where I can find more information regarding the ROM bootloader?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When boot&amp;nbsp;from FlexSPI, it lists a hyper flash as follows:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_3.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/36839iCB22E65389FEB35D/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_3.png" alt="pastedImage_3.png" /&gt;&lt;/span&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is the ROM boot loader works with QSPI flash on FLEXSPI_A or FLEXSPI_B port, if yes, how it behaviors? Which IC is selected first? FLEXSPI_A_SS0_B or&amp;nbsp;&amp;nbsp;&lt;SPAN&gt;FLEXSPI_B_SS0_B? What is required connections?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Any&amp;nbsp; help is appreciated! Thank you in advance!&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 20 Mar 2018 14:40:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1050-Rom-Boot-loader-devices-connections/m-p/716914#M13</guid>
      <dc:creator>jamesli</dc:creator>
      <dc:date>2018-03-20T14:40:57Z</dc:date>
    </item>
    <item>
      <title>Re: RT1050 Rom Boot loader devices connections</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1050-Rom-Boot-loader-devices-connections/m-p/716915#M14</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jian Li,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The ROM bootloader supports&amp;nbsp;booting through UART with RX/TX only (no hardware flow control). Additionally, I do not know of any other documents with deep information&amp;nbsp;on the ROM bootloader, but I will ask around and let you know if I find something useful. For instance you can take a look here:&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/docs/en/application-note/AN12107.pdf" title="https://www.nxp.com/docs/en/application-note/AN12107.pdf"&gt;https://www.nxp.com/docs/en/application-note/AN12107.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Regards,&lt;BR /&gt;Carlos&lt;BR /&gt;NXP Technical Support&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 23 Mar 2018 20:27:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1050-Rom-Boot-loader-devices-connections/m-p/716915#M14</guid>
      <dc:creator>Carlos_Musich</dc:creator>
      <dc:date>2018-03-23T20:27:16Z</dc:date>
    </item>
    <item>
      <title>Re: RT1050 Rom Boot loader devices connections</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1050-Rom-Boot-loader-devices-connections/m-p/716916#M15</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Carlos_Musich: Thank you for help and promise for more info.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 23 Mar 2018 21:12:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1050-Rom-Boot-loader-devices-connections/m-p/716916#M15</guid>
      <dc:creator>jamesli</dc:creator>
      <dc:date>2018-03-23T21:12:02Z</dc:date>
    </item>
  </channel>
</rss>