<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Query related to Power consumption is DMA in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Query-related-to-Power-consumption-is-DMA/m-p/1299213#M14974</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;We are using NXP i.MX RT 1052 controller.&lt;/P&gt;&lt;P&gt;We already know that DMA is used for parallel processing and to improve overall processor performance.&lt;/P&gt;&lt;P&gt;But, we are trying to understand whether DMA can be used to minimize current consumption or not.&lt;/P&gt;&lt;P&gt;My question is as below -&lt;/P&gt;&lt;P&gt;Consider the below 2 cases,&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;SPI DMA is used to transfer SPI data between memory and SPI transfer registers, CPU(Cortex M7 core) is in sleep mode.&lt;/LI&gt;&lt;LI&gt;Normal SPI is used (SPI DMA is not enabled) to transfer the same amount of data between memory and SPI transfer registers using CPU.&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;For these 2 cases, in which case, the current consumption will be more?&lt;/P&gt;&lt;P&gt;Also, please provide if any analytical document is available for this.&lt;/P&gt;</description>
    <pubDate>Mon, 28 Jun 2021 16:55:35 GMT</pubDate>
    <dc:creator>suhel_mulla</dc:creator>
    <dc:date>2021-06-28T16:55:35Z</dc:date>
    <item>
      <title>Query related to Power consumption is DMA</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Query-related-to-Power-consumption-is-DMA/m-p/1299213#M14974</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;We are using NXP i.MX RT 1052 controller.&lt;/P&gt;&lt;P&gt;We already know that DMA is used for parallel processing and to improve overall processor performance.&lt;/P&gt;&lt;P&gt;But, we are trying to understand whether DMA can be used to minimize current consumption or not.&lt;/P&gt;&lt;P&gt;My question is as below -&lt;/P&gt;&lt;P&gt;Consider the below 2 cases,&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;SPI DMA is used to transfer SPI data between memory and SPI transfer registers, CPU(Cortex M7 core) is in sleep mode.&lt;/LI&gt;&lt;LI&gt;Normal SPI is used (SPI DMA is not enabled) to transfer the same amount of data between memory and SPI transfer registers using CPU.&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;For these 2 cases, in which case, the current consumption will be more?&lt;/P&gt;&lt;P&gt;Also, please provide if any analytical document is available for this.&lt;/P&gt;</description>
      <pubDate>Mon, 28 Jun 2021 16:55:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Query-related-to-Power-consumption-is-DMA/m-p/1299213#M14974</guid>
      <dc:creator>suhel_mulla</dc:creator>
      <dc:date>2021-06-28T16:55:35Z</dc:date>
    </item>
    <item>
      <title>Re: Query related to Power consumption is DMA</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Query-related-to-Power-consumption-is-DMA/m-p/1299439#M14984</link>
      <description>&lt;P&gt;Hi,&lt;BR /&gt;Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.&lt;BR /&gt;1) My question is as below -&lt;BR /&gt;Consider the below 2 cases,&lt;BR /&gt;SPI DMA is used to transfer SPI data between memory and SPI transfer registers, CPU(Cortex M7 core) is in sleep mode.&lt;BR /&gt;Normal SPI is used (SPI DMA is not enabled) to transfer the same amount of data between memory and SPI transfer registers using the CPU.&lt;BR /&gt;For these 2 cases, in which case, the current consumption will be more?&lt;BR /&gt;-- Case 2 will cost more power consumption.&lt;BR /&gt;And there's an &lt;A href="https://www.cypress.com/file/103546/download" target="_self"&gt;article&lt;/A&gt; that explains the DMA's advantage and hopes it can help you.&lt;/P&gt;
&lt;P&gt;Hope it helps.&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 29 Jun 2021 06:10:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Query-related-to-Power-consumption-is-DMA/m-p/1299439#M14984</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2021-06-29T06:10:57Z</dc:date>
    </item>
    <item>
      <title>Re: Query related to Power consumption is DMA</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Query-related-to-Power-consumption-is-DMA/m-p/1299443#M14985</link>
      <description>&lt;P&gt;Thanks for the answer.&lt;/P&gt;&lt;P&gt;Can you share link of the article which explains it?&lt;/P&gt;</description>
      <pubDate>Tue, 29 Jun 2021 06:10:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Query-related-to-Power-consumption-is-DMA/m-p/1299443#M14985</guid>
      <dc:creator>suhel_mulla</dc:creator>
      <dc:date>2021-06-29T06:10:24Z</dc:date>
    </item>
    <item>
      <title>Re: Query related to Power consumption is DMA</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Query-related-to-Power-consumption-is-DMA/m-p/1299456#M14986</link>
      <description>&lt;P&gt;Thanks for the answer and sharing the article. It will solve my query.&lt;/P&gt;</description>
      <pubDate>Tue, 29 Jun 2021 06:28:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Query-related-to-Power-consumption-is-DMA/m-p/1299456#M14986</guid>
      <dc:creator>suhel_mulla</dc:creator>
      <dc:date>2021-06-29T06:28:40Z</dc:date>
    </item>
  </channel>
</rss>