<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX RT Crossover MCUsのトピックRe: LED Brightness control with PWM</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/LED-Brightness-control-with-PWM/m-p/1297078#M14882</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;Within the SDK for the RT1050-EVKB you will find a PWM example. This is a good starting point for your application. If you want to see the PWM through an LED, you have two options:&amp;nbsp;&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;Connect an external LED to one of the PWM outputs of the example.&amp;nbsp;&lt;/LI&gt;
&lt;LI&gt;The USER_LED of the RT1050-EVKB is connected to pin&amp;nbsp;GPIO_AD_B0_09. This pin has PWM functionality. So, you can modify the SDK example to activate this pin as well. This way, you will see the PWM through the onboard LED.&amp;nbsp;&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Victor&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 23 Jun 2021 18:30:39 GMT</pubDate>
    <dc:creator>victorjimenez</dc:creator>
    <dc:date>2021-06-23T18:30:39Z</dc:date>
    <item>
      <title>LED Brightness control with PWM</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/LED-Brightness-control-with-PWM/m-p/1295440#M14808</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am very new to MXRT1050EVKB. I am trying to control with PWM signal. I have configure a pin as pwm1&lt;/P&gt;&lt;P&gt;peripheral. The pwm signal has also generated.But what more i should do control brightness of LED..what more have to implement and how?Please help&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 21 Jun 2021 12:57:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/LED-Brightness-control-with-PWM/m-p/1295440#M14808</guid>
      <dc:creator>DavidChang0</dc:creator>
      <dc:date>2021-06-21T12:57:35Z</dc:date>
    </item>
    <item>
      <title>Re: LED Brightness control with PWM</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/LED-Brightness-control-with-PWM/m-p/1297078#M14882</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;Within the SDK for the RT1050-EVKB you will find a PWM example. This is a good starting point for your application. If you want to see the PWM through an LED, you have two options:&amp;nbsp;&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;Connect an external LED to one of the PWM outputs of the example.&amp;nbsp;&lt;/LI&gt;
&lt;LI&gt;The USER_LED of the RT1050-EVKB is connected to pin&amp;nbsp;GPIO_AD_B0_09. This pin has PWM functionality. So, you can modify the SDK example to activate this pin as well. This way, you will see the PWM through the onboard LED.&amp;nbsp;&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Victor&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 23 Jun 2021 18:30:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/LED-Brightness-control-with-PWM/m-p/1297078#M14882</guid>
      <dc:creator>victorjimenez</dc:creator>
      <dc:date>2021-06-23T18:30:39Z</dc:date>
    </item>
  </channel>
</rss>