<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX RT Crossover MCUsのトピックexample code for multiple ADC CHANNELS</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/example-code-for-multiple-ADC-CHANNELS/m-p/1294430#M14774</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;i am using rt1050 EVKB board. i am able to read the voltage from single channel ADC1 channel 0.&lt;/P&gt;&lt;P&gt;i want to use another four channels. please help me with an example code.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;jagadeesh&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Fri, 18 Jun 2021 05:37:30 GMT</pubDate>
    <dc:creator>jagadeesh_11</dc:creator>
    <dc:date>2021-06-18T05:37:30Z</dc:date>
    <item>
      <title>example code for multiple ADC CHANNELS</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/example-code-for-multiple-ADC-CHANNELS/m-p/1294430#M14774</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;i am using rt1050 EVKB board. i am able to read the voltage from single channel ADC1 channel 0.&lt;/P&gt;&lt;P&gt;i want to use another four channels. please help me with an example code.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;jagadeesh&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 18 Jun 2021 05:37:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/example-code-for-multiple-ADC-CHANNELS/m-p/1294430#M14774</guid>
      <dc:creator>jagadeesh_11</dc:creator>
      <dc:date>2021-06-18T05:37:30Z</dc:date>
    </item>
    <item>
      <title>Re: example code for multiple ADC CHANNELS</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/example-code-for-multiple-ADC-CHANNELS/m-p/1295095#M14800</link>
      <description>&lt;P&gt;Hi,&lt;BR /&gt;Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.&lt;BR /&gt;1) I want to use another four channels. please help me with an example code.&lt;BR /&gt;-- To provide the fastest possible support, I'd highly recommend you to refer to the adc_etc demo in the SDK library, the demo illustrates how to use the ADC-ETC module to sample multiple ADC pins in order.&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Mon, 21 Jun 2021 02:53:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/example-code-for-multiple-ADC-CHANNELS/m-p/1295095#M14800</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2021-06-21T02:53:59Z</dc:date>
    </item>
  </channel>
</rss>