<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX RT Crossover MCUsのトピックRe: Debugger error with 'Empty board files' projects</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Debugger-error-with-Empty-board-files-projects/m-p/1293842#M14751</link>
    <description>&lt;P&gt;Hi,&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/60336"&gt;@kerryzhou&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;yes, flash driver is not set by default when creating 'Empty board files' project.&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Maciek&lt;/P&gt;</description>
    <pubDate>Thu, 17 Jun 2021 06:51:17 GMT</pubDate>
    <dc:creator>Maciek</dc:creator>
    <dc:date>2021-06-17T06:51:17Z</dc:date>
    <item>
      <title>Debugger error with 'Empty board files' projects</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Debugger-error-with-Empty-board-files-projects/m-p/1293216#M14730</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm trying to run my first simple programs on i.MXRT1064 EVK board (in default/factory hardware configuration) using MCUXpresso.&lt;BR /&gt;I can flash and debug various demo apps from SDK. If I create new project with all defalults in 'new project wizard' AND with 'Default board files' it compiles and I can debug the same as example projects.&lt;/P&gt;&lt;P&gt;If I create a new project with all defaults from 'new project wizard' but with 'Empty board files': it builds with no errors but I got error while trying debugging "Remote communication error. Target disconnected.: Success.".&lt;BR /&gt;I've attached the screenshot with this error. After such error I can't also mass erase the flash: it ends with 'Unable to perform operation! Command failed with exit code 1'.&lt;/P&gt;&lt;P&gt;When I then switch to SDK demo app or project with 'Default board files' everything works.&lt;/P&gt;&lt;P&gt;How to configure simplest new project to be able to debug it in MCUXpresso without this error ???&lt;/P&gt;&lt;P&gt;Thanks for help&lt;BR /&gt;Maciek&lt;/P&gt;</description>
      <pubDate>Wed, 16 Jun 2021 10:51:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Debugger-error-with-Empty-board-files-projects/m-p/1293216#M14730</guid>
      <dc:creator>Maciek</dc:creator>
      <dc:date>2021-06-16T10:51:53Z</dc:date>
    </item>
    <item>
      <title>Re: Debugger error with 'Empty board files' projects</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Debugger-error-with-Empty-board-files-projects/m-p/1293419#M14731</link>
      <description>&lt;P&gt;Solved.&lt;/P&gt;</description>
      <pubDate>Wed, 16 Jun 2021 15:52:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Debugger-error-with-Empty-board-files-projects/m-p/1293419#M14731</guid>
      <dc:creator>Maciek</dc:creator>
      <dc:date>2021-06-16T15:52:12Z</dc:date>
    </item>
    <item>
      <title>Re: Debugger error with 'Empty board files' projects</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Debugger-error-with-Empty-board-files-projects/m-p/1293692#M14743</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/12402"&gt;@Maciek&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp; &amp;nbsp;Thanks for the updated information, from your picture, seems the flashdriver is wrong.&lt;/P&gt;
&lt;P&gt;&amp;nbsp; &amp;nbsp;Anyway, if you have any new issues in the future, welcome to create the new question post.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;kerry&lt;/P&gt;</description>
      <pubDate>Thu, 17 Jun 2021 01:58:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Debugger-error-with-Empty-board-files-projects/m-p/1293692#M14743</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2021-06-17T01:58:49Z</dc:date>
    </item>
    <item>
      <title>Re: Debugger error with 'Empty board files' projects</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Debugger-error-with-Empty-board-files-projects/m-p/1293842#M14751</link>
      <description>&lt;P&gt;Hi,&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/60336"&gt;@kerryzhou&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;yes, flash driver is not set by default when creating 'Empty board files' project.&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Maciek&lt;/P&gt;</description>
      <pubDate>Thu, 17 Jun 2021 06:51:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Debugger-error-with-Empty-board-files-projects/m-p/1293842#M14751</guid>
      <dc:creator>Maciek</dc:creator>
      <dc:date>2021-06-17T06:51:17Z</dc:date>
    </item>
    <item>
      <title>Re: Debugger error with 'Empty board files' projects</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Debugger-error-with-Empty-board-files-projects/m-p/1293845#M14752</link>
      <description>&lt;P&gt;So, after you select the flashdriver, issue resolved, right?&lt;/P&gt;
&lt;P&gt;If your question is solved, please help to mark the correct answer, just to close this case.&lt;/P&gt;
&lt;P&gt;Any issues in the future, welcome to create the new question post.&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;kerry&lt;/P&gt;</description>
      <pubDate>Thu, 17 Jun 2021 06:58:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Debugger-error-with-Empty-board-files-projects/m-p/1293845#M14752</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2021-06-17T06:58:57Z</dc:date>
    </item>
  </channel>
</rss>