<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX RT Crossover MCUsのトピックDebug encrypted HAB image</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Debug-encrypted-HAB-image/m-p/1289676#M14618</link>
    <description>&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;We are using HAB with an encrypted image and download the image with the MfgTool.&lt;BR /&gt;The application runs this way, but we need to debug a problem.&lt;/P&gt;&lt;P&gt;The problem only happens with the encrypted image (not with the same code and an unencrypted image), therefore we need to debug the encryped image.&lt;/P&gt;&lt;P&gt;Is it possible at all to debug an encrypted image with the SWD debugger?&lt;/P&gt;&lt;P&gt;Thanks and regards,&lt;BR /&gt;Daniel&lt;/P&gt;</description>
    <pubDate>Wed, 09 Jun 2021 07:05:15 GMT</pubDate>
    <dc:creator>dh1</dc:creator>
    <dc:date>2021-06-09T07:05:15Z</dc:date>
    <item>
      <title>Debug encrypted HAB image</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Debug-encrypted-HAB-image/m-p/1289676#M14618</link>
      <description>&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;We are using HAB with an encrypted image and download the image with the MfgTool.&lt;BR /&gt;The application runs this way, but we need to debug a problem.&lt;/P&gt;&lt;P&gt;The problem only happens with the encrypted image (not with the same code and an unencrypted image), therefore we need to debug the encryped image.&lt;/P&gt;&lt;P&gt;Is it possible at all to debug an encrypted image with the SWD debugger?&lt;/P&gt;&lt;P&gt;Thanks and regards,&lt;BR /&gt;Daniel&lt;/P&gt;</description>
      <pubDate>Wed, 09 Jun 2021 07:05:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Debug-encrypted-HAB-image/m-p/1289676#M14618</guid>
      <dc:creator>dh1</dc:creator>
      <dc:date>2021-06-09T07:05:15Z</dc:date>
    </item>
    <item>
      <title>Re: Debug encrypted HAB image</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Debug-encrypted-HAB-image/m-p/1289807#M14620</link>
      <description>&lt;P&gt;Hi,&lt;BR /&gt;Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.&lt;BR /&gt;1）Is it possible at all to debug an encrypted image with the SWD debugger?&lt;BR /&gt;-- No, I'm afraid not.&lt;BR /&gt;I'd like to suggest you to consider other debug trick like terminal print, etc.&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Wed, 09 Jun 2021 09:38:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Debug-encrypted-HAB-image/m-p/1289807#M14620</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2021-06-09T09:38:17Z</dc:date>
    </item>
  </channel>
</rss>