<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX RT Crossover MCUsのトピックRe: MIMXRT1050-EVK with P&amp;E Micro</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/MIMXRT1050-EVK-with-P-E-Micro/m-p/829196#M1448</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I just tested programming the hello_wold example from MCUXpresso SDK on MIMXRT1050-EVKB board with P&amp;amp;E Multilink FX rev. B, and it worked properly. The key points to consider are the following:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Please ensure that MCUXpresso IDE have the proper launch configurations for P&amp;amp;E.&lt;/LI&gt;&lt;LI&gt;Double check that the EVKB board is properly powered (jumpers on J1).&lt;/LI&gt;&lt;LI&gt;Verify if the P&amp;amp;E Multilink FX has the updated firmware.&lt;/LI&gt;&lt;LI&gt;Double check the cable connection/orientation between Multilink FX and EVKB board. I tested with a 20-pin ribbon cable on PORT_B of the Multilink FX, and also with a 20-pin mini ribbon cable on PORT_F with an adapter on the other end. In both cases, it was connected to J21 header of the EVKB board.&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;BR /&gt;Hope this will be useful for you.&lt;BR /&gt;Best regards!&lt;BR /&gt;/Carlos&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 24 Sep 2018 22:11:39 GMT</pubDate>
    <dc:creator>CarlosCasillas</dc:creator>
    <dc:date>2018-09-24T22:11:39Z</dc:date>
    <item>
      <title>MIMXRT1050-EVK with P&amp;E Micro</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/MIMXRT1050-EVK-with-P-E-Micro/m-p/829195#M1447</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using MIMXRT1050-EVK and I have P&amp;amp;E multi link FX (Rev.A). I try to use P&amp;amp;E which I have to debug EVK on MCUXpresso but IDE show illegal device. Does&amp;nbsp;&lt;SPAN&gt;P&amp;amp;E multi link FX (Rev.A) support I.MXRT 1050 device?&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 15 Sep 2018 14:41:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/MIMXRT1050-EVK-with-P-E-Micro/m-p/829195#M1447</guid>
      <dc:creator>Childe</dc:creator>
      <dc:date>2018-09-15T14:41:53Z</dc:date>
    </item>
    <item>
      <title>Re: MIMXRT1050-EVK with P&amp;E Micro</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/MIMXRT1050-EVK-with-P-E-Micro/m-p/829196#M1448</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I just tested programming the hello_wold example from MCUXpresso SDK on MIMXRT1050-EVKB board with P&amp;amp;E Multilink FX rev. B, and it worked properly. The key points to consider are the following:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Please ensure that MCUXpresso IDE have the proper launch configurations for P&amp;amp;E.&lt;/LI&gt;&lt;LI&gt;Double check that the EVKB board is properly powered (jumpers on J1).&lt;/LI&gt;&lt;LI&gt;Verify if the P&amp;amp;E Multilink FX has the updated firmware.&lt;/LI&gt;&lt;LI&gt;Double check the cable connection/orientation between Multilink FX and EVKB board. I tested with a 20-pin ribbon cable on PORT_B of the Multilink FX, and also with a 20-pin mini ribbon cable on PORT_F with an adapter on the other end. In both cases, it was connected to J21 header of the EVKB board.&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;BR /&gt;Hope this will be useful for you.&lt;BR /&gt;Best regards!&lt;BR /&gt;/Carlos&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 24 Sep 2018 22:11:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/MIMXRT1050-EVK-with-P-E-Micro/m-p/829196#M1448</guid>
      <dc:creator>CarlosCasillas</dc:creator>
      <dc:date>2018-09-24T22:11:39Z</dc:date>
    </item>
  </channel>
</rss>