<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic iMXRT1064 / How to set up CSI for raw camera data? in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/iMXRT1064-How-to-set-up-CSI-for-raw-camera-data/m-p/1284821#M14477</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I'm developing camera application for iMXRT1064.&lt;/P&gt;&lt;P&gt;The camera we are using is a b/w camera sensor that outputs RAW-10 (RAW-8) data. The camera outputs MIPI serial data, so we have a bridge IC that converts the serial data to parallel CSI data. We have an 8-bit wide interface in use from the bridge IC to iMX; CSI_DATA09 .. CSI_DATA02.&lt;/P&gt;&lt;P&gt;As I understand, our current setup gives data as follows;&amp;nbsp;on even lines BGBGBG... and on odd lines GRGRGR..., and each element is an 8-bit value. Both the camera and the bridge IC are successfully initialized and configured when starting up the camera application. I can see CSI reporting two buffers being filled in, and after that it tells that no buffer is full.&lt;/P&gt;&lt;P&gt;What would be the optimal configuration for the CSI receiver in this case where incoming data is raw data?&lt;/P&gt;&lt;P&gt;Any advice on how to receive and process raw data by CSI would be appreciated.&lt;/P&gt;&lt;P&gt;Thanks for your support!&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Jari&lt;/P&gt;</description>
    <pubDate>Mon, 31 May 2021 13:22:36 GMT</pubDate>
    <dc:creator>jaripeltonen</dc:creator>
    <dc:date>2021-05-31T13:22:36Z</dc:date>
    <item>
      <title>iMXRT1064 / How to set up CSI for raw camera data?</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/iMXRT1064-How-to-set-up-CSI-for-raw-camera-data/m-p/1284821#M14477</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I'm developing camera application for iMXRT1064.&lt;/P&gt;&lt;P&gt;The camera we are using is a b/w camera sensor that outputs RAW-10 (RAW-8) data. The camera outputs MIPI serial data, so we have a bridge IC that converts the serial data to parallel CSI data. We have an 8-bit wide interface in use from the bridge IC to iMX; CSI_DATA09 .. CSI_DATA02.&lt;/P&gt;&lt;P&gt;As I understand, our current setup gives data as follows;&amp;nbsp;on even lines BGBGBG... and on odd lines GRGRGR..., and each element is an 8-bit value. Both the camera and the bridge IC are successfully initialized and configured when starting up the camera application. I can see CSI reporting two buffers being filled in, and after that it tells that no buffer is full.&lt;/P&gt;&lt;P&gt;What would be the optimal configuration for the CSI receiver in this case where incoming data is raw data?&lt;/P&gt;&lt;P&gt;Any advice on how to receive and process raw data by CSI would be appreciated.&lt;/P&gt;&lt;P&gt;Thanks for your support!&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Jari&lt;/P&gt;</description>
      <pubDate>Mon, 31 May 2021 13:22:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/iMXRT1064-How-to-set-up-CSI-for-raw-camera-data/m-p/1284821#M14477</guid>
      <dc:creator>jaripeltonen</dc:creator>
      <dc:date>2021-05-31T13:22:36Z</dc:date>
    </item>
    <item>
      <title>Re: iMXRT1064 / How to set up CSI for raw camera data?</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/iMXRT1064-How-to-set-up-CSI-for-raw-camera-data/m-p/1287057#M14529</link>
      <description>&lt;P&gt;Hi Jari,&lt;/P&gt;
&lt;P&gt;RT1064 supports 8-bit/10-bit/16-bit Bayer data input for raw data from the image sensor. You can find more information about this in the CSI chapter of the RM.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Felipe&lt;/P&gt;</description>
      <pubDate>Thu, 03 Jun 2021 22:11:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/iMXRT1064-How-to-set-up-CSI-for-raw-camera-data/m-p/1287057#M14529</guid>
      <dc:creator>FelipeGarcia</dc:creator>
      <dc:date>2021-06-03T22:11:36Z</dc:date>
    </item>
  </channel>
</rss>