<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX RT Crossover MCUsのトピックCMSIS-DAP: SWD/JTAG Communication Failure after working previously</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/CMSIS-DAP-SWD-JTAG-Communication-Failure-after-working/m-p/1282484#M14378</link>
    <description>&lt;P&gt;&lt;SPAN class="test-id__field-value slds-form-element__static slds-grow  is-read-only"&gt;&lt;SPAN class="uiOutputTextArea"&gt;I am using the MIMXRT1170-EVK together with the Keil uVision5 IDE and MCUXpresso Config Tools and was initially able to successfully program the board (e.g. with example projects).&amp;nbsp;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="test-id__field-value slds-form-element__static slds-grow  is-read-only"&gt;&lt;SPAN class="uiOutputTextArea"&gt;After developing a small program using the LPSPI peripheral in transfer mode and running it in debug mode, debugging stopped with an error message (i can't recall what it said). After that, connection to the board via the CMSIS-DAP debugger is not possible anymore (error message SWD/JTAG Communication Failure). For debug setting see attached picture. I already tried different max clock settings. I didn't modify any jumpers or switches compared to the previously working default configuration.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="test-id__field-value slds-form-element__static slds-grow  is-read-only"&gt;&lt;SPAN class="uiOutputTextArea"&gt;I also tried to connect to the board via MCUXpresso IDE but it didn't work either.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="test-id__field-value slds-form-element__static slds-grow  is-read-only"&gt;&lt;SPAN class="uiOutputTextArea"&gt;Can someone help me recover the board?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Wed, 26 May 2021 10:02:56 GMT</pubDate>
    <dc:creator>MISO_27</dc:creator>
    <dc:date>2021-05-26T10:02:56Z</dc:date>
    <item>
      <title>CMSIS-DAP: SWD/JTAG Communication Failure after working previously</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/CMSIS-DAP-SWD-JTAG-Communication-Failure-after-working/m-p/1282484#M14378</link>
      <description>&lt;P&gt;&lt;SPAN class="test-id__field-value slds-form-element__static slds-grow  is-read-only"&gt;&lt;SPAN class="uiOutputTextArea"&gt;I am using the MIMXRT1170-EVK together with the Keil uVision5 IDE and MCUXpresso Config Tools and was initially able to successfully program the board (e.g. with example projects).&amp;nbsp;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="test-id__field-value slds-form-element__static slds-grow  is-read-only"&gt;&lt;SPAN class="uiOutputTextArea"&gt;After developing a small program using the LPSPI peripheral in transfer mode and running it in debug mode, debugging stopped with an error message (i can't recall what it said). After that, connection to the board via the CMSIS-DAP debugger is not possible anymore (error message SWD/JTAG Communication Failure). For debug setting see attached picture. I already tried different max clock settings. I didn't modify any jumpers or switches compared to the previously working default configuration.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="test-id__field-value slds-form-element__static slds-grow  is-read-only"&gt;&lt;SPAN class="uiOutputTextArea"&gt;I also tried to connect to the board via MCUXpresso IDE but it didn't work either.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="test-id__field-value slds-form-element__static slds-grow  is-read-only"&gt;&lt;SPAN class="uiOutputTextArea"&gt;Can someone help me recover the board?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 26 May 2021 10:02:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/CMSIS-DAP-SWD-JTAG-Communication-Failure-after-working/m-p/1282484#M14378</guid>
      <dc:creator>MISO_27</dc:creator>
      <dc:date>2021-05-26T10:02:56Z</dc:date>
    </item>
    <item>
      <title>Re: CMSIS-DAP: SWD/JTAG Communication Failure after working previously</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/CMSIS-DAP-SWD-JTAG-Communication-Failure-after-working/m-p/1283179#M14398</link>
      <description>&lt;P&gt;The solution is to use the serial downloader ("SDP Mode"; SW1: 0-0-0-1; SW2: all 0s), erase data in QSPI flash and program a example project. After a power reset the board can be debugged in default configuration again.&lt;/P&gt;&lt;P&gt;This document details the procedure:&lt;SPAN&gt; &lt;A href="https://community.nxp.com/pwmxy87654/attachments/pwmxy87654/mcux-blogs/123/1/RT1170_BriefOverview_v110.pdf" target="_blank"&gt;https://community.nxp.com/pwmxy87654/attachments/pwmxy87654/mcux-blogs/123/1/RT1170_BriefOverview_v110.pdf&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 27 May 2021 07:18:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/CMSIS-DAP-SWD-JTAG-Communication-Failure-after-working/m-p/1283179#M14398</guid>
      <dc:creator>MISO_27</dc:creator>
      <dc:date>2021-05-27T07:18:36Z</dc:date>
    </item>
  </channel>
</rss>