<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: IMX RT1011 Cannot Connect JLink in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IMX-RT1011-Cannot-Connect-JLink/m-p/1273393#M14128</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;A id="link_12" class="lia-link-navigation lia-page-link lia-user-name-link" href="https://community.nxp.com/t5/user/viewprofilepage/user-id/185970" target="_self" aria-label="View Profile of whermann"&gt;&lt;SPAN class=""&gt;whermann&lt;/SPAN&gt;&lt;/A&gt;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp; &amp;nbsp;RT1011 is using the SWD interface in default, not the JTAG, so when you connect the board, you need to use the SWD instead of the JTAG.&lt;/P&gt;
&lt;P&gt;&amp;nbsp; Now, to your not working board, could you please use the JLINK commander to check your board, whether you can find the ARM core or not?&lt;/P&gt;
&lt;P&gt;&amp;nbsp; If you can't find the ARM core, it means your hardware still have issues, if you can find the ARM core, your issues may in the code project side.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="kerryzhou_0-1620362812248.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/144151i2834CC022B0DA58F/image-size/medium?v=v2&amp;amp;px=400" role="button" title="kerryzhou_0-1620362812248.png" alt="kerryzhou_0-1620362812248.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Please check it, and also share me your JLINK command result.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Kerry&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Fri, 07 May 2021 04:47:23 GMT</pubDate>
    <dc:creator>kerryzhou</dc:creator>
    <dc:date>2021-05-07T04:47:23Z</dc:date>
    <item>
      <title>IMX RT1011 Cannot Connect JLink</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IMX-RT1011-Cannot-Connect-JLink/m-p/1272496#M14102</link>
      <description>&lt;P&gt;I have two custom boards using the i.MX RT1011 MCU. Both have identical power and debug connections. One board works fine (this one has an MIMXRT1011DAE5A) and my JLink has no problem connecting. The other board (this one has an MIMXRT1011CAE4A) seems to power-up fine (all supply pins are at expected levels), but I cannot connect with the JLink debugger.&lt;/P&gt;&lt;P&gt;When trying to debug with MCUXpresso, I just get a message saying JLink could not connect. Using the JLink Commander, I can get some more detail. The snippet below is the output when trying to connect using JTAG:&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;&lt;FONT face="courier new,courier"&gt;Device "MIMXRT1011XXX4A" selected.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;Connecting to target via JTAG&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;TotalIRLen = 5, IRPrint = 0x01&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;JTAG chain detection found 1 devices:&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;#0 Id: 0x088C701D, IRLen: 04, JTAG-DP&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;Found 1 device in JTAG chain, IRPost/DRPost != 0. Reset IRPost/DRPost to 0.&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;Failed to power up DAP&lt;/FONT&gt;&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;FONT face="arial,helvetica,sans-serif"&gt;And in SWD mode:&lt;/FONT&gt;&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;&lt;FONT face="courier new,courier"&gt;J-Link&amp;gt;connect&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;Device "MIMXRT1011XXX4A" selected.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;Connecting to target via SWD&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;Cannot connect to target.&lt;/FONT&gt;&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;FONT face="arial,helvetica,sans-serif"&gt;Interestingly, when using my working board, it shows unable to connect using JTAG, but it can connect with SWD:&lt;/FONT&gt;&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;&lt;FONT face="courier new,courier"&gt;J-Link&amp;gt;connect&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;Device "MIMXRT1011XXX4A" selected.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;Connecting to target via JTAG&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;TotalIRLen = ?, IRPrint = 0x..000000000000000000000000&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;TotalIRLen = ?, IRPrint = 0x..000000000000000000000000&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;TotalIRLen = ?, IRPrint = 0x..000000000000000000000000&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;TotalIRLen = ?, IRPrint = 0x..000000000000000000000000&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;Cannot connect to target.&lt;/FONT&gt;&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;FONT face="arial,helvetica,sans-serif"&gt;SWD:&lt;/FONT&gt;&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;&lt;FONT face="courier new,courier"&gt;J-Link&amp;gt;connect&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;Device "MIMXRT1011XXX4A" selected.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;Connecting to target via SWD&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;Found SW-DP with ID 0x0BD11477&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;DPIDR: 0x0BD11477&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;Scanning AP map to find all available APs&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;AP[1]: Stopped AP scan as end of AP map has been reached&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;AP[0]: AHB-AP (IDR: 0x04770041)&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;Iterating through AP map to find AHB-AP to use&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;AP[0]: Core found&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;AP[0]: AHB-AP ROM base: 0xE00FD000&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;CPUID register: 0x411FC272. Implementer code: 0x41 (ARM)&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;Found Cortex-M7 r1p2, Little endian.&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;FPUnit: 8 code (BP) slots and 0 literal slots&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;CoreSight components:&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;ROMTbl[0] @ E00FD000&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;ROMTbl[0][0]: E00FE000, CID: B105100D, PID: 000BB4C8 ROM Table&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;ROMTbl[1] @ E00FE000&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;ROMTbl[1][0]: E00FF000, CID: B105100D, PID: 000BB4C7 ROM Table&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;ROMTbl[2] @ E00FF000&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;ROMTbl[2][0]: E000E000, CID: B105E00D, PID: 000BB00C SCS-M7&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;ROMTbl[2][1]: E0001000, CID: B105E00D, PID: 000BB002 DWT&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;ROMTbl[2][2]: E0002000, CID: B105E00D, PID: 000BB00E FPB-M7&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;ROMTbl[2][3]: E0000000, CID: B105E00D, PID: 000BB001 ITM&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;ROMTbl[1][1]: E0041000, CID: B105900D, PID: 001BB975 ETM-M7&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;ROMTbl[1][2]: E0042000, CID: B105900D, PID: 004BB906 CTI&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;ROMTbl[0][1]: E0040000, CID: B105900D, PID: 000BB9A9 TPIU-M7&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;ROMTbl[0][2]: E0043000, CID: B105F00D, PID: 001BB101 TSG&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;Cache: Separate I- and D-cache.&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;I-Cache L1: 16 KB, 256 Sets, 32 Bytes/Line, 2-Way&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;D-Cache L1: 8 KB, 64 Sets, 32 Bytes/Line, 4-Way&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;Cortex-M7 identified.&lt;/FONT&gt;&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;FONT face="arial,helvetica,sans-serif"&gt;The only other significant difference between these two boards is with the main 24MHz oscillator: the working board is using the standard 24MHz fundamental mode crystal connected between XTALI and XTALO, while the non-functional board uses an external oscillator feeding into XTALI with XTALO floating. The clock amplitude is as suggested in the reference manual and I do see a signal on XTALO, and I can also see the quiescent current drop significantly if I pull XTALI to GND, so I believe this is working as intended.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="arial,helvetica,sans-serif"&gt;I'm worried this might have something to do with one of the JTAG security settings, but don't know how to check if that is the case. Is there any difference between the MIMXRT1011DAE5A and MIMXRT1011CAE4A with regards to JTAG/SWD or boot? My understanding is that the only differences between these two devices are operating temperature range and maximum frequency.&lt;/FONT&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 05 May 2021 22:56:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IMX-RT1011-Cannot-Connect-JLink/m-p/1272496#M14102</guid>
      <dc:creator>whermann</dc:creator>
      <dc:date>2021-05-05T22:56:39Z</dc:date>
    </item>
    <item>
      <title>Re: IMX RT1011 Cannot Connect JLink</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IMX-RT1011-Cannot-Connect-JLink/m-p/1273393#M14128</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;A id="link_12" class="lia-link-navigation lia-page-link lia-user-name-link" href="https://community.nxp.com/t5/user/viewprofilepage/user-id/185970" target="_self" aria-label="View Profile of whermann"&gt;&lt;SPAN class=""&gt;whermann&lt;/SPAN&gt;&lt;/A&gt;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp; &amp;nbsp;RT1011 is using the SWD interface in default, not the JTAG, so when you connect the board, you need to use the SWD instead of the JTAG.&lt;/P&gt;
&lt;P&gt;&amp;nbsp; Now, to your not working board, could you please use the JLINK commander to check your board, whether you can find the ARM core or not?&lt;/P&gt;
&lt;P&gt;&amp;nbsp; If you can't find the ARM core, it means your hardware still have issues, if you can find the ARM core, your issues may in the code project side.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="kerryzhou_0-1620362812248.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/144151i2834CC022B0DA58F/image-size/medium?v=v2&amp;amp;px=400" role="button" title="kerryzhou_0-1620362812248.png" alt="kerryzhou_0-1620362812248.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Please check it, and also share me your JLINK command result.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Kerry&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 07 May 2021 04:47:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IMX-RT1011-Cannot-Connect-JLink/m-p/1273393#M14128</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2021-05-07T04:47:23Z</dc:date>
    </item>
    <item>
      <title>Re: IMX RT1011 Cannot Connect JLink</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IMX-RT1011-Cannot-Connect-JLink/m-p/1273887#M14149</link>
      <description>&lt;P&gt;After days of debug I finally figured out the problem. On my board there is an external pullup on pin GPIO_AD_11, which is JTAG_MOD. There is a small note in the datasheet about this pin needing to be pulled down for normal operation of the debug port. Removing my pullup allowed me to connect via SWD.&lt;/P&gt;</description>
      <pubDate>Fri, 07 May 2021 23:43:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IMX-RT1011-Cannot-Connect-JLink/m-p/1273887#M14149</guid>
      <dc:creator>whermann</dc:creator>
      <dc:date>2021-05-07T23:43:21Z</dc:date>
    </item>
  </channel>
</rss>