<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic the MIMXRT1050-EVK uart pin (in the arduino port) is it the UART1 instance ? in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/the-MIMXRT1050-EVK-uart-pin-in-the-arduino-port-is-it-the-UART1/m-p/826783#M1400</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have a two MIMXRT1050-EVK boards and I want to communicate between them using UART.&lt;/P&gt;&lt;P&gt;As indicated in the user's guide (picture attached to this post) there is a UART pin in the arduino expansion port, so I want to use it. But I don't know in which instance this pin is attached to ?&lt;/P&gt;&lt;P&gt;(UART1 or UART2 or ...)&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 27 Aug 2018 12:19:53 GMT</pubDate>
    <dc:creator>wassimhammami</dc:creator>
    <dc:date>2018-08-27T12:19:53Z</dc:date>
    <item>
      <title>the MIMXRT1050-EVK uart pin (in the arduino port) is it the UART1 instance ?</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/the-MIMXRT1050-EVK-uart-pin-in-the-arduino-port-is-it-the-UART1/m-p/826783#M1400</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have a two MIMXRT1050-EVK boards and I want to communicate between them using UART.&lt;/P&gt;&lt;P&gt;As indicated in the user's guide (picture attached to this post) there is a UART pin in the arduino expansion port, so I want to use it. But I don't know in which instance this pin is attached to ?&lt;/P&gt;&lt;P&gt;(UART1 or UART2 or ...)&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 27 Aug 2018 12:19:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/the-MIMXRT1050-EVK-uart-pin-in-the-arduino-port-is-it-the-UART1/m-p/826783#M1400</guid>
      <dc:creator>wassimhammami</dc:creator>
      <dc:date>2018-08-27T12:19:53Z</dc:date>
    </item>
    <item>
      <title>Re: the MIMXRT1050-EVK uart pin (in the arduino port) is it the UART1 instance ?</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/the-MIMXRT1050-EVK-uart-pin-in-the-arduino-port-is-it-the-UART1/m-p/826784#M1401</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The UART3 port is used in the Arduino interface of the i.MX RT1050 EVK board.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Artur&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Aug 2018 12:36:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/the-MIMXRT1050-EVK-uart-pin-in-the-arduino-port-is-it-the-UART1/m-p/826784#M1401</guid>
      <dc:creator>art</dc:creator>
      <dc:date>2018-08-28T12:36:47Z</dc:date>
    </item>
  </channel>
</rss>