<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic AddressSanitizer with RT1021 and MCUXpresso? in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/AddressSanitizer-with-RT1021-and-MCUXpresso/m-p/1263525#M13851</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Can you tell me how I can get set up with the AddressSanitizer for the RT1021 in MCUXpresso please?&lt;/P&gt;&lt;P&gt;I have found the&amp;nbsp;&lt;SPAN&gt;-fsanitize=address etc settings, but I don't know how or where to get the library it requires. (Otherwise I get lots of messages like "undefined reference to __ubsan_handle_pointer_overflow" etc.)&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Also if I turn&amp;nbsp;-fsanitize=address etc on for the C compiler, it does not compile. For example:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;arm-none-eabi-gcc: error: unrecognized command line option '-fsanitize-address'; did you mean '-fsanitize=address'?&lt;BR /&gt;arm-none-eabi-gcc: error: unrecognized command line option '-fsanitize-pointer-compare'; did you mean '-fsanitize=pointer-compare'?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Any help much appreciated.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Fri, 16 Apr 2021 11:36:40 GMT</pubDate>
    <dc:creator>rshipman</dc:creator>
    <dc:date>2021-04-16T11:36:40Z</dc:date>
    <item>
      <title>AddressSanitizer with RT1021 and MCUXpresso?</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/AddressSanitizer-with-RT1021-and-MCUXpresso/m-p/1263525#M13851</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Can you tell me how I can get set up with the AddressSanitizer for the RT1021 in MCUXpresso please?&lt;/P&gt;&lt;P&gt;I have found the&amp;nbsp;&lt;SPAN&gt;-fsanitize=address etc settings, but I don't know how or where to get the library it requires. (Otherwise I get lots of messages like "undefined reference to __ubsan_handle_pointer_overflow" etc.)&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Also if I turn&amp;nbsp;-fsanitize=address etc on for the C compiler, it does not compile. For example:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;arm-none-eabi-gcc: error: unrecognized command line option '-fsanitize-address'; did you mean '-fsanitize=address'?&lt;BR /&gt;arm-none-eabi-gcc: error: unrecognized command line option '-fsanitize-pointer-compare'; did you mean '-fsanitize=pointer-compare'?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Any help much appreciated.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 16 Apr 2021 11:36:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/AddressSanitizer-with-RT1021-and-MCUXpresso/m-p/1263525#M13851</guid>
      <dc:creator>rshipman</dc:creator>
      <dc:date>2021-04-16T11:36:40Z</dc:date>
    </item>
    <item>
      <title>Re: AddressSanitizer with RT1021 and MCUXpresso?</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/AddressSanitizer-with-RT1021-and-MCUXpresso/m-p/1265257#M13888</link>
      <description>&lt;P&gt;Hi Ronnie,&lt;/P&gt;
&lt;P&gt;Unfortunately, we do not have an official way to set up AddressSanitizer in MCUXpresso IDE. Please check the community thread below that provides a more detailed explanation about this.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/S32-Design-Studio/How-to-use-AddressSanitizer-in-S32-Design-studio/m-p/997027" target="_blank"&gt; How to use AddressSanitizer in S32 Design studio - NXP Community &lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Have a great day,&lt;/P&gt;
&lt;P&gt;Felipe&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;/P&gt;
&lt;P&gt;Note:&lt;/P&gt;
&lt;P&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored. Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;/P&gt;
&lt;P&gt;------------------------------------------------------------------------------&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 20 Apr 2021 15:34:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/AddressSanitizer-with-RT1021-and-MCUXpresso/m-p/1265257#M13888</guid>
      <dc:creator>FelipeGarcia</dc:creator>
      <dc:date>2021-04-20T15:34:01Z</dc:date>
    </item>
  </channel>
</rss>