<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX RT Crossover MCUsのトピックRe: Cortex M7 Quad Timer QTMR Clock Speed</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Cortex-M7-Quad-Timer-QTMR-Clock-Speed/m-p/1261547#M13784</link>
    <description>&lt;P&gt;Hello!&lt;/P&gt;
&lt;P&gt;It is not possible to select a different clock as the clock source. However, if you need to count to 1 second then you can chain the first channel and the second channel, this way you can interrupt every 1 sec. I recommend you to check the qtmr_timer example of the SDK that implements this with different scenarios.&lt;/P&gt;
&lt;P&gt;You can change the count time as you mentioned as well, please check the same example I mentioned above to see how you can do it in more detail.&lt;/P&gt;
&lt;P&gt;Regarding your last question, If you do not need an interrupt to be triggered at match time you can leave interrupt disabled.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Felipe&lt;/P&gt;</description>
    <pubDate>Tue, 13 Apr 2021 22:49:45 GMT</pubDate>
    <dc:creator>FelipeGarcia</dc:creator>
    <dc:date>2021-04-13T22:49:45Z</dc:date>
    <item>
      <title>Cortex M7 Quad Timer QTMR Clock Speed</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Cortex-M7-Quad-Timer-QTMR-Clock-Speed/m-p/1259833#M13722</link>
      <description>&lt;P&gt;I am using the MIMXRT1050 board with Keilv5 Pro edition. I am working with the Quad Timer (QTMR) and I want to set the timer count to 1 second. Looking at the manual, it states that the QTMR timers all use the IP Bus Clock Frequency, and the&amp;nbsp;QTMR_SetTimerPeriod function uses a 16 bit register to set the count.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;This means that the max timer count time with a prescaler of 128 is&amp;nbsp;65535 resulting in a 55ms timer. Is there anyway to change the clock to the&amp;nbsp;OSC_CLK or a slower clock? How can I use the QTMR timer to a higher count time?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;My goal is to use the QTMR timer to clear the&amp;nbsp;OFLAG when the counter time is reached. I will be changing the count time during runtime. Is there a way to do this with the current setup of the QTMR?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Also if I set the&amp;nbsp;OUTMODE register to "Clear OFLAG output on successful compare (001), do I still need an interrupt for the timer or just hitting the count will work?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I will be setting the&amp;nbsp;OFLAG using&amp;nbsp;Force OFLAG Output bit.&lt;/P&gt;</description>
      <pubDate>Fri, 09 Apr 2021 18:39:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Cortex-M7-Quad-Timer-QTMR-Clock-Speed/m-p/1259833#M13722</guid>
      <dc:creator>kamal1</dc:creator>
      <dc:date>2021-04-09T18:39:44Z</dc:date>
    </item>
    <item>
      <title>Re: Cortex M7 Quad Timer QTMR Clock Speed</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Cortex-M7-Quad-Timer-QTMR-Clock-Speed/m-p/1261547#M13784</link>
      <description>&lt;P&gt;Hello!&lt;/P&gt;
&lt;P&gt;It is not possible to select a different clock as the clock source. However, if you need to count to 1 second then you can chain the first channel and the second channel, this way you can interrupt every 1 sec. I recommend you to check the qtmr_timer example of the SDK that implements this with different scenarios.&lt;/P&gt;
&lt;P&gt;You can change the count time as you mentioned as well, please check the same example I mentioned above to see how you can do it in more detail.&lt;/P&gt;
&lt;P&gt;Regarding your last question, If you do not need an interrupt to be triggered at match time you can leave interrupt disabled.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Felipe&lt;/P&gt;</description>
      <pubDate>Tue, 13 Apr 2021 22:49:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Cortex-M7-Quad-Timer-QTMR-Clock-Speed/m-p/1261547#M13784</guid>
      <dc:creator>FelipeGarcia</dc:creator>
      <dc:date>2021-04-13T22:49:45Z</dc:date>
    </item>
  </channel>
</rss>