<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Errors using LPSPI on RT1050 as Slave in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Errors-using-LPSPI-on-RT1050-as-Slave/m-p/824380#M1375</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Which SDK version are you using?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 11 Dec 2018 07:41:29 GMT</pubDate>
    <dc:creator>jimmychan</dc:creator>
    <dc:date>2018-12-11T07:41:29Z</dc:date>
    <item>
      <title>Errors using LPSPI on RT1050 as Slave</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Errors-using-LPSPI-on-RT1050-as-Slave/m-p/824379#M1374</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm trying to run the LPSPI examples in the SDK (evkbimxrt1050_cmsis_lpspi_int_b2b_transfer_slave) on my EVKB board with a SPI USB emulator (TotalPhase) as Master on my Windows 10.&amp;nbsp; I'm able to send correct data to the RT1050, but the return data is corrupted.&amp;nbsp; In addition to using the CMSIS send/receive commands, I've also tried the Transfer command with the same results. Also tried switching from SPI3 to SPI1 channels that are connected to the J24 connector.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I try to load the TX data buffer for output to the PC Master with anything other than 0's, even the data *sent* to the RT1050 is corrupted.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I saw that the errata for the RT1050 indicated there is an issue if writing to the TCR then writing to the FIFO (ERR011097).&amp;nbsp; Does this affect the performance of the LPSPI port in the RT1050?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for any help you can give me.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 30 Nov 2018 23:57:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Errors-using-LPSPI-on-RT1050-as-Slave/m-p/824379#M1374</guid>
      <dc:creator>peter_lombrozo</dc:creator>
      <dc:date>2018-11-30T23:57:28Z</dc:date>
    </item>
    <item>
      <title>Re: Errors using LPSPI on RT1050 as Slave</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Errors-using-LPSPI-on-RT1050-as-Slave/m-p/824380#M1375</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Which SDK version are you using?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Dec 2018 07:41:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Errors-using-LPSPI-on-RT1050-as-Slave/m-p/824380#M1375</guid>
      <dc:creator>jimmychan</dc:creator>
      <dc:date>2018-12-11T07:41:29Z</dc:date>
    </item>
    <item>
      <title>Re: Errors using LPSPI on RT1050 as Slave</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Errors-using-LPSPI-on-RT1050-as-Slave/m-p/824381#M1376</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;jimmychan-&amp;gt;&amp;nbsp; I'm using 2.4.0, manifest 3.3.0.&amp;nbsp; I'm realizing now there might be a problem in the USB SPI emulator I'm using where the clock timing is off sending and receiving each bit.&amp;nbsp; The loopback example (SPI1 &amp;lt;-&amp;gt; SPI3) works.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 17 Dec 2018 19:01:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Errors-using-LPSPI-on-RT1050-as-Slave/m-p/824381#M1376</guid>
      <dc:creator>peter_lombrozo</dc:creator>
      <dc:date>2018-12-17T19:01:22Z</dc:date>
    </item>
    <item>
      <title>Re: Errors using LPSPI on RT1050 as Slave</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Errors-using-LPSPI-on-RT1050-as-Slave/m-p/824382#M1377</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;There is 2.5.0 SDK. Please try the latest version of SDK.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 Dec 2018 03:44:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Errors-using-LPSPI-on-RT1050-as-Slave/m-p/824382#M1377</guid>
      <dc:creator>jimmychan</dc:creator>
      <dc:date>2018-12-18T03:44:42Z</dc:date>
    </item>
    <item>
      <title>Re: Errors using LPSPI on RT1050 as Slave</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Errors-using-LPSPI-on-RT1050-as-Slave/m-p/824383#M1378</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, did upgrade, no change.&amp;nbsp; Even sending 1 byte from RT1050 as slave to master only got 4 bits, rest are 0.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 Dec 2018 22:50:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Errors-using-LPSPI-on-RT1050-as-Slave/m-p/824383#M1378</guid>
      <dc:creator>peter_lombrozo</dc:creator>
      <dc:date>2018-12-18T22:50:21Z</dc:date>
    </item>
  </channel>
</rss>