<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic HyperRAM RWDS and FlexSPI DQS in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/HyperRAM-RWDS-and-FlexSPI-DQS/m-p/1244960#M13179</link>
    <description>&lt;P&gt;Hi guys,&lt;/P&gt;&lt;P&gt;I'm looking at the documentation of the FlexSPI and HyperRAM devices, and I don't understand the RWDS(DQS in the IMXRT) timing, when this signal is used as DATA MASK during the write transaction.&amp;nbsp;&lt;/P&gt;&lt;P&gt;In the attached file JPG file, there are 2 pictures.&lt;/P&gt;&lt;P&gt;The top picture shows the write transaction signaling from hyperRAM's datasheet. The bottom picture shows the FlexSPI signaling for a HyperBus device, taken from IMXRT Ref Manual.&lt;/P&gt;&lt;P&gt;As you can see the RWDS signal is not aligned as shown in the in the HyperRAM's datasheet.&lt;BR /&gt;Is the RWDS being used as DATA MASK in the EVKs during write transactions or it is simple held at zero all times?&lt;/P&gt;&lt;P&gt;Thanks a lot&lt;/P&gt;&lt;P&gt;Patricio&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Hyperbus_RWDS_FlexSPI_DQS.jpg" style="width: 948px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/139515iFC173233C4D01EBB/image-size/large?v=v2&amp;amp;px=999" role="button" title="Hyperbus_RWDS_FlexSPI_DQS.jpg" alt="Hyperbus_RWDS_FlexSPI_DQS.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;</description>
    <pubDate>Fri, 12 Mar 2021 16:45:42 GMT</pubDate>
    <dc:creator>patriciocohen</dc:creator>
    <dc:date>2021-03-12T16:45:42Z</dc:date>
    <item>
      <title>HyperRAM RWDS and FlexSPI DQS</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/HyperRAM-RWDS-and-FlexSPI-DQS/m-p/1244960#M13179</link>
      <description>&lt;P&gt;Hi guys,&lt;/P&gt;&lt;P&gt;I'm looking at the documentation of the FlexSPI and HyperRAM devices, and I don't understand the RWDS(DQS in the IMXRT) timing, when this signal is used as DATA MASK during the write transaction.&amp;nbsp;&lt;/P&gt;&lt;P&gt;In the attached file JPG file, there are 2 pictures.&lt;/P&gt;&lt;P&gt;The top picture shows the write transaction signaling from hyperRAM's datasheet. The bottom picture shows the FlexSPI signaling for a HyperBus device, taken from IMXRT Ref Manual.&lt;/P&gt;&lt;P&gt;As you can see the RWDS signal is not aligned as shown in the in the HyperRAM's datasheet.&lt;BR /&gt;Is the RWDS being used as DATA MASK in the EVKs during write transactions or it is simple held at zero all times?&lt;/P&gt;&lt;P&gt;Thanks a lot&lt;/P&gt;&lt;P&gt;Patricio&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Hyperbus_RWDS_FlexSPI_DQS.jpg" style="width: 948px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/139515iFC173233C4D01EBB/image-size/large?v=v2&amp;amp;px=999" role="button" title="Hyperbus_RWDS_FlexSPI_DQS.jpg" alt="Hyperbus_RWDS_FlexSPI_DQS.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 12 Mar 2021 16:45:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/HyperRAM-RWDS-and-FlexSPI-DQS/m-p/1244960#M13179</guid>
      <dc:creator>patriciocohen</dc:creator>
      <dc:date>2021-03-12T16:45:42Z</dc:date>
    </item>
    <item>
      <title>Re: HyperRAM RWDS and FlexSPI DQS</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/HyperRAM-RWDS-and-FlexSPI-DQS/m-p/1245322#M13207</link>
      <description>&lt;P&gt;Hi,&lt;BR /&gt;Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.&lt;BR /&gt;In my opinion, the above two figures both show CK and Data are center-aligned, however, in the below figure, the RWDS shift a half-cycle phase versus the above figure.&lt;BR /&gt;About using the HyperRAM with the i.MX RT, to provide the fastest possible support, I'd highly recommend you refer to the &lt;A href="https://www.nxp.com.cn/docs/en/nxp/application-notes/AN12239.pdf" target="_self"&gt;application note&lt;/A&gt; and &lt;A href="https://www.nxp.com.cn/docs/en/nxp/application-notes-software/AN12239SW.zip" target="_self"&gt;its corresponding code.&lt;/A&gt;&lt;BR /&gt;corresponding code.&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Mon, 15 Mar 2021 03:16:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/HyperRAM-RWDS-and-FlexSPI-DQS/m-p/1245322#M13207</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2021-03-15T03:16:07Z</dc:date>
    </item>
  </channel>
</rss>