<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: RT1020 Boot from FlexSPI in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1020-Boot-from-FlexSPI/m-p/820010#M1304</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Carlos,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I saw that paragraph in the reference manual but my question is with the details of the FlexSPI1 interface.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Below is a picture of Table 8-1 of the reference manual.&amp;nbsp; It states that the FlexSPI 1 interface consist of pins FLEXSPI_A_xxx and FLEXSPI_Bxxx.&amp;nbsp; The RT1020 EVK uses FlexSPI_A_xxx to&amp;nbsp;connect to and boot from the&amp;nbsp;Serial NOR Flash.&amp;nbsp; When BOOT_CFG1 [7:4] fuses is programmed to 0b’0000 can the Serial NOR Flash be connected to FLEXSPI_B to load the&amp;nbsp;parameters provided in the configuration block of the Serial NOR flash.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Brian&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="ROM Bootloader.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/65684i8B258807CFC09252/image-size/large?v=v2&amp;amp;px=999" role="button" title="ROM Bootloader.png" alt="ROM Bootloader.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 17 Jul 2018 18:17:00 GMT</pubDate>
    <dc:creator>brianchiatmo</dc:creator>
    <dc:date>2018-07-17T18:17:00Z</dc:date>
    <item>
      <title>RT1020 Boot from FlexSPI</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1020-Boot-from-FlexSPI/m-p/820008#M1302</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am planning a design with the&amp;nbsp;MIMXRT1021DAF5A and&amp;nbsp;was wondering if it is possible to&amp;nbsp;boot from Serial NOR Flash over FlexSPI B?&amp;nbsp; &amp;nbsp;In the Reference Manual, Table 8-1 ROM Bootloader Peripheral PinMux seems to indicate that FlexSPI B is initialized but there weren't any details on how to select channel B over channel A.&amp;nbsp; Is is possible to disable channel A or does the ROM boot loader try both channels sequentially?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Brian&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 17 Jul 2018 13:34:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1020-Boot-from-FlexSPI/m-p/820008#M1302</guid>
      <dc:creator>brianchiatmo</dc:creator>
      <dc:date>2018-07-17T13:34:23Z</dc:date>
    </item>
    <item>
      <title>Re: RT1020 Boot from FlexSPI</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1020-Boot-from-FlexSPI/m-p/820009#M1303</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Brian,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The Boot ROM attempts to boot from Serial NOR flash if the BOOT_CFG1 [7:4] fuses are programmed to 0b’0000, then the ROM will initialize FlexSPI1 interface. FlexSPI interface initialization is a two-step process. In the second step, ROM configures FlexSPI1 interface with the parameters provided in configuration block read from Serial NOR flash and starts the boot procedure.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As it is not possible to edit Boot ROM then it is not possible to boot from any SPI instance other than FlexSPI1.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Regards,&lt;BR /&gt;Carlos&lt;BR /&gt;NXP Technical Support&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 17 Jul 2018 17:22:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1020-Boot-from-FlexSPI/m-p/820009#M1303</guid>
      <dc:creator>Carlos_Musich</dc:creator>
      <dc:date>2018-07-17T17:22:10Z</dc:date>
    </item>
    <item>
      <title>Re: RT1020 Boot from FlexSPI</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1020-Boot-from-FlexSPI/m-p/820010#M1304</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Carlos,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I saw that paragraph in the reference manual but my question is with the details of the FlexSPI1 interface.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Below is a picture of Table 8-1 of the reference manual.&amp;nbsp; It states that the FlexSPI 1 interface consist of pins FLEXSPI_A_xxx and FLEXSPI_Bxxx.&amp;nbsp; The RT1020 EVK uses FlexSPI_A_xxx to&amp;nbsp;connect to and boot from the&amp;nbsp;Serial NOR Flash.&amp;nbsp; When BOOT_CFG1 [7:4] fuses is programmed to 0b’0000 can the Serial NOR Flash be connected to FLEXSPI_B to load the&amp;nbsp;parameters provided in the configuration block of the Serial NOR flash.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Brian&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="ROM Bootloader.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/65684i8B258807CFC09252/image-size/large?v=v2&amp;amp;px=999" role="button" title="ROM Bootloader.png" alt="ROM Bootloader.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 17 Jul 2018 18:17:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1020-Boot-from-FlexSPI/m-p/820010#M1304</guid>
      <dc:creator>brianchiatmo</dc:creator>
      <dc:date>2018-07-17T18:17:00Z</dc:date>
    </item>
    <item>
      <title>Re: RT1020 Boot from FlexSPI</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1020-Boot-from-FlexSPI/m-p/820011#M1305</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Brian,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;all pin mentioned in Table 8-1 can be used during internal boot from FlexSPI. It only depends on flash type configuration, e.g.:&lt;/P&gt;&lt;P&gt;HyperFlash - uses GPIO_SD_B1_00 up to&amp;nbsp;&lt;SPAN&gt;GPIO_SD_B1_11 (both FlexSPI A and FlexSPI B on SD domain)&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;QSPI 3B - uses&amp;nbsp;GPIO_SD_B1_06 up to&amp;nbsp;&lt;SPAN&gt;GPIO_SD_B1_11 (only FlexSPI A on SD domain)&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;SPAN&gt;or QSPI 3B secondary pin option -&amp;nbsp;GPIO_AD_B1_09 -&amp;nbsp;GPIO_AD_B1_15 (only FlexSPI A on analog domain)&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;Regards,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;Carlos&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 30 Jul 2018 22:21:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1020-Boot-from-FlexSPI/m-p/820011#M1305</guid>
      <dc:creator>Carlos_Musich</dc:creator>
      <dc:date>2018-07-30T22:21:18Z</dc:date>
    </item>
  </channel>
</rss>