<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX RT Crossover MCUsのトピックRe: Raspberry Pi HQ camera</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Raspberry-Pi-HQ-camera/m-p/1236099#M12887</link>
    <description>&lt;P&gt;The raspberry pi HQ camera output is RAW format which requires an ISP to convert to a usable color space.&amp;nbsp; The raspberry pi does this, unfortunately the i.MX RT parts do not have an internal ISP.&amp;nbsp; The cameras mentioned above - MT9M114 and OV7725 are modules which contain an ISP chip and then output a YUV type output to a CSI interface.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The i.MX 8M Plus does have an ISP and the camera built for it by Basler uses an OnSemi AR0821 image sensor and outputs raw.&amp;nbsp; It has a M12 lens mount so you can add different lenses.&lt;/P&gt;</description>
    <pubDate>Wed, 24 Feb 2021 20:48:12 GMT</pubDate>
    <dc:creator>john_phillippe</dc:creator>
    <dc:date>2021-02-24T20:48:12Z</dc:date>
    <item>
      <title>Raspberry Pi HQ camera</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Raspberry-Pi-HQ-camera/m-p/1233982#M12813</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Has anyone successfully used a Rpi HQ camera with the i.MX RT series?&lt;/P&gt;&lt;P&gt;It has a pretty nice 12.3 megapixel&amp;nbsp;Sony IMX477R sensor&lt;BR /&gt;&lt;A href="https://www.raspberrypi.org/products/raspberry-pi-high-quality-camera/" target="_blank"&gt;https://www.raspberrypi.org/products/raspberry-pi-high-quality-camera/&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;The interface coming from the camera is a 2-lane MIPI CSI-2, so a&amp;nbsp;Parallel Bridge IC or FPGA would be needed to feed the imxRT. Costwise this might not make any sense though, but just curious if someone have it up &amp;amp; running.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Sun, 21 Feb 2021 18:36:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Raspberry-Pi-HQ-camera/m-p/1233982#M12813</guid>
      <dc:creator>dav1</dc:creator>
      <dc:date>2021-02-21T18:36:22Z</dc:date>
    </item>
    <item>
      <title>Re: Raspberry Pi HQ camera</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Raspberry-Pi-HQ-camera/m-p/1234178#M12826</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;SPAN&gt;dav1,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&amp;nbsp; Until now, I didn't see any customer use the HQ camera in the RT. so we still don't have any solutions about&amp;nbsp;12.3 megapixel&amp;nbsp;Sony IMX477R sensor with RT.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&amp;nbsp; &amp;nbsp;We are mainly using&amp;nbsp;MT9M114 or OV7725 camera module.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&amp;nbsp; &amp;nbsp;Maybe you also can check your&amp;nbsp;Sony IMX477R sensor, whether that can meet the RT CSI demand. About the RT CSI feature, you can check the RT reference manual, CSI chapter.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&amp;nbsp; &amp;nbsp;If you still need help from my side, just kindly let me know.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Best Regards,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Kerry&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&amp;nbsp; &amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&amp;nbsp; &amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 22 Feb 2021 07:16:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Raspberry-Pi-HQ-camera/m-p/1234178#M12826</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2021-02-22T07:16:36Z</dc:date>
    </item>
    <item>
      <title>Re: Raspberry Pi HQ camera</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Raspberry-Pi-HQ-camera/m-p/1234241#M12832</link>
      <description>&lt;P&gt;hi, thanks will check what we can do. might look at imx8mini instead&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 22 Feb 2021 08:50:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Raspberry-Pi-HQ-camera/m-p/1234241#M12832</guid>
      <dc:creator>dav1</dc:creator>
      <dc:date>2021-02-22T08:50:21Z</dc:date>
    </item>
    <item>
      <title>Re: Raspberry Pi HQ camera</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Raspberry-Pi-HQ-camera/m-p/1236099#M12887</link>
      <description>&lt;P&gt;The raspberry pi HQ camera output is RAW format which requires an ISP to convert to a usable color space.&amp;nbsp; The raspberry pi does this, unfortunately the i.MX RT parts do not have an internal ISP.&amp;nbsp; The cameras mentioned above - MT9M114 and OV7725 are modules which contain an ISP chip and then output a YUV type output to a CSI interface.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The i.MX 8M Plus does have an ISP and the camera built for it by Basler uses an OnSemi AR0821 image sensor and outputs raw.&amp;nbsp; It has a M12 lens mount so you can add different lenses.&lt;/P&gt;</description>
      <pubDate>Wed, 24 Feb 2021 20:48:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Raspberry-Pi-HQ-camera/m-p/1236099#M12887</guid>
      <dc:creator>john_phillippe</dc:creator>
      <dc:date>2021-02-24T20:48:12Z</dc:date>
    </item>
    <item>
      <title>Re: Raspberry Pi HQ camera</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Raspberry-Pi-HQ-camera/m-p/1692311#M26040</link>
      <description>&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is there any update on the support for the r&lt;A href="https://www.arducam.com/product/12-3mp-imx477-hq-camera-module-b024001/" target="_self"&gt;aspberry pi HQ cam&lt;/A&gt;&amp;nbsp;(which can be used on the&amp;nbsp;&lt;SPAN&gt;DEBIX Model A)?&amp;nbsp;&lt;BR /&gt;Or could I only use the&amp;nbsp;OKdo &lt;A href="https://debix.io/Search/index.html?q=camera" target="_self"&gt;Camera 500 to 1300A camera's&lt;/A&gt;?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;And is this limited by the &lt;A href="https://debix.io/Document/manual_info/id/17/q/camera.html#m163" target="_self"&gt;DEBIX OS support for camera's&lt;/A&gt;?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks in advance!&lt;/P&gt;</description>
      <pubDate>Tue, 25 Jul 2023 13:35:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Raspberry-Pi-HQ-camera/m-p/1692311#M26040</guid>
      <dc:creator>qntn</dc:creator>
      <dc:date>2023-07-25T13:35:58Z</dc:date>
    </item>
    <item>
      <title>Re: Raspberry Pi HQ camera</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Raspberry-Pi-HQ-camera/m-p/1693783#M26071</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/220757"&gt;@qntn&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp; If you have any issues, please create your own question post, thanks.&lt;/P&gt;
&lt;P&gt;&amp;nbsp; Then we will help you in your own question post, please also tell use which NXP chip you are using in your own post.&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Kerry&lt;/P&gt;</description>
      <pubDate>Thu, 27 Jul 2023 04:58:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Raspberry-Pi-HQ-camera/m-p/1693783#M26071</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2023-07-27T04:58:22Z</dc:date>
    </item>
  </channel>
</rss>