<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: How to run evkmimxrt1060_lwip_httpssrv_ota_freertos? in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/How-to-run-evkmimxrt1060-lwip-httpssrv-ota-freertos/m-p/1232862#M12749</link>
    <description>&lt;P&gt;Thank, Kerry, it really helps&lt;/P&gt;&lt;P&gt;A few questions:&lt;/P&gt;&lt;P&gt;1. Does the app need to set both XIP_EXTERNAL_FLASH and XIP_BOOT_EXTERNAL_FLASH to 1? In other words, both bootloader and application needs to include the bootable image Header?&lt;/P&gt;&lt;P&gt;2. Does the App run on its own without bootloader programmed into the flash area? Or it has to be jumped here by bootloader and then run?&lt;/P&gt;&lt;P&gt;3. I cannot run as i don't have the board, really helpful if NXP can include the example into EVK_1024 and EVK_1064. I only have these 2 boards. Recently have to change to use RT1024 only as it is not BGA and still has internal flash.&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;P&gt;Ping&lt;/P&gt;</description>
    <pubDate>Thu, 18 Feb 2021 13:24:09 GMT</pubDate>
    <dc:creator>ping1</dc:creator>
    <dc:date>2021-02-18T13:24:09Z</dc:date>
    <item>
      <title>How to run evkmimxrt1060_lwip_httpssrv_ota_freertos?</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/How-to-run-evkmimxrt1060-lwip-httpssrv-ota-freertos/m-p/977955#M5106</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I want to add OTA function to my application, so I test the SDK sample&amp;nbsp;evkmimxrt1060_lwip_httpssrv_ota_freertos, but fail to run. How to fix it?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;my steps are:&lt;/P&gt;&lt;P&gt;SW7 setting: 0010&lt;/P&gt;&lt;P&gt;1) program&amp;nbsp;evkmimxrt1060_ota_bootloader (using default address 0x60000000)&lt;/P&gt;&lt;P&gt;2) program&amp;nbsp;evkmimxrt1060_lwip_httpssrv_ota_freertos (using default address 0x60040000)&lt;/P&gt;&lt;P&gt;3) press SW4 to reset&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can not connect EVK using browser, and the EVK RJ45 connector LED is not flash. I guess the application not run.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Jan 2020 11:47:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/How-to-run-evkmimxrt1060-lwip-httpssrv-ota-freertos/m-p/977955#M5106</guid>
      <dc:creator>felix1</dc:creator>
      <dc:date>2020-01-07T11:47:54Z</dc:date>
    </item>
    <item>
      <title>Re: How to run evkmimxrt1060_lwip_httpssrv_ota_freertos?</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/How-to-run-evkmimxrt1060-lwip-httpssrv-ota-freertos/m-p/977956#M5107</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi NXP,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can you give me a suggestion about SDK sample? Or guide me how to do OTA?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 10 Jan 2020 01:41:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/How-to-run-evkmimxrt1060-lwip-httpssrv-ota-freertos/m-p/977956#M5107</guid>
      <dc:creator>felix1</dc:creator>
      <dc:date>2020-01-10T01:41:18Z</dc:date>
    </item>
    <item>
      <title>Re: How to run evkmimxrt1060_lwip_httpssrv_ota_freertos?</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/How-to-run-evkmimxrt1060-lwip-httpssrv-ota-freertos/m-p/977957#M5108</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I got the following messages from bootloader, but still failed to connect EVK using browser.&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Have anyone tried the OTA sample?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;===&lt;/P&gt;&lt;P&gt;Running bootloader_reliable_update_as_requested...&lt;BR /&gt;Boot Meta summary:&lt;BR /&gt;---------------------------&lt;BR /&gt;Boot Partition: start=0x60000000, size=0x00040000&lt;BR /&gt;Primary Partition: start=0x60040000, size=0x00100000&lt;BR /&gt;Secondary Partition: start=0x60140000, size=0x00101000&lt;BR /&gt;Swap Meta summary:&lt;BR /&gt;---------------------------&lt;BR /&gt;swap_type:kSwapType_None&lt;BR /&gt;swap_progress: offset=0x00000000, scratch_size=0x00000000, stage=kSwapStage_NotStarted, remaining_size=0x00000000&lt;BR /&gt;Image Info:image[0].size=0x0x00000400, image[1].size=0x0x00000000&lt;BR /&gt;Swap Meta summary:&lt;BR /&gt;---------------------------&lt;BR /&gt;swap_type:kSwapType_None&lt;BR /&gt;swap_progress: offset=0x00000000, scratch_size=0x00000000, stage=kSwapStage_NotStarted, remaining_size=0x00000000&lt;BR /&gt;Image Info:image[0].size=0x0x00000400, image[1].size=0x0x00000000&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Running bootloader...&lt;BR /&gt;Bootloader version K2.7.0&lt;BR /&gt;Initing HID&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 10 Jan 2020 09:47:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/How-to-run-evkmimxrt1060-lwip-httpssrv-ota-freertos/m-p/977957#M5108</guid>
      <dc:creator>felix1</dc:creator>
      <dc:date>2020-01-10T09:47:07Z</dc:date>
    </item>
    <item>
      <title>Re: How to run evkmimxrt1060_lwip_httpssrv_ota_freertos?</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/How-to-run-evkmimxrt1060-lwip-httpssrv-ota-freertos/m-p/977958#M5109</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;evkmimxrt1060_ota_bootloader seems stuck in get_active_peripheral(), why?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 13 Jan 2020 11:19:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/How-to-run-evkmimxrt1060-lwip-httpssrv-ota-freertos/m-p/977958#M5109</guid>
      <dc:creator>felix1</dc:creator>
      <dc:date>2020-01-13T11:19:17Z</dc:date>
    </item>
    <item>
      <title>Re: How to run evkmimxrt1060_lwip_httpssrv_ota_freertos?</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/How-to-run-evkmimxrt1060-lwip-httpssrv-ota-freertos/m-p/977959#M5110</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;SPAN class=""&gt;&lt;A _jive_internal="true" data-userid="340883" data-username="felix@portalinks.com.tw" href="https://community.nxp.com/people/felix@portalinks.com.tw"&gt;Felix Shih&lt;/A&gt;&lt;/SPAN&gt;,&lt;/P&gt;&lt;P&gt;&amp;nbsp; Sorry for our later reply!&lt;/P&gt;&lt;P&gt;&amp;nbsp; Please tell me which SDK version you are using? SDK2.7.0?&lt;/P&gt;&lt;P&gt;&amp;nbsp; All the examples in the SDK is tested.&lt;/P&gt;&lt;P&gt;&amp;nbsp; Do you fully follow the SDK ota bootloader and lwip_httpssrv_ota readme to test it?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Kerry&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jan 2020 09:57:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/How-to-run-evkmimxrt1060-lwip-httpssrv-ota-freertos/m-p/977959#M5110</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2020-01-15T09:57:10Z</dc:date>
    </item>
    <item>
      <title>Re: How to run evkmimxrt1060_lwip_httpssrv_ota_freertos?</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/How-to-run-evkmimxrt1060-lwip-httpssrv-ota-freertos/m-p/977960#M5111</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;1)&amp;nbsp;SDK_2.7.0_EVK-MIMXRT1060&lt;/P&gt;&lt;P&gt;2)&amp;nbsp;evkmimxrt1060_ota_bootloader,&amp;nbsp;evkmimxrt1060_lwip_httpssrv_ota_freertos&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; follow the readme to test it. You can tell me which readme item should be noticed, maybe I not notice it.&lt;/P&gt;&lt;P&gt;3) If you can jump to the application success, please give your console log for me to trace the steps.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jan 2020 10:36:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/How-to-run-evkmimxrt1060-lwip-httpssrv-ota-freertos/m-p/977960#M5111</guid>
      <dc:creator>felix1</dc:creator>
      <dc:date>2020-01-15T10:36:45Z</dc:date>
    </item>
    <item>
      <title>Re: How to run evkmimxrt1060_lwip_httpssrv_ota_freertos?</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/How-to-run-evkmimxrt1060-lwip-httpssrv-ota-freertos/m-p/977961#M5112</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Kerry,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;any updated information?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 17 Jan 2020 07:19:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/How-to-run-evkmimxrt1060-lwip-httpssrv-ota-freertos/m-p/977961#M5112</guid>
      <dc:creator>felix1</dc:creator>
      <dc:date>2020-01-17T07:19:40Z</dc:date>
    </item>
    <item>
      <title>Re: How to run evkmimxrt1060_lwip_httpssrv_ota_freertos?</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/How-to-run-evkmimxrt1060-lwip-httpssrv-ota-freertos/m-p/977962#M5113</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;SPAN class=""&gt;&lt;A _jive_internal="true" class="" data-userid="340883" data-username="felix@portalinks.com.tw" href="https://community.nxp.com/people/felix@portalinks.com.tw"&gt;Felix Shih&lt;/A&gt;&lt;/SPAN&gt;,&lt;/P&gt;&lt;P&gt;&amp;nbsp; Sorry for my later reply, there are really too many cases on the queue.&lt;/P&gt;&lt;P&gt;&amp;nbsp; I will find time to test it, and give you the log, and I have contact with our SDK testing team, they confirmed this example works.&lt;/P&gt;&lt;P&gt;&amp;nbsp; So, please give me more time, after I test it, I will let you know the log and result.&lt;/P&gt;&lt;P&gt;&amp;nbsp; Thanks a lot for your understanding.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Kerry&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 17 Jan 2020 09:02:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/How-to-run-evkmimxrt1060-lwip-httpssrv-ota-freertos/m-p/977962#M5113</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2020-01-17T09:02:11Z</dc:date>
    </item>
    <item>
      <title>Re: How to run evkmimxrt1060_lwip_httpssrv_ota_freertos?</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/How-to-run-evkmimxrt1060-lwip-httpssrv-ota-freertos/m-p/977963#M5114</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P style="color: #656668; background-color: #ffffff; font-weight: 300; font-size: 16px; margin: 0px 0px 15px;"&gt;&lt;SPAN style="color: #000000;"&gt;1. Login to ALM project (as in your example code, declare 'td' object then login and connect to an ALM project)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #000000;"&gt;2. Get hold of a&amp;nbsp;&lt;SPAN&gt;Test object&lt;/SPAN&gt;&amp;nbsp;from TDConnection object, then&amp;nbsp;&lt;SPAN&gt;TestFactory object&lt;/SPAN&gt;&amp;nbsp;by the ID or name of the test case.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #000000;"&gt;3. Use '&lt;SPAN&gt;CoverRequirement&lt;/SPAN&gt;' method of Test object to add a requirement to be covered by this test, by requirement ID.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #000000;"&gt;4. Use&amp;nbsp;&lt;SPAN&gt;'&lt;/SPAN&gt;&lt;SPAN&gt;RemoveCoverage&lt;/SPAN&gt;'&amp;nbsp;mthod of&amp;nbsp;&lt;SPAN&gt;Test object&lt;/SPAN&gt;&amp;nbsp;to remove the requirement object.&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="color: #656668; background-color: #ffffff; font-weight: 300; font-size: 16px; margin: 0px 0px 15px;"&gt;&lt;SPAN style="color: #000000;"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="color: #656668; background-color: #ffffff; font-weight: 300; font-size: 16px; margin: 0px 0px 15px;"&gt;&lt;SPAN style="color: #000000;"&gt;Is there any opictorial representation(diagram) of object model available listing the objects and fuctions through which can understand the flow.&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="color: #656668; background-color: #ffffff; font-weight: 300; font-size: 16px; margin: 0px 0px 15px;"&gt;&amp;nbsp;&lt;STRONG&gt;&lt;SPAN data-sheets-userformat="{&amp;quot;2&amp;quot;:768,&amp;quot;11&amp;quot;:3,&amp;quot;12&amp;quot;:0}" data-sheets-value="{&amp;quot;1&amp;quot;:2,&amp;quot;2&amp;quot;:&amp;quot;Mybkexperience&amp;quot;}" style="font-size: 10pt;"&gt;&lt;A href="https://www.mybkexperience.xyz/"&gt;Mybkexperience&lt;/A&gt;&lt;/SPAN&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 17 Jan 2020 09:08:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/How-to-run-evkmimxrt1060-lwip-httpssrv-ota-freertos/m-p/977963#M5114</guid>
      <dc:creator>willieken49</dc:creator>
      <dc:date>2020-01-17T09:08:27Z</dc:date>
    </item>
    <item>
      <title>Re: How to run evkmimxrt1060_lwip_httpssrv_ota_freertos?</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/How-to-run-evkmimxrt1060-lwip-httpssrv-ota-freertos/m-p/977964#M5115</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Madison,&lt;/P&gt;&lt;P&gt;About the above steps, I do not know what it means?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hi Kerry,&amp;nbsp;&lt;/P&gt;&lt;P&gt;Do you have time to test OTA sample before Chinese New Year?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Jan 2020 05:53:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/How-to-run-evkmimxrt1060-lwip-httpssrv-ota-freertos/m-p/977964#M5115</guid>
      <dc:creator>felix1</dc:creator>
      <dc:date>2020-01-21T05:53:10Z</dc:date>
    </item>
    <item>
      <title>Re: How to run evkmimxrt1060_lwip_httpssrv_ota_freertos?</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/How-to-run-evkmimxrt1060-lwip-httpssrv-ota-freertos/m-p/977965#M5116</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Felix,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Which toolchain do you use?&lt;/P&gt;&lt;P&gt;How do you program the bootloader and the application to FLASH memory?&lt;/P&gt;&lt;P&gt;Do you use debugger in IDE or do you program it using flash loader (e.g. blhost)?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The intended workflow is to program the bootloader, let it run at lease once (the bootloader creates default partition set, i.e. formats the FLASH) and then program the application and reboot. The example in the final 2.7.0 release should be then able to start from cold boot&amp;nbsp;without issues.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards, Pavel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 Jan 2020 09:16:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/How-to-run-evkmimxrt1060-lwip-httpssrv-ota-freertos/m-p/977965#M5116</guid>
      <dc:creator>pavel_chromy</dc:creator>
      <dc:date>2020-01-23T09:16:27Z</dc:date>
    </item>
    <item>
      <title>Re: How to run evkmimxrt1060_lwip_httpssrv_ota_freertos?</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/How-to-run-evkmimxrt1060-lwip-httpssrv-ota-freertos/m-p/977966#M5117</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Pavel,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;my steps are as fellow,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;IDE: MCUXpresso IDE v11.1.0&lt;BR /&gt;SDK: SDK_2.7.0_EVK-MIMXRT1060&lt;BR /&gt;HW: MIMXRT1060-EVK&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1) use MCUXpresso to program evkmimxrt1060_ota_bootloader&lt;BR /&gt; see the following messages from UART,&lt;BR /&gt;...&lt;BR /&gt; Running bootloader...&lt;BR /&gt; Bootloader version K2.7.0&lt;BR /&gt; Initing HID&lt;BR /&gt; &lt;BR /&gt;2) use MCUXpresso to program evkmimxrt1060_lwip_httpssrv_ota_freertos&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;3) press SW3 to reboot&lt;/P&gt;&lt;P&gt;still just the bootloader messages from UART,&lt;BR /&gt;...&lt;BR /&gt; Running bootloader...&lt;BR /&gt; Bootloader version K2.7.0&lt;BR /&gt; Initing HID&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 30 Jan 2020 03:54:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/How-to-run-evkmimxrt1060-lwip-httpssrv-ota-freertos/m-p/977966#M5117</guid>
      <dc:creator>felix1</dc:creator>
      <dc:date>2020-01-30T03:54:34Z</dc:date>
    </item>
    <item>
      <title>Re: How to run evkmimxrt1060_lwip_httpssrv_ota_freertos?</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/How-to-run-evkmimxrt1060-lwip-httpssrv-ota-freertos/m-p/977967#M5118</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Felix,&lt;/P&gt;&lt;P&gt;I was able to reproduce the issue and it seems to be related to MCUX build of OTA bootloader - it is fine with other toolchain(s). This is indeed a bug, unfortunately root cause and workaround it not known yet. I am creating ticket for this.&lt;/P&gt;&lt;P&gt;Best regards, Pavel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 07 Feb 2020 12:25:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/How-to-run-evkmimxrt1060-lwip-httpssrv-ota-freertos/m-p/977967#M5118</guid>
      <dc:creator>pavel_chromy</dc:creator>
      <dc:date>2020-02-07T12:25:29Z</dc:date>
    </item>
    <item>
      <title>Re: How to run evkmimxrt1060_lwip_httpssrv_ota_freertos?</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/How-to-run-evkmimxrt1060-lwip-httpssrv-ota-freertos/m-p/977968#M5119</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Any update on this?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am having the same issue with my own custom MIMXRT1061 board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The system eternally waits for HID initialization with: 'Initing HID' message.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Mar 2020 21:10:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/How-to-run-evkmimxrt1060-lwip-httpssrv-ota-freertos/m-p/977968#M5119</guid>
      <dc:creator>tkroeger</dc:creator>
      <dc:date>2020-03-20T21:10:04Z</dc:date>
    </item>
    <item>
      <title>Re: How to run evkmimxrt1060_lwip_httpssrv_ota_freertos?</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/How-to-run-evkmimxrt1060-lwip-httpssrv-ota-freertos/m-p/977969#M5120</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have exactly the same question.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using the MIMXRT1060-EVK and I'm trying to run the SDK 2.7's evkmimxrt1060_httpssrv_ota_freertos example via MCUXpresso IDE. This example runs a webserver through which I should be able to upload new firmware.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;From reading the the h&lt;SPAN&gt;ttpssrv_ota_freertos&amp;nbsp;&lt;/SPAN&gt;readme.txt, it seems I first need to write ota_bootloader to flash. So I get the SDK's evkmimxrt1060_ota_bootloader code,&amp;nbsp;and build it. Then I launch and load the debugger. SW7 is set to 0010 (QSPI flash).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;During execution, main() gets stuck in bootloader_init(). Specifically, it&amp;nbsp;hangs&amp;nbsp;in get_active_peripheral():&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt; Thread #1 1 (Suspended : Step) &lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;get_active_peripheral() at bl_main.c:425 0x600061ce &lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;bootloader_init() at bl_main.c:583 0x600061ce &lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;main() at bl_main.c:639 0x600061ce&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It never exits this loop. No diagnostic messages appear via the serial port.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can you help me execute the httpssrv_ota_freertos example??&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;regards&lt;/P&gt;&lt;P&gt;-Rob&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 Apr 2020 23:04:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/How-to-run-evkmimxrt1060-lwip-httpssrv-ota-freertos/m-p/977969#M5120</guid>
      <dc:creator>rob4</dc:creator>
      <dc:date>2020-04-23T23:04:54Z</dc:date>
    </item>
    <item>
      <title>Re: How to run evkmimxrt1060_lwip_httpssrv_ota_freertos?</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/How-to-run-evkmimxrt1060-lwip-httpssrv-ota-freertos/m-p/977970#M5121</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&amp;nbsp;&lt;A _jive_internal="true" data-content-finding="Community" data-userid="358514" data-username="rob@signalessence.com" href="https://community.nxp.com/people/rob@signalessence.com" style="color: #3d9ce7; background-color: #ffffff; border: 0px; font-weight: 200; text-decoration: underline; font-size: 1.286rem;"&gt;Rob Yu&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;&amp;nbsp; Do you try to download the&amp;nbsp;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;ota_bootloader release version at first instead of the debug version? This version should works.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;&amp;nbsp;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Best Regards,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Kerry&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 27 Apr 2020 04:20:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/How-to-run-evkmimxrt1060-lwip-httpssrv-ota-freertos/m-p/977970#M5121</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2020-04-27T04:20:07Z</dc:date>
    </item>
    <item>
      <title>Re: How to run evkmimxrt1060_lwip_httpssrv_ota_freertos?</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/How-to-run-evkmimxrt1060-lwip-httpssrv-ota-freertos/m-p/977971#M5122</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi Kerry,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I just cleaned + rebuilt the project as a "release" version, then executed it from the debugger.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The LED flashes and I don't see anything on serial port terminal (I don't know if this is expected from a "release" executable).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I hit the pause button, I can see that execution is still in bootloader_init()--it never gets to bootloader_run().&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'andale mono', monospace;"&gt;Thread #1 1 (Suspended : Signal : SIGINT:Interrupt) &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="font-family: 'andale mono', monospace;"&gt;&amp;nbsp; usb_hid_poll_for_activity() at usb_hid_msc_peripheral_interface.c:119 0x600062b2 &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="font-family: 'andale mono', monospace;"&gt;&amp;nbsp; get_active_peripheral() at bl_main.c:425 0x60005ace &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="font-family: 'andale mono', monospace;"&gt;&amp;nbsp; bootloader_init() at bl_main.c:583 0x60005ace &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="font-family: 'andale mono', monospace;"&gt;&amp;nbsp; main() at bl_main.c:639 0x60005ace&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do you have any suggestions for how to proceed? Is the&amp;nbsp;executable looking for a USB peripheral and not finding it?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Apr 2020 01:09:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/How-to-run-evkmimxrt1060-lwip-httpssrv-ota-freertos/m-p/977971#M5122</guid>
      <dc:creator>rob4</dc:creator>
      <dc:date>2020-04-28T01:09:25Z</dc:date>
    </item>
    <item>
      <title>Re: How to run evkmimxrt1060_lwip_httpssrv_ota_freertos?</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/How-to-run-evkmimxrt1060-lwip-httpssrv-ota-freertos/m-p/977972#M5123</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&amp;nbsp;&lt;A _jive_internal="true" class="" data-content-finding="Community" data-userid="358514" data-username="rob@signalessence.com" href="https://community.nxp.com/people/rob@signalessence.com" style="color: #3d9ce7; background-color: #ffffff; border: 0px; font-weight: 200; text-decoration: underline; font-size: 1.286rem;"&gt;Rob Yu&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;I will find time to test it on my side, please keep patient, any updated information, I will let you know.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Kerry&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 29 Apr 2020 07:25:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/How-to-run-evkmimxrt1060-lwip-httpssrv-ota-freertos/m-p/977972#M5123</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2020-04-29T07:25:18Z</dc:date>
    </item>
    <item>
      <title>Re: How to run evkmimxrt1060_lwip_httpssrv_ota_freertos?</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/How-to-run-evkmimxrt1060-lwip-httpssrv-ota-freertos/m-p/977973#M5124</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;thanks Kerry. I appreciate your help.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-Rob&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 29 Apr 2020 16:02:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/How-to-run-evkmimxrt1060-lwip-httpssrv-ota-freertos/m-p/977973#M5124</guid>
      <dc:creator>rob4</dc:creator>
      <dc:date>2020-04-29T16:02:42Z</dc:date>
    </item>
    <item>
      <title>Re: How to run evkmimxrt1060_lwip_httpssrv_ota_freertos?</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/How-to-run-evkmimxrt1060-lwip-httpssrv-ota-freertos/m-p/977974#M5125</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Note that the uTasker project has supported HTTP OTA web server upgrade integrated (also encrypted uploads) so can be used without needing to solve problems with examples and saves professional projects time. It also works on all standard processors and boards without any porting effort:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="text-decoration: underline;"&gt;Ethernet processors:&lt;/SPAN&gt;&lt;BR /&gt;MIMXRT1020-EVK with i.MX RT 1021 - &lt;A href="https://www.utasker.com/iMX/RT1020.html" target="test_blank"&gt;https://www.utasker.com/iMX/RT1020.html&lt;/A&gt;&lt;BR /&gt;MIMXRT1050-EVK with i.MX RT 1052 - &lt;A href="https://www.utasker.com/iMX/RT1050.html" target="test_blank"&gt;https://www.utasker.com/iMX/RT1050.html&lt;/A&gt;&lt;BR /&gt;Embedded Artists iMX RT1052 OEM with i.MX RT 1052 - &lt;A href="https://www.utasker.com/iMX/iMX_RT1052_OEM.html" target="test_blank"&gt;https://www.utasker.com/iMX/iMX_RT1052_OEM.html&lt;/A&gt;&lt;BR /&gt;MIMXRT1060-EVK with i.MX RT 1062 - &lt;A href="https://www.utasker.com/iMX/RT1060.html" target="test_blank"&gt;https://www.utasker.com/iMX/RT1060.html&lt;/A&gt;&lt;BR /&gt;Embedded Artists iMX RT1062 OEM with i.MX RT 1062 - &lt;A href="https://www.utasker.com/iMX/iMX_RT1062_OEM.html" target="test_blank"&gt;https://www.utasker.com/iMX/iMX_RT1062_OEM.html&lt;/A&gt;&lt;BR /&gt;MIMXRT1064-EVK with i.MX RT 1064 - &lt;A href="https://www.utasker.com/iMX/RT1064.html" target="test_blank"&gt;https://www.utasker.com/iMX/RT1064.html&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;BR /&gt;&lt;EM&gt;[uTasker project developer for Kinetis and i.MX RT]&lt;/EM&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 29 Apr 2020 16:20:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/How-to-run-evkmimxrt1060-lwip-httpssrv-ota-freertos/m-p/977974#M5125</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2020-04-29T16:20:05Z</dc:date>
    </item>
  </channel>
</rss>