<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX RT Crossover MCUsのトピックAdditional SDRAM input using CS1</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Additional-SDRAM-input-using-CS1/m-p/1230614#M12663</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm trying to use an additional SDRAM(total 2 SDRAM) to RT1064.&lt;/P&gt;&lt;P&gt;It is connected&amp;nbsp; CS0(GPIO_EMC_29) to the first SDRAM as EVK board and I'm going to use&amp;nbsp; SEMC_CSX0(GPIO_EMC_41) for CS1 of the second SDRAM.&lt;/P&gt;&lt;P&gt;However, an error occurs in the MUX_CSX0 PIN as shown below.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="youngsangcho_0-1613163165643.png" style="width: 477px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/137146i53F84C49060B06F3/image-dimensions/477x98?v=v2" width="477" height="98" role="button" title="youngsangcho_0-1613163165643.png" alt="youngsangcho_0-1613163165643.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Is it an MCUXpresso Config tool bug or I can't use the&amp;nbsp;SEMC_CSX0(GPIO_EMC_41)&amp;nbsp; pin for SDRAM CS1?&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;YC&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Fri, 12 Feb 2021 21:01:26 GMT</pubDate>
    <dc:creator>youngsangcho</dc:creator>
    <dc:date>2021-02-12T21:01:26Z</dc:date>
    <item>
      <title>Additional SDRAM input using CS1</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Additional-SDRAM-input-using-CS1/m-p/1230614#M12663</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm trying to use an additional SDRAM(total 2 SDRAM) to RT1064.&lt;/P&gt;&lt;P&gt;It is connected&amp;nbsp; CS0(GPIO_EMC_29) to the first SDRAM as EVK board and I'm going to use&amp;nbsp; SEMC_CSX0(GPIO_EMC_41) for CS1 of the second SDRAM.&lt;/P&gt;&lt;P&gt;However, an error occurs in the MUX_CSX0 PIN as shown below.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="youngsangcho_0-1613163165643.png" style="width: 477px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/137146i53F84C49060B06F3/image-dimensions/477x98?v=v2" width="477" height="98" role="button" title="youngsangcho_0-1613163165643.png" alt="youngsangcho_0-1613163165643.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Is it an MCUXpresso Config tool bug or I can't use the&amp;nbsp;SEMC_CSX0(GPIO_EMC_41)&amp;nbsp; pin for SDRAM CS1?&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;YC&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 12 Feb 2021 21:01:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Additional-SDRAM-input-using-CS1/m-p/1230614#M12663</guid>
      <dc:creator>youngsangcho</dc:creator>
      <dc:date>2021-02-12T21:01:26Z</dc:date>
    </item>
    <item>
      <title>Re: Additional SDRAM input using CS1</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Additional-SDRAM-input-using-CS1/m-p/1232645#M12737</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;&amp;nbsp; It is possible to use SEMC_CSX0(GPIO_EMC_41) as CS1 for the second SDRAM.&lt;BR /&gt;Customers can use i.MX Pins tool.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/design/designs/config-tools-for-i-mx-applications-processors:CONFIG-TOOLS-IMX" target="_blank"&gt;https://www.nxp.com/design/designs/config-tools-for-i-mx-applications-processors:CONFIG-TOOLS-IMX&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Yuri.&lt;/P&gt;</description>
      <pubDate>Thu, 18 Feb 2021 07:51:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Additional-SDRAM-input-using-CS1/m-p/1232645#M12737</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2021-02-18T07:51:32Z</dc:date>
    </item>
    <item>
      <title>Re: Additional SDRAM input using CS1</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Additional-SDRAM-input-using-CS1/m-p/1233149#M12760</link>
      <description>&lt;P&gt;Thanks for the confirmation.&lt;/P&gt;&lt;P&gt;Young&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 18 Feb 2021 22:38:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Additional-SDRAM-input-using-CS1/m-p/1233149#M12760</guid>
      <dc:creator>youngsangcho</dc:creator>
      <dc:date>2021-02-18T22:38:07Z</dc:date>
    </item>
  </channel>
</rss>