<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX RT Crossover MCUs中的主题 Re: OTP Memory Usage</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/OTP-Memory-Usage/m-p/1226184#M12565</link>
    <description>&lt;P&gt;Thanks for you reply.According to the datesheet,some area is for special use,for example,the rom patch.&lt;/P&gt;&lt;P&gt;I just want to use the area that doesnot&amp;nbsp;affect other functions. Can you give some suggestion?&lt;/P&gt;</description>
    <pubDate>Thu, 04 Feb 2021 07:50:44 GMT</pubDate>
    <dc:creator>goodboy2024</dc:creator>
    <dc:date>2021-02-04T07:50:44Z</dc:date>
    <item>
      <title>OTP Memory Usage</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/OTP-Memory-Usage/m-p/1226030#M12558</link>
      <description>&lt;P&gt;RT1061 is used in our project.Recently we want to use the OTP function.I have a few questions as below.&lt;/P&gt;&lt;P&gt;1.All OTP space that can be used is shown in the OTP Memory Footprint?&lt;/P&gt;&lt;P&gt;2. Which part can be free used for our own&amp;nbsp;software？It seems that some are used for&amp;nbsp;special purpose&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 04 Feb 2021 03:18:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/OTP-Memory-Usage/m-p/1226030#M12558</guid>
      <dc:creator>goodboy2024</dc:creator>
      <dc:date>2021-02-04T03:18:58Z</dc:date>
    </item>
    <item>
      <title>Re: OTP Memory Usage</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/OTP-Memory-Usage/m-p/1226167#M12563</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.&lt;BR /&gt;1) All OTP space that can be used is shown in the OTP Memory Footprint?&lt;BR /&gt;-- No, the shadow registers don't reload to the value of all OTP space.&lt;BR /&gt;2) Which part can be free used for our own software？&lt;BR /&gt;-- It's able to manipulate all OTP space.&lt;BR /&gt;Hope this is clear&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Thu, 04 Feb 2021 07:25:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/OTP-Memory-Usage/m-p/1226167#M12563</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2021-02-04T07:25:54Z</dc:date>
    </item>
    <item>
      <title>Re: OTP Memory Usage</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/OTP-Memory-Usage/m-p/1226184#M12565</link>
      <description>&lt;P&gt;Thanks for you reply.According to the datesheet,some area is for special use,for example,the rom patch.&lt;/P&gt;&lt;P&gt;I just want to use the area that doesnot&amp;nbsp;affect other functions. Can you give some suggestion?&lt;/P&gt;</description>
      <pubDate>Thu, 04 Feb 2021 07:50:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/OTP-Memory-Usage/m-p/1226184#M12565</guid>
      <dc:creator>goodboy2024</dc:creator>
      <dc:date>2021-02-04T07:50:44Z</dc:date>
    </item>
    <item>
      <title>Re: OTP Memory Usage</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/OTP-Memory-Usage/m-p/1226757#M12581</link>
      <description>&lt;P&gt;Hi,&lt;BR /&gt;Thanks for your reply.&lt;BR /&gt;In the Fuse map, it doesn't demonstrate the area (0x830~0x870), in my opinion, this area likes the reserved area. Customers must not attempt to burn these.&lt;BR /&gt;If you want to store some data in the Fuse, you can program the value to the General Purpose fuse registers.&lt;BR /&gt;Hope it helps.&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Fri, 05 Feb 2021 03:18:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/OTP-Memory-Usage/m-p/1226757#M12581</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2021-02-05T03:18:40Z</dc:date>
    </item>
  </channel>
</rss>