<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: RT1064 EVK Flashloader example removed from SDK? in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1064-EVK-Flashloader-example-removed-from-SDK/m-p/1220475#M12400</link>
    <description>&lt;P&gt;Oh, but it doesn't include CAN. That's only available in the binary?&lt;/P&gt;</description>
    <pubDate>Mon, 25 Jan 2021 10:49:22 GMT</pubDate>
    <dc:creator>p_shep</dc:creator>
    <dc:date>2021-01-25T10:49:22Z</dc:date>
    <item>
      <title>RT1064 EVK Flashloader example removed from SDK?</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1064-EVK-Flashloader-example-removed-from-SDK/m-p/1220437#M12398</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I'm looking to build the example flashloader project for the RT1064... but I can't find it.&lt;/P&gt;&lt;P&gt;In the SDK 2.9.1 (and 2.9.0) there's some source code in&amp;nbsp;.\middleware\mcu-boot, but I'm not sure how that fits into to a project. I could probably work it out, but I suspect there are example projects already available somewhere!&lt;/P&gt;&lt;P&gt;I have found the flashloader binary for the RT1064, but want to change a few things around for our purposes.&lt;/P&gt;&lt;P&gt;In RT1050 SDK there is the example flashloader project which I guess can be ported, but wonder if that might be older code.&lt;/P&gt;&lt;P&gt;So, where can I find the example flashloader project for the RT1064-EVK?&lt;/P&gt;</description>
      <pubDate>Mon, 25 Jan 2021 10:14:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1064-EVK-Flashloader-example-removed-from-SDK/m-p/1220437#M12398</guid>
      <dc:creator>p_shep</dc:creator>
      <dc:date>2021-01-25T10:14:58Z</dc:date>
    </item>
    <item>
      <title>Re: RT1064 EVK Flashloader example removed from SDK?</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1064-EVK-Flashloader-example-removed-from-SDK/m-p/1220451#M12399</link>
      <description>&lt;P&gt;Ah, so the magic is to select the USB host option on the SDK middleware components... ???&lt;/P&gt;&lt;P&gt;Now it's in the SDK build.&lt;/P&gt;</description>
      <pubDate>Mon, 25 Jan 2021 10:28:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1064-EVK-Flashloader-example-removed-from-SDK/m-p/1220451#M12399</guid>
      <dc:creator>p_shep</dc:creator>
      <dc:date>2021-01-25T10:28:25Z</dc:date>
    </item>
    <item>
      <title>Re: RT1064 EVK Flashloader example removed from SDK?</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1064-EVK-Flashloader-example-removed-from-SDK/m-p/1220475#M12400</link>
      <description>&lt;P&gt;Oh, but it doesn't include CAN. That's only available in the binary?&lt;/P&gt;</description>
      <pubDate>Mon, 25 Jan 2021 10:49:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1064-EVK-Flashloader-example-removed-from-SDK/m-p/1220475#M12400</guid>
      <dc:creator>p_shep</dc:creator>
      <dc:date>2021-01-25T10:49:22Z</dc:date>
    </item>
  </channel>
</rss>