<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Using MFGtools with MIMRX1060-EVK in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Using-MFGtools-with-MIMRX1060-EVK/m-p/1217105#M12286</link>
    <description>&lt;P&gt;Hello Kerry!&lt;/P&gt;&lt;P&gt;Always thank you for your generous support. Yes, I managed to get MFG tool working with with my dev board for IMXRt1060 MCU.&lt;/P&gt;&lt;P&gt;Now, I am trying to repeat same process on my new dev board iMX RT1176xxxxA. I repeated same steps (of course with different files), but I could not get the blinky LED to work. Again I attached the files I generated.&lt;/P&gt;&lt;P&gt;I also added these to my IDE: XIP_EXTERNAL_FLASH=1, XIP_BOOT_HEADER_ENABLE=0,XIP_BOOT_HEADER_DCD_ENABLE=0.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Please have a look and see if I am missing anything.&lt;/P&gt;</description>
    <pubDate>Tue, 19 Jan 2021 20:36:02 GMT</pubDate>
    <dc:creator>fmabrouk</dc:creator>
    <dc:date>2021-01-19T20:36:02Z</dc:date>
    <item>
      <title>Using MFGtools with MIMRX1060-EVK</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Using-MFGtools-with-MIMRX1060-EVK/m-p/1211997#M12192</link>
      <description>&lt;P&gt;I am using MFGtools to program the spi nor flash. I followed all the steps as described in some of the manuals. I initially set up the board for serial boot using the dip switches on SW7 and after I finished I put the dip switches back so that it is on internal boot. I reset the unit but I did not see the LED flashes.&lt;/P&gt;&lt;P&gt;any Idea what I could missed?&lt;/P&gt;</description>
      <pubDate>Fri, 15 Jan 2021 00:55:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Using-MFGtools-with-MIMRX1060-EVK/m-p/1211997#M12192</guid>
      <dc:creator>fmabrouk</dc:creator>
      <dc:date>2021-01-15T00:55:51Z</dc:date>
    </item>
    <item>
      <title>Re: Using MFGtools with MIMRX1060-EVK</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Using-MFGtools-with-MIMRX1060-EVK/m-p/1212010#M12193</link>
      <description>&lt;P&gt;I initially used .bin file that I copied to elftosb\win directory.&lt;/P&gt;&lt;P&gt;But later when I tried using a .s19 file, the no boot image was generated.&lt;/P&gt;</description>
      <pubDate>Fri, 15 Jan 2021 01:23:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Using-MFGtools-with-MIMRX1060-EVK/m-p/1212010#M12193</guid>
      <dc:creator>fmabrouk</dc:creator>
      <dc:date>2021-01-15T01:23:52Z</dc:date>
    </item>
    <item>
      <title>Re: Using MFGtools with MIMRX1060-EVK</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Using-MFGtools-with-MIMRX1060-EVK/m-p/1212013#M12194</link>
      <description>&lt;P&gt;In this case, do I need to generate a .srec output file? I am able to only generate .s19 file. How can I generated .serc file if that's what I need to copy to the MFGTool folder?&lt;/P&gt;</description>
      <pubDate>Fri, 15 Jan 2021 01:33:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Using-MFGtools-with-MIMRX1060-EVK/m-p/1212013#M12194</guid>
      <dc:creator>fmabrouk</dc:creator>
      <dc:date>2021-01-15T01:33:16Z</dc:date>
    </item>
    <item>
      <title>Re: Using MFGtools with MIMRX1060-EVK</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Using-MFGtools-with-MIMRX1060-EVK/m-p/1212083#M12197</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;SPAN&gt;fmabrouk,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&amp;nbsp; In fact, if you just want to download the code, I highly suggest you use the MCUBootUtility tool instead of the MFG tool, MCUBootutility tool can be downloaded from this link, it is based on the GUI, and more easy to use, just need to provide the app firmware is OK. This tool is also based on the elftosb, blhost and sdphost.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&lt;A href="https://github.com/JayHeng/NXP-MCUBootUtility/releases/tag/v3.0.0" target="_blank" rel="noopener"&gt;https://github.com/JayHeng/NXP-MCUBootUtility/releases/tag/v3.0.0&lt;/A&gt; &lt;BR /&gt;the related user manual is:&lt;BR /&gt;&lt;A href="https://github.com/JayHeng/NXP-MCUBootUtility" target="_blank" rel="noopener"&gt;https://github.com/JayHeng/NXP-MCUBootUtility&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;But talk back to your MFG tool question,&amp;nbsp; please refer to this application note step by step:&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN12108.pdf" target="_blank" rel="noopener"&gt;https://www.nxp.com/docs/en/application-note/AN12108.pdf&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;.S19 is also OK, it is just the .srec, please don't worry.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;You also need to use the&amp;nbsp;imx-flexspinor-normal-unsigned.bd,&amp;nbsp;program_flexspinor_image_qspinor.bd, do you also use that file?&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&amp;nbsp; I suggest you use the MCUBootUtiltiy tool to download the code at first, after it is success, you can try the MFG method again, the MCUbootUtility also have the detail command log.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;BTW, in imx-flexspinor-normal-unsigned.bd you also can set your enterPointAddress to your real app entry point.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Eg, the following .srec or .s19, the entry point is :&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;entryPointAddress = 0x60004699;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="image.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/134828i2F1DD7EEDB3F87E8/image-size/large?v=v2&amp;amp;px=999" role="button" title="image.png" alt="image.png" /&gt;&lt;/span&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Wish it helps you!&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;If you still have questions about it, please kindly let me know.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Best Regards,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Kerry&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 19 Jan 2021 01:25:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Using-MFGtools-with-MIMRX1060-EVK/m-p/1212083#M12197</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2021-01-19T01:25:10Z</dc:date>
    </item>
    <item>
      <title>Re: Using MFGtools with MIMRX1060-EVK</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Using-MFGtools-with-MIMRX1060-EVK/m-p/1213584#M12255</link>
      <description>&lt;P&gt;Hello Kerry!&lt;/P&gt;&lt;P&gt;I am not using this imx-flexspinor-plugin-unsigned.bd ; do I need to use it?&lt;/P&gt;&lt;P&gt;here is a log of what I did:&lt;/P&gt;&lt;P&gt;C:\Users\...\Documents\NXP Tools\FLASHLOADER-RT106x-1-GA\Flashloader_RT106x_1.0_GA\Tools\elftosb\win&amp;gt;elftosb.exe -f imx -V -c ../../bd_file/imx10xx/imx-flexspinor-normal-unsigned.bd -o ivt_evkmimxrt1060_igpio_led_output.bin evkmimxrt1060_igpio_led_output.bin&lt;BR /&gt;Section: 0x0&lt;BR /&gt;iMX bootable image generated successfully&lt;/P&gt;&lt;P&gt;C:\Users\..\Documents\NXP Tools\FLASHLOADER-RT106x-1-GA\Flashloader_RT106x_1.0_GA\Tools\elftosb\win&amp;gt;elftosb.exe -f kinetis -V -c ../../bd_file/imx10xx/program_flexspinor_image_qspinor.bd -o boot_image.sb ivt_evkmimxrt1060_igpio_led_output_nopadding.bin&lt;BR /&gt;Boot Section 0x00000000:&lt;BR /&gt;FILL | adr=0x00002000 | len=0x00000004 | ptn=0xc0000007&lt;BR /&gt;ENA | adr=0x00002000 | cnt=0x00000004 | flg=0x0900&lt;BR /&gt;ERAS | adr=0x60000000 | cnt=0x00010000 | flg=0x0000&lt;BR /&gt;FILL | adr=0x00003000 | len=0x00000004 | ptn=0xf000000f&lt;BR /&gt;ENA | adr=0x00003000 | cnt=0x00000004 | flg=0x0900&lt;BR /&gt;LOAD | adr=0x60001000 | len=0x00006b60 | crc=0xe6d8d7e0 | flg=0x0000&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Attached are the boot files.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can you please verify what's wrong?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;About MCUboot utility, i am not able to open it on my wondows10. It just does not open up. Is there any changes I need to do to my PC?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;</description>
      <pubDate>Mon, 18 Jan 2021 20:48:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Using-MFGtools-with-MIMRX1060-EVK/m-p/1213584#M12255</guid>
      <dc:creator>fmabrouk</dc:creator>
      <dc:date>2021-01-18T20:48:03Z</dc:date>
    </item>
    <item>
      <title>Re: Using MFGtools with MIMRX1060-EVK</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Using-MFGtools-with-MIMRX1060-EVK/m-p/1216391#M12259</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;SPAN class=""&gt;&lt;A id="link_12" class="lia-link-navigation lia-page-link lia-user-name-link" href="https://community.nxp.com/t5/user/viewprofilepage/user-id/180445" target="_self"&gt;fmabrouk&lt;/A&gt;,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN class=""&gt;&amp;nbsp; It's the&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;imx-flexspinor-normal-unsigned.bd, not the&amp;nbsp;imx-flexspinor-plugin-unsigned.bd, sorry for the mistyping in the last reply.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&amp;nbsp; I checked your&amp;nbsp;evkmimxrt1060_igpio_led_output.bin, it already contains the IVT area, when you generate the code, you need to refer to&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN12108.pdf" target="_blank" rel="noopener nofollow noopener noreferrer"&gt;https://www.nxp.com/docs/en/application-note/AN12108.pdf&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt; configure :&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;XIP_EXTERNAL_FLASH=1,&amp;nbsp;XIP_BOOT_HEADER_ENABLE=0,XIP_BOOT_HEADER_DCD_ENABLE=0,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Then generate the .bin or .srec, and use the elftosb two command to generate the .sb again.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Your original&amp;nbsp;evkmimxrt1060_igpio_led_output.bin should not contain the IVT header.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Please try it again.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Wish it helps you!&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Best Regards,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Kerry&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 19 Jan 2021 01:52:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Using-MFGtools-with-MIMRX1060-EVK/m-p/1216391#M12259</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2021-01-19T01:52:14Z</dc:date>
    </item>
    <item>
      <title>Re: Using MFGtools with MIMRX1060-EVK</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Using-MFGtools-with-MIMRX1060-EVK/m-p/1216401#M12260</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;A id="link_12" class="lia-link-navigation lia-page-link lia-user-name-link" href="https://community.nxp.com/t5/user/viewprofilepage/user-id/180445" target="_self"&gt;fmabrouk&lt;/A&gt;&lt;SPAN&gt;,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;Share you my related files, my .sb file can work on my side, it has been tested.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 19 Jan 2021 02:03:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Using-MFGtools-with-MIMRX1060-EVK/m-p/1216401#M12260</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2021-01-19T02:03:46Z</dc:date>
    </item>
    <item>
      <title>Re: Using MFGtools with MIMRX1060-EVK</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Using-MFGtools-with-MIMRX1060-EVK/m-p/1217105#M12286</link>
      <description>&lt;P&gt;Hello Kerry!&lt;/P&gt;&lt;P&gt;Always thank you for your generous support. Yes, I managed to get MFG tool working with with my dev board for IMXRt1060 MCU.&lt;/P&gt;&lt;P&gt;Now, I am trying to repeat same process on my new dev board iMX RT1176xxxxA. I repeated same steps (of course with different files), but I could not get the blinky LED to work. Again I attached the files I generated.&lt;/P&gt;&lt;P&gt;I also added these to my IDE: XIP_EXTERNAL_FLASH=1, XIP_BOOT_HEADER_ENABLE=0,XIP_BOOT_HEADER_DCD_ENABLE=0.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Please have a look and see if I am missing anything.&lt;/P&gt;</description>
      <pubDate>Tue, 19 Jan 2021 20:36:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Using-MFGtools-with-MIMRX1060-EVK/m-p/1217105#M12286</guid>
      <dc:creator>fmabrouk</dc:creator>
      <dc:date>2021-01-19T20:36:02Z</dc:date>
    </item>
    <item>
      <title>Re: Using MFGtools with MIMRX1060-EVK</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Using-MFGtools-with-MIMRX1060-EVK/m-p/1217515#M12292</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;SPAN&gt;fmabrouk,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&amp;nbsp; &amp;nbsp;You are always welcome!&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&amp;nbsp; &amp;nbsp;About the new question to&amp;nbsp;RT1176xxxxA, could you please create a new question post or case?&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&amp;nbsp; I also have the&amp;nbsp;RT1176xxxxA board on my side, but the new case also need the working time, so could you please create one new case, if you still want me to provide service for you, you can write assign to Kerry Zhou in your question content.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&amp;nbsp; &amp;nbsp;After you create the new question, I will help you to test it on my MIMXRT1170-EVK board and reply to you in your new case, thanks a lot for your understanding!&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Best Regards,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Kerry&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 20 Jan 2021 01:56:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Using-MFGtools-with-MIMRX1060-EVK/m-p/1217515#M12292</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2021-01-20T01:56:57Z</dc:date>
    </item>
  </channel>
</rss>